<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: SPI availability on i.MX rt1170 in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SPI-availability-on-i-MX-rt1170/m-p/1744779#M27299</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/224536"&gt;@Nishantt&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Sorry for the inconvenience, I'm not understanding your question, is there a possibility for you to share with me a connection diagram and which camera you are using?&lt;/P&gt;
&lt;P&gt;You said your pins are&lt;/P&gt;
&lt;P&gt;CLK, MOSI, MISO, CLK. These connections are for normal SPI.&lt;/P&gt;
&lt;P&gt;I've found this post that could possibly help you.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-RT/imxrt1052-dual-spi/m-p/1656412" target="_self"&gt;Dual SPI&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Also, the iMXRT1170, supports MIPI CSI (Camera Serial Inteface) which can help you with the connection of the cameras.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards, Miguel.&lt;/P&gt;</description>
    <pubDate>Mon, 23 Oct 2023 21:16:39 GMT</pubDate>
    <dc:creator>Miguel04</dc:creator>
    <dc:date>2023-10-23T21:16:39Z</dc:date>
    <item>
      <title>SPI availability on i.MX rt1170</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SPI-availability-on-i-MX-rt1170/m-p/1742070#M27255</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;We are planning to use i.MX RT1170 in one of our project and I wanted to know about the SPI availability on i.MX RT1170 as we are going to use SPI for Camera interface. We wanted to connect two SPI Camera interface.&amp;nbsp;&lt;/P&gt;&lt;P&gt;So, Please let me know that it is possible to connect two SPI camera module to &lt;LI-PRODUCT title="iMXRT1170" id="iMXRT1170"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;or not.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Also I am interested to know that how many maximum camera I can connect to&amp;nbsp; &lt;LI-PRODUCT title="iMXRT1170" id="iMXRT1170"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;over SPI.&lt;BR /&gt;&lt;BR /&gt;Thank you.&lt;/P&gt;</description>
      <pubDate>Wed, 18 Oct 2023 11:29:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SPI-availability-on-i-MX-rt1170/m-p/1742070#M27255</guid>
      <dc:creator>Nishantt</dc:creator>
      <dc:date>2023-10-18T11:29:53Z</dc:date>
    </item>
    <item>
      <title>Re: SPI availability on i.MX rt1170</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SPI-availability-on-i-MX-rt1170/m-p/1742317#M27263</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/224536"&gt;@Nishantt&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The i.MXRT1170 has 6 SPI interfaces available, if your application only requires 2 cameras you will not have any issue regarding the compatibility.&lt;/P&gt;
&lt;BLOCKQUOTE&gt;
&lt;P&gt;&lt;SPAN&gt;Also I am interested to know that how many maximum camera I can connect to&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&lt;A id="hoverCardLink_1" class="lia-link-navigation lia-product-hover-card-link lia-product-mention lia-tooltip-trigger" href="https://community.nxp.com/t5/c-pwmxy87654/iMXRT1170/pd-p/iMXRT1170" aria-describedby="hoverCardLink_2-tooltip-element" aria-controls="hoverCardLink_2-tooltip-element" target="_blank"&gt;iMXRT1170&lt;/A&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;over SPI.&lt;/SPAN&gt;&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P&gt;It's complicated to calculate exactly how many can be supported, each SPI interfaces can be configured to have more than one ChipSelect pin and the iMXRT1170 has 2 FlexIO interfaces which can simulate SPI communication.&lt;/P&gt;
&lt;P&gt;Is there a particular amount of cameras you would like to use?&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards, Miguel.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 18 Oct 2023 18:35:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SPI-availability-on-i-MX-rt1170/m-p/1742317#M27263</guid>
      <dc:creator>Miguel04</dc:creator>
      <dc:date>2023-10-18T18:35:01Z</dc:date>
    </item>
    <item>
      <title>Re: SPI availability on i.MX rt1170</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SPI-availability-on-i-MX-rt1170/m-p/1742589#M27265</link>
      <description>&lt;P&gt;Hello Miguel,&lt;BR /&gt;&lt;BR /&gt;Thank you for reply.&lt;BR /&gt;&lt;BR /&gt;I wanted to know that can we connect Dual SPI Mode to i.MXRT1170 normal SPI pins?&lt;BR /&gt;&lt;BR /&gt;Our Camera has below SPI pinouts, so we require the Dual SPI Mode interface.&lt;BR /&gt;&lt;BR /&gt;1. CLK&lt;BR /&gt;2. D0 (MOSI)&lt;BR /&gt;3. D1 (MISO)&lt;BR /&gt;4. CS&lt;BR /&gt;&lt;BR /&gt;Thank You.&lt;/P&gt;</description>
      <pubDate>Thu, 19 Oct 2023 05:48:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SPI-availability-on-i-MX-rt1170/m-p/1742589#M27265</guid>
      <dc:creator>Nishantt</dc:creator>
      <dc:date>2023-10-19T05:48:29Z</dc:date>
    </item>
    <item>
      <title>Re: SPI availability on i.MX rt1170</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SPI-availability-on-i-MX-rt1170/m-p/1743149#M27270</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/224536"&gt;@Nishantt&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;What do you mean with&amp;nbsp;&lt;SPAN&gt;&lt;STRONG&gt;&lt;EM&gt;Dual SPI Mode&lt;/EM&gt;&lt;/STRONG&gt;, are you refering to a half duplex or full duplex communication?&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;The iMXRT1170's LPSPI module feature both modes according to the reference manual Chapter&amp;nbsp;&lt;EM&gt;&lt;STRONG&gt;70.2.2 Features&lt;/STRONG&gt;&lt;/EM&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;However, the examples on the SDK, uses different pins for Serial Data Input and Serial Data Output.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Miguel04_0-1697740991278.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/245995iB6515A8D5D3EB2A5/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Miguel04_0-1697740991278.png" alt="Miguel04_0-1697740991278.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Best Regards, Miguel.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 19 Oct 2023 18:43:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SPI-availability-on-i-MX-rt1170/m-p/1743149#M27270</guid>
      <dc:creator>Miguel04</dc:creator>
      <dc:date>2023-10-19T18:43:18Z</dc:date>
    </item>
    <item>
      <title>Re: SPI availability on i.MX rt1170</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SPI-availability-on-i-MX-rt1170/m-p/1743634#M27280</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hello Miguel,&lt;BR /&gt;&lt;BR /&gt;&lt;/SPAN&gt;We are going to use Half Duplex in Dual SPI mode.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;How many Dual SPI mode does &lt;LI-PRODUCT title="iMXRT1170" id="iMXRT1170"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;supports?&amp;nbsp;&lt;BR /&gt;As we are planning to connect maximum 4 dual SPI based cameras to &lt;LI-PRODUCT title="iMXRT1170" id="iMXRT1170"&gt;&lt;/LI-PRODUCT&gt;.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;I also wanted to know that can we use Cascading in Dual SPI Mode? So, it will reduce the total SPI requirements.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Let me know if you required any other information.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Thank You.&lt;/P&gt;</description>
      <pubDate>Fri, 20 Oct 2023 10:37:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SPI-availability-on-i-MX-rt1170/m-p/1743634#M27280</guid>
      <dc:creator>Nishantt</dc:creator>
      <dc:date>2023-10-20T10:37:51Z</dc:date>
    </item>
    <item>
      <title>Re: SPI availability on i.MX rt1170</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SPI-availability-on-i-MX-rt1170/m-p/1744779#M27299</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/224536"&gt;@Nishantt&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Sorry for the inconvenience, I'm not understanding your question, is there a possibility for you to share with me a connection diagram and which camera you are using?&lt;/P&gt;
&lt;P&gt;You said your pins are&lt;/P&gt;
&lt;P&gt;CLK, MOSI, MISO, CLK. These connections are for normal SPI.&lt;/P&gt;
&lt;P&gt;I've found this post that could possibly help you.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-RT/imxrt1052-dual-spi/m-p/1656412" target="_self"&gt;Dual SPI&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Also, the iMXRT1170, supports MIPI CSI (Camera Serial Inteface) which can help you with the connection of the cameras.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards, Miguel.&lt;/P&gt;</description>
      <pubDate>Mon, 23 Oct 2023 21:16:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SPI-availability-on-i-MX-rt1170/m-p/1744779#M27299</guid>
      <dc:creator>Miguel04</dc:creator>
      <dc:date>2023-10-23T21:16:39Z</dc:date>
    </item>
    <item>
      <title>Re: SPI availability on i.MX rt1170</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SPI-availability-on-i-MX-rt1170/m-p/1745613#M27313</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/206759"&gt;@Miguel04&lt;/a&gt;,&lt;BR /&gt;&lt;BR /&gt;&lt;/SPAN&gt;Sure, No problem. Please find below more detailed explanation to understand my question.&lt;BR /&gt;&lt;BR /&gt;We are planning to use GC032A VGA CMOS Image Sensor based camera module.&amp;nbsp;&lt;BR /&gt;This are the pins in Camera module:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Nishantt_0-1698210379515.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/246646i543660B1FE7F8B18/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Nishantt_0-1698210379515.png" alt="Nishantt_0-1698210379515.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I understand the MISO MOSI are used in simple SPI mode, but as per my knowledge MISO and MOSI will work as a D0 and D1 data lines for Dual SPI Mode. For make it more clear please find below Image about Dual SPI mode for your reference.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Nishantt_1-1698211095984.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/246647iFF2D01C3E531BDF4/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Nishantt_1-1698211095984.png" alt="Nishantt_1-1698211095984.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Thank You.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 25 Oct 2023 05:19:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SPI-availability-on-i-MX-rt1170/m-p/1745613#M27313</guid>
      <dc:creator>Nishantt</dc:creator>
      <dc:date>2023-10-25T05:19:08Z</dc:date>
    </item>
    <item>
      <title>Re: SPI availability on i.MX rt1170</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SPI-availability-on-i-MX-rt1170/m-p/1749795#M27371</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/224536"&gt;@Nishantt&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thank you for the information, it was very usefull.&lt;/P&gt;
&lt;P&gt;According to the documentation it should be possible to use the LPSPI as half duplex in dual spi mode, to find reference and information regarding this, look into the reference manual. chapters:&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;70.4 Signal descriptions&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;70.2.2 Features &lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;However we do not provide any examples for this application, I apolize for the inconvenience.&lt;/P&gt;
&lt;P&gt;Best Regards, Miguel.&lt;/P&gt;</description>
      <pubDate>Tue, 31 Oct 2023 21:05:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SPI-availability-on-i-MX-rt1170/m-p/1749795#M27371</guid>
      <dc:creator>Miguel04</dc:creator>
      <dc:date>2023-10-31T21:05:24Z</dc:date>
    </item>
  </channel>
</rss>