<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUs中的主题 Re: USB host example code for mimxrt1170-evk not working as expected.</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/USB-host-example-code-for-mimxrt1170-evk-not-working-as-expected/m-p/1733453#M27075</link>
    <description>&lt;P&gt;I found the solution for the post you are referring.&lt;BR /&gt;Yes this post is about the same code but different issue. I only need your support for this particular post&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/186731"&gt;@EdwinHz&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;More specifically the problem I have is, according to the documentation given, a software should installed automatically after running the code. But when I am running the code, the expected software does not get installed. Thats problem now I am dealing with. &lt;LI-PRODUCT title="iMXRT1170" id="iMXRT1170"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 04 Oct 2023 04:07:06 GMT</pubDate>
    <dc:creator>Shehan_Janidu</dc:creator>
    <dc:date>2023-10-04T04:07:06Z</dc:date>
    <item>
      <title>USB host example code for mimxrt1170-evk not working as expected.</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/USB-host-example-code-for-mimxrt1170-evk-not-working-as-expected/m-p/1732923#M27061</link>
      <description>&lt;P&gt;I loaded the example code given to connect USB virtual printer. The code compiles properly giving no errors. But when the code is loaded, the expected functionality doesn't take place. The overview of the full example project and expected functionality is explained in the attached pdf.&amp;nbsp;&lt;/P&gt;&lt;P&gt;The example project name is "dev_printer_virtual_text_bm_cm7"&lt;/P&gt;&lt;P&gt;The project can be accessed through following link&amp;nbsp;&amp;nbsp;&lt;A href="https://arescomp-my.sharepoint.com/:u:/p/janidu/EX94sLHrE5VCsLj9NBMcwZYBIrTs4FtcoyYd1e-LcXlDwQ?e=XkrntJ" target="_self"&gt;Link to project&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;LI-PRODUCT title="iMXRT1170" id="iMXRT1170"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 03 Oct 2023 07:20:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/USB-host-example-code-for-mimxrt1170-evk-not-working-as-expected/m-p/1732923#M27061</guid>
      <dc:creator>Shehan_Janidu</dc:creator>
      <dc:date>2023-10-03T07:20:45Z</dc:date>
    </item>
    <item>
      <title>Re: USB host example code for mimxrt1170-evk not working as expected.</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/USB-host-example-code-for-mimxrt1170-evk-not-working-as-expected/m-p/1733409#M27069</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/222472"&gt;@Shehan_Janidu&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I believe this is a duplicated post from the following link:&amp;nbsp;&lt;A href="https://community.nxp.com/t5/i-MX-RT/USB-host-example-code-for-mimxrt1170-evk-not-working-properly/td-p/1732431" target="_blank"&gt;https://community.nxp.com/t5/i-MX-RT/USB-host-example-code-for-mimxrt1170-evk-not-working-properly/td-p/1732431&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;If it is ok with you, I will continue supporting on that other post in order to prevent double efforts.&lt;/P&gt;
&lt;P&gt;BR,&lt;BR /&gt;Edwin.&lt;/P&gt;</description>
      <pubDate>Tue, 03 Oct 2023 22:55:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/USB-host-example-code-for-mimxrt1170-evk-not-working-as-expected/m-p/1733409#M27069</guid>
      <dc:creator>EdwinHz</dc:creator>
      <dc:date>2023-10-03T22:55:39Z</dc:date>
    </item>
    <item>
      <title>Re: USB host example code for mimxrt1170-evk not working as expected.</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/USB-host-example-code-for-mimxrt1170-evk-not-working-as-expected/m-p/1733453#M27075</link>
      <description>&lt;P&gt;I found the solution for the post you are referring.&lt;BR /&gt;Yes this post is about the same code but different issue. I only need your support for this particular post&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/186731"&gt;@EdwinHz&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;More specifically the problem I have is, according to the documentation given, a software should installed automatically after running the code. But when I am running the code, the expected software does not get installed. Thats problem now I am dealing with. &lt;LI-PRODUCT title="iMXRT1170" id="iMXRT1170"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 04 Oct 2023 04:07:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/USB-host-example-code-for-mimxrt1170-evk-not-working-as-expected/m-p/1733453#M27075</guid>
      <dc:creator>Shehan_Janidu</dc:creator>
      <dc:date>2023-10-04T04:07:06Z</dc:date>
    </item>
    <item>
      <title>Re: USB host example code for mimxrt1170-evk not working as expected.</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/USB-host-example-code-for-mimxrt1170-evk-not-working-as-expected/m-p/1734448#M27120</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/222472"&gt;@Shehan_Janidu&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;You should be able to install the driver manually by following this community post:&amp;nbsp;&lt;A href="https://community.nxp.com/t5/Kinetis-Microcontrollers/quot-MCU-VIRTUAL-COM-DEMO-quot-and-demo-app-for-USB-KW24D512-can/m-p/625448" target="_blank"&gt;https://community.nxp.com/t5/Kinetis-Microcontrollers/quot-MCU-VIRTUAL-COM-DEMO-quot-and-demo-app-for-USB-KW24D512-can/m-p/625448&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Rather than using the path specified by that post, however, you would use the following:&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;"&amp;lt;SDK installation root&amp;gt;\SDK_2_14_0_MIMXRT1170-EVKB.zip\middleware\usb"&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;By default, the SDK installation root is:&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;"C:\Users\&amp;lt;user&amp;gt;\mcuxpresso\02\SDKPackages"&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I hope this helps,&lt;BR /&gt;Edwin,&lt;/P&gt;</description>
      <pubDate>Thu, 05 Oct 2023 21:04:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/USB-host-example-code-for-mimxrt1170-evk-not-working-as-expected/m-p/1734448#M27120</guid>
      <dc:creator>EdwinHz</dc:creator>
      <dc:date>2023-10-05T21:04:36Z</dc:date>
    </item>
    <item>
      <title>Re: USB host example code for mimxrt1170-evk not working as expected.</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/USB-host-example-code-for-mimxrt1170-evk-not-working-as-expected/m-p/1735687#M27147</link>
      <description>&lt;P&gt;I ran the code again and followed following steps,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; in device manager following icons were displayed,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="usb 1.png" style="width: 872px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/244078i0CF6F5B28F15E91E/image-size/large?v=v2&amp;amp;px=999" role="button" title="usb 1.png" alt="usb 1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;After that I updated the drivers both ways, manually and by clicking on "let me pick"&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="usb 2.png" style="width: 756px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/244080i82723167776FF0FA/image-size/large?v=v2&amp;amp;px=999" role="button" title="usb 2.png" alt="usb 2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;But even after doing that, still generic printer is not shown in the printer section,&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="usb 3.png" style="width: 827px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/244084iB49E9CD4721BAEFB/image-size/large?v=v2&amp;amp;px=999" role="button" title="usb 3.png" alt="usb 3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;And when I go to devices and printers folder, it shows like this,&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="usb 4.png" style="width: 751px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/244086iCD698875321845E6/image-size/large?v=v2&amp;amp;px=999" role="button" title="usb 4.png" alt="usb 4.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Can u suggest what can I do to fix this issue. In addition I have a doubt to clear out. The printing process that we going to do here is fully virtual one instead of physical one. Am I right ?&lt;/P&gt;&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/186731"&gt;@EdwinHz&lt;/a&gt;&amp;nbsp; &lt;LI-PRODUCT title="iMXRT1170" id="iMXRT1170"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 09 Oct 2023 09:35:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/USB-host-example-code-for-mimxrt1170-evk-not-working-as-expected/m-p/1735687#M27147</guid>
      <dc:creator>Shehan_Janidu</dc:creator>
      <dc:date>2023-10-09T09:35:02Z</dc:date>
    </item>
  </channel>
</rss>