<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUsのトピックRe: RT1170 Custom Board SDRAM Memory Order</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1170-Custom-Board-SDRAM-Memory-Order/m-p/1731962#M27033</link>
    <description>&lt;P&gt;Well, it seems to be about the DCD table. To be able to move the external RAM to the second place in the memory configurations for generated variables and buffers to reside, a DCD table is required. Without a DCD table, our board crashes. We've tried it with the SLN-TLHMI Kit, when we created a custom project without DCD, we were not able to move the external ram into the second position after flash, but with the DCD table taken from the example project. We were able to move the external ram right after flash.&amp;nbsp;&lt;/P&gt;&lt;P&gt;So We need to create a DCD table for our custom board, what is the best way to do it? Any advice on this matter? Thank you in advance!&lt;/P&gt;</description>
    <pubDate>Fri, 29 Sep 2023 12:30:37 GMT</pubDate>
    <dc:creator>Wobaffet</dc:creator>
    <dc:date>2023-09-29T12:30:37Z</dc:date>
    <item>
      <title>RT1170 Custom Board SDRAM Memory Order</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1170-Custom-Board-SDRAM-Memory-Order/m-p/1728592#M26958</link>
      <description>&lt;P&gt;We have a problem with our custom board, when we move the BOARD_SDRAM section right after flash, board crashes. We have to do full chip erase in order to program again. But in the below configuration everything seems to working fine. The test code for the sdram from the sdk works but when we move sdram upto the second place nothing works. Also the reason we are trying to move the external ram section into the second place is to configure a frame buffer. Do you have any idea what causes this problem?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Wobaffet_0-1695624000197.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/242422i8E7317A7C60BB662/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Wobaffet_0-1695624000197.png" alt="Wobaffet_0-1695624000197.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Wobaffet_0-1695624000197.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;</description>
      <pubDate>Mon, 25 Sep 2023 06:41:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1170-Custom-Board-SDRAM-Memory-Order/m-p/1728592#M26958</guid>
      <dc:creator>Wobaffet</dc:creator>
      <dc:date>2023-09-25T06:41:14Z</dc:date>
    </item>
    <item>
      <title>Re: RT1170 Custom Board SDRAM Memory Order</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1170-Custom-Board-SDRAM-Memory-Order/m-p/1729647#M26987</link>
      <description>&lt;P&gt;reminder.&lt;/P&gt;</description>
      <pubDate>Tue, 26 Sep 2023 10:35:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1170-Custom-Board-SDRAM-Memory-Order/m-p/1729647#M26987</guid>
      <dc:creator>Wobaffet</dc:creator>
      <dc:date>2023-09-26T10:35:56Z</dc:date>
    </item>
    <item>
      <title>Re: RT1170 Custom Board SDRAM Memory Order</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1170-Custom-Board-SDRAM-Memory-Order/m-p/1731134#M27018</link>
      <description>&lt;P&gt;reminder.&lt;/P&gt;</description>
      <pubDate>Thu, 28 Sep 2023 08:19:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1170-Custom-Board-SDRAM-Memory-Order/m-p/1731134#M27018</guid>
      <dc:creator>Wobaffet</dc:creator>
      <dc:date>2023-09-28T08:19:20Z</dc:date>
    </item>
    <item>
      <title>Re: RT1170 Custom Board SDRAM Memory Order</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1170-Custom-Board-SDRAM-Memory-Order/m-p/1731962#M27033</link>
      <description>&lt;P&gt;Well, it seems to be about the DCD table. To be able to move the external RAM to the second place in the memory configurations for generated variables and buffers to reside, a DCD table is required. Without a DCD table, our board crashes. We've tried it with the SLN-TLHMI Kit, when we created a custom project without DCD, we were not able to move the external ram into the second position after flash, but with the DCD table taken from the example project. We were able to move the external ram right after flash.&amp;nbsp;&lt;/P&gt;&lt;P&gt;So We need to create a DCD table for our custom board, what is the best way to do it? Any advice on this matter? Thank you in advance!&lt;/P&gt;</description>
      <pubDate>Fri, 29 Sep 2023 12:30:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1170-Custom-Board-SDRAM-Memory-Order/m-p/1731962#M27033</guid>
      <dc:creator>Wobaffet</dc:creator>
      <dc:date>2023-09-29T12:30:37Z</dc:date>
    </item>
    <item>
      <title>Re: RT1170 Custom Board SDRAM Memory Order</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1170-Custom-Board-SDRAM-Memory-Order/m-p/1734002#M27104</link>
      <description>&lt;P&gt;Hello&lt;BR /&gt;I hope you are well.&lt;/P&gt;
&lt;P&gt;Since SDRAM is moved to the second place, all data placed on the alias "RAM(SRAM)" will now be placed on SDRAM. It is needed that the SDRAM is initialized by the time this is relocated, this is done through the DCD.&lt;BR /&gt;You can create your DCD on config tools referencing the register values from semc example or if SDRAM&amp;nbsp; is similar to the one on the EVK you can use the DCD from Secure Provisioning Tool.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Omar_Anguiano_0-1696465895600.png" style="width: 465px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/243653i1FB9212CBD9CE76C/image-dimensions/465x41?v=v2" width="465" height="41" role="button" title="Omar_Anguiano_0-1696465895600.png" alt="Omar_Anguiano_0-1696465895600.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Omar_Anguiano_0-1696465895600.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 05 Oct 2023 00:31:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1170-Custom-Board-SDRAM-Memory-Order/m-p/1734002#M27104</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2023-10-05T00:31:57Z</dc:date>
    </item>
  </channel>
</rss>