<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: RT1061 does not boot when code size on flash memory is exceed 256k in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1061-does-not-boot-when-code-size-on-flash-memory-is-exceed/m-p/1712576#M26598</link>
    <description>&lt;P&gt;Hello, my name is Pavel, and I will be supporting your case, I reviewed your information and I have these questions.&lt;/P&gt;
&lt;P&gt;&lt;FONT&gt;Are you using the EVK? If yes, the boot mode should be at internal boot.&lt;BR /&gt;How do you determine what is not going well? Could you share the LOG?&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT&gt;What is the number of the memory?&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&lt;FONT&gt;Best regards,&lt;BR /&gt;Pavel&lt;/FONT&gt;&lt;/P&gt;</description>
    <pubDate>Mon, 28 Aug 2023 18:31:33 GMT</pubDate>
    <dc:creator>Pavel_Hernandez</dc:creator>
    <dc:date>2023-08-28T18:31:33Z</dc:date>
    <item>
      <title>RT1061 does not boot when code size on flash memory is exceed 256k</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1061-does-not-boot-when-code-size-on-flash-memory-is-exceed/m-p/1712314#M26594</link>
      <description>&lt;P&gt;Hi, I am using MIMXRT1061DVL6B with 8MB flash memory from winbond.&lt;/P&gt;&lt;P&gt;the problem is once the code size on flash is exceed 256kbyte.&lt;/P&gt;&lt;P&gt;RT1061 is not properly booted.&lt;/P&gt;&lt;P&gt;is there any possible reason and solution for it?&lt;/P&gt;&lt;P&gt;I am using this device for consumer electronics.&lt;/P&gt;&lt;P&gt;thank you&lt;/P&gt;</description>
      <pubDate>Mon, 28 Aug 2023 11:20:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1061-does-not-boot-when-code-size-on-flash-memory-is-exceed/m-p/1712314#M26594</guid>
      <dc:creator>Mithy</dc:creator>
      <dc:date>2023-08-28T11:20:43Z</dc:date>
    </item>
    <item>
      <title>Re: RT1061 does not boot when code size on flash memory is exceed 256k</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1061-does-not-boot-when-code-size-on-flash-memory-is-exceed/m-p/1712576#M26598</link>
      <description>&lt;P&gt;Hello, my name is Pavel, and I will be supporting your case, I reviewed your information and I have these questions.&lt;/P&gt;
&lt;P&gt;&lt;FONT&gt;Are you using the EVK? If yes, the boot mode should be at internal boot.&lt;BR /&gt;How do you determine what is not going well? Could you share the LOG?&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT&gt;What is the number of the memory?&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&lt;FONT&gt;Best regards,&lt;BR /&gt;Pavel&lt;/FONT&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 28 Aug 2023 18:31:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1061-does-not-boot-when-code-size-on-flash-memory-is-exceed/m-p/1712576#M26598</guid>
      <dc:creator>Pavel_Hernandez</dc:creator>
      <dc:date>2023-08-28T18:31:33Z</dc:date>
    </item>
  </channel>
</rss>