<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUsのトピックDoes RT1060 support IAP function</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Does-RT1060-support-IAP-function/m-p/1710600#M26561</link>
    <description>&lt;P&gt;May I ask how I.MX rt1060 supports IAP functionality? Is there an official demo available for reference?&lt;BR /&gt;Previously used ST's F4 and F7 series (Cortex m4/m7), ST has an official website that provides examples of upgrading IAP applications. The basic operation is to reset the APP's stack start address in flash in the bootloader code,&lt;BR /&gt;__ Set_ MSP (* (uint32_t *) APP_ FLASH_ ADDRESS;&lt;BR /&gt;Then, a jump command can successfully jump to the upgraded APP program.&lt;BR /&gt;(pFunction) (* (uint32_t *) (USER-FLASH_ADDRESS+4)) ();&lt;BR /&gt;Now that we are using RT1060 as a product, we also need to upgrade to IAP. Is there an example code (command for Cortex-m7) provided that allows us to use this code to jump to different sectors for execution?&lt;BR /&gt;Or does the official provide bootloader for the rt1060 series for guidance? Can this directly add some upgrade code to the bootloader to achieve IAP functionality? Thank you very much.&lt;/P&gt;</description>
    <pubDate>Thu, 24 Aug 2023 10:01:15 GMT</pubDate>
    <dc:creator>lw3</dc:creator>
    <dc:date>2023-08-24T10:01:15Z</dc:date>
    <item>
      <title>Does RT1060 support IAP function</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Does-RT1060-support-IAP-function/m-p/1710600#M26561</link>
      <description>&lt;P&gt;May I ask how I.MX rt1060 supports IAP functionality? Is there an official demo available for reference?&lt;BR /&gt;Previously used ST's F4 and F7 series (Cortex m4/m7), ST has an official website that provides examples of upgrading IAP applications. The basic operation is to reset the APP's stack start address in flash in the bootloader code,&lt;BR /&gt;__ Set_ MSP (* (uint32_t *) APP_ FLASH_ ADDRESS;&lt;BR /&gt;Then, a jump command can successfully jump to the upgraded APP program.&lt;BR /&gt;(pFunction) (* (uint32_t *) (USER-FLASH_ADDRESS+4)) ();&lt;BR /&gt;Now that we are using RT1060 as a product, we also need to upgrade to IAP. Is there an example code (command for Cortex-m7) provided that allows us to use this code to jump to different sectors for execution?&lt;BR /&gt;Or does the official provide bootloader for the rt1060 series for guidance? Can this directly add some upgrade code to the bootloader to achieve IAP functionality? Thank you very much.&lt;/P&gt;</description>
      <pubDate>Thu, 24 Aug 2023 10:01:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Does-RT1060-support-IAP-function/m-p/1710600#M26561</guid>
      <dc:creator>lw3</dc:creator>
      <dc:date>2023-08-24T10:01:15Z</dc:date>
    </item>
    <item>
      <title>Re: Does RT1060 support IAP function</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Does-RT1060-support-IAP-function/m-p/1711620#M26582</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/221760"&gt;@lw3&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Yes the RT1060 support IAP, you can find information of the APIs on the reference manual chapter 9.13. Also, on the SDK you can find the example&amp;nbsp;&lt;EM&gt;&lt;STRONG&gt;evkbmimxrt1060_flexspi_nor_edma_transfer&lt;/STRONG&gt;&lt;/EM&gt;, this example writes on the flash of the EVK. It is important to consider the configuration of the memory changes.&lt;/P&gt;
&lt;P&gt;Best Regards, Miguel.&lt;/P&gt;</description>
      <pubDate>Fri, 25 Aug 2023 19:34:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Does-RT1060-support-IAP-function/m-p/1711620#M26582</guid>
      <dc:creator>Miguel04</dc:creator>
      <dc:date>2023-08-25T19:34:45Z</dc:date>
    </item>
  </channel>
</rss>