<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: RT1050 UUID in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1050-UUID/m-p/1706104#M26429</link>
    <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/59276"&gt;@Kan_Li&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;Thank you, I've seen this ticket, it talks about the Unique ID instead of Universally Unique ID. You provided the 8-byte (reg0x410 and reg0x420) data is not the UUID either. Correct me if I'm wrong.&lt;/P&gt;</description>
    <pubDate>Thu, 17 Aug 2023 00:43:17 GMT</pubDate>
    <dc:creator>ffloree</dc:creator>
    <dc:date>2023-08-17T00:43:17Z</dc:date>
    <item>
      <title>RT1050 UUID</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1050-UUID/m-p/1705440#M26401</link>
      <description>&lt;P&gt;Does RT1050 have UUID (instead of UID)? if it does, which registers I can get it from?&lt;/P&gt;&lt;P&gt;I know RT685 has it, see the &lt;SPAN&gt;UM11147 Section 4.5.5.52, but I didn't find it in RT1050 reference manual, it just mentions a 8-byte UID which can be read from OCOTP-&amp;gt;CFG0 and OCOTP-&amp;gt;CFG1, but I don't think it's the standard 16-byte UUID following&amp;nbsp;rfc4122&amp;nbsp;&lt;A title="rfc4122" href="https://www.rfc-editor.org/rfc/rfc4122" target="_self"&gt;https://www.rfc-editor.org/rfc/rfc4122&lt;/A&gt;&amp;nbsp;.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 16 Aug 2023 06:26:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1050-UUID/m-p/1705440#M26401</guid>
      <dc:creator>ffloree</dc:creator>
      <dc:date>2023-08-16T06:26:31Z</dc:date>
    </item>
    <item>
      <title>Re: RT1050 UUID</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1050-UUID/m-p/1705531#M26408</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/114055"&gt;@ffloree&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Yes, there is a thread on similar topic, and you may refer to&amp;nbsp;&lt;A href="https://community.nxp.com/t5/i-MX-RT/Read-UID-Unique-ID-on-i-MXRT-RT1050/m-p/1202637" target="_blank"&gt;https://community.nxp.com/t5/i-MX-RT/Read-UID-Unique-ID-on-i-MXRT-RT1050/m-p/1202637&lt;/A&gt;&amp;nbsp;for details.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You may refer to chapter 22 in the RM for more details.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Kan_Li_0-1692172115020.png" style="width: 530px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/236644i72EA64C3F4D93CEB/image-dimensions/530x204?v=v2" width="530" height="204" role="button" title="Kan_Li_0-1692172115020.png" alt="Kan_Li_0-1692172115020.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Kan_Li_0-1692172115020.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope that helps,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Wed, 16 Aug 2023 07:49:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1050-UUID/m-p/1705531#M26408</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2023-08-16T07:49:55Z</dc:date>
    </item>
    <item>
      <title>Re: RT1050 UUID</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1050-UUID/m-p/1706104#M26429</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/59276"&gt;@Kan_Li&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;Thank you, I've seen this ticket, it talks about the Unique ID instead of Universally Unique ID. You provided the 8-byte (reg0x410 and reg0x420) data is not the UUID either. Correct me if I'm wrong.&lt;/P&gt;</description>
      <pubDate>Thu, 17 Aug 2023 00:43:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1050-UUID/m-p/1706104#M26429</guid>
      <dc:creator>ffloree</dc:creator>
      <dc:date>2023-08-17T00:43:17Z</dc:date>
    </item>
    <item>
      <title>回复： RT1050 UUID</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1050-UUID/m-p/1707301#M26477</link>
      <description>&lt;P&gt;UUID is from the fuse 0x410 and 0x420. We can use the shadow registers to get its value.For RT1050, you can use the following code to get the UUID.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;UUID_L = *(uint32_t *)0x401f4410;&lt;/P&gt;
&lt;P&gt;UUID_H = *(uint32_t *)0x401f4420;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 18 Aug 2023 06:49:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1050-UUID/m-p/1707301#M26477</guid>
      <dc:creator>lucas_cao</dc:creator>
      <dc:date>2023-08-18T06:49:44Z</dc:date>
    </item>
  </channel>
</rss>