<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUsのトピックRe: RT1052 eDMA transfer on GPIO edge trigger</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1052-eDMA-transfer-on-GPIO-edge-trigger/m-p/1695368#M26112</link>
    <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I don't know the answer to the speeds (without doing additional measurements) but I have a couple of videos as reference:&lt;BR /&gt;&lt;BR /&gt;Using GPIO to trigger DMA via XBAR: &lt;A href="https://www.youtube.com/watch?v=zNWIG-O7ZW0&amp;amp;list=PLWKlVb_MqDQEOCnsNOJO8gd3jDCwiyKKe&amp;amp;index=6" target="_blank"&gt;https://www.youtube.com/watch?v=zNWIG-O7ZW0&amp;amp;list=PLWKlVb_MqDQEOCnsNOJO8gd3jDCwiyKKe&amp;amp;index=6&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;Using high speed ports: &lt;A href="https://www.youtube.com/watch?v=nLInUIboLR0&amp;amp;list=PLWKlVb_MqDQEOCnsNOJO8gd3jDCwiyKKe&amp;amp;index=14" target="_blank"&gt;https://www.youtube.com/watch?v=nLInUIboLR0&amp;amp;list=PLWKlVb_MqDQEOCnsNOJO8gd3jDCwiyKKe&amp;amp;index=14&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;Since the 1052 doesn't have high speed ports there may be some limitations (due to the GPIO not being closely coupled) and you may like to look at using a 1062 instead. The 1062 is compatible but has better features and more memory at modest price increase.&lt;BR /&gt;&lt;BR /&gt;For stocks of 1062 available see here: &lt;A href="https://www.utasker.com/Shop/semi.html" target="_blank"&gt;https://www.utasker.com/Shop/semi.html&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;Regards&lt;BR /&gt;&lt;BR /&gt;Mark&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
    <pubDate>Sun, 30 Jul 2023 14:47:13 GMT</pubDate>
    <dc:creator>mjbcswitzerland</dc:creator>
    <dc:date>2023-07-30T14:47:13Z</dc:date>
    <item>
      <title>RT1052 eDMA transfer on GPIO edge trigger</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1052-eDMA-transfer-on-GPIO-edge-trigger/m-p/1694582#M26086</link>
      <description>&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt;In my application, I need to trigger eDMA to transfer data from GPIO to memory (DTCM) via a clock signal.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt; Currently, the clock signal is input from a PIN, connected via xBAR to the eDMA channel request, while the data is input from GPIO in parallel, with a data width of 32 bits.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt; Are there parameters to indicate what the transfer rate can be reached?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt; According to my current tests, the maximum input frequency can only reach 8 MHz, which means the maximum transmission rate is 32 MB/s.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt; Is this correct?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 28 Jul 2023 02:33:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1052-eDMA-transfer-on-GPIO-edge-trigger/m-p/1694582#M26086</guid>
      <dc:creator>HuangJun</dc:creator>
      <dc:date>2023-07-28T02:33:33Z</dc:date>
    </item>
    <item>
      <title>Re: RT1052 eDMA transfer on GPIO edge trigger</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1052-eDMA-transfer-on-GPIO-edge-trigger/m-p/1695368#M26112</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I don't know the answer to the speeds (without doing additional measurements) but I have a couple of videos as reference:&lt;BR /&gt;&lt;BR /&gt;Using GPIO to trigger DMA via XBAR: &lt;A href="https://www.youtube.com/watch?v=zNWIG-O7ZW0&amp;amp;list=PLWKlVb_MqDQEOCnsNOJO8gd3jDCwiyKKe&amp;amp;index=6" target="_blank"&gt;https://www.youtube.com/watch?v=zNWIG-O7ZW0&amp;amp;list=PLWKlVb_MqDQEOCnsNOJO8gd3jDCwiyKKe&amp;amp;index=6&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;Using high speed ports: &lt;A href="https://www.youtube.com/watch?v=nLInUIboLR0&amp;amp;list=PLWKlVb_MqDQEOCnsNOJO8gd3jDCwiyKKe&amp;amp;index=14" target="_blank"&gt;https://www.youtube.com/watch?v=nLInUIboLR0&amp;amp;list=PLWKlVb_MqDQEOCnsNOJO8gd3jDCwiyKKe&amp;amp;index=14&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;Since the 1052 doesn't have high speed ports there may be some limitations (due to the GPIO not being closely coupled) and you may like to look at using a 1062 instead. The 1062 is compatible but has better features and more memory at modest price increase.&lt;BR /&gt;&lt;BR /&gt;For stocks of 1062 available see here: &lt;A href="https://www.utasker.com/Shop/semi.html" target="_blank"&gt;https://www.utasker.com/Shop/semi.html&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;Regards&lt;BR /&gt;&lt;BR /&gt;Mark&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Sun, 30 Jul 2023 14:47:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1052-eDMA-transfer-on-GPIO-edge-trigger/m-p/1695368#M26112</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2023-07-30T14:47:13Z</dc:date>
    </item>
  </channel>
</rss>