<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Flex CAN Self Test / Loop back mode in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Flex-CAN-Self-Test-Loop-back-mode/m-p/1683480#M25865</link>
    <description>&lt;P&gt;The error detection is related to the methods described in 66.3.14 from the RM.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
    <pubDate>Thu, 06 Jul 2023 23:23:11 GMT</pubDate>
    <dc:creator>Omar_Anguiano</dc:creator>
    <dc:date>2023-07-06T23:23:11Z</dc:date>
    <item>
      <title>Flex CAN Self Test / Loop back mode</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Flex-CAN-Self-Test-Loop-back-mode/m-p/1676720#M25677</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am trying to implement the self test mechanism for Flex CAN on RT1176 , for which I am using the internal loopback mode for implementing the self test of the Flex CAN module. However I would love to know if any failure causes can be detected for the same as the reference module does not give much of the details on the same.&lt;/P&gt;&lt;P&gt;I meant that if the Loop back fails to receive the message it transmitted, any mechanism on detecting the same.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in Advance&lt;/P&gt;&lt;P&gt;Basavanagouda&lt;/P&gt;</description>
      <pubDate>Tue, 27 Jun 2023 07:03:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Flex-CAN-Self-Test-Loop-back-mode/m-p/1676720#M25677</guid>
      <dc:creator>basu_gouda</dc:creator>
      <dc:date>2023-06-27T07:03:39Z</dc:date>
    </item>
    <item>
      <title>Re: Flex CAN Self Test / Loop back mode</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Flex-CAN-Self-Test-Loop-back-mode/m-p/1682383#M25842</link>
      <description>&lt;P&gt;Hello&lt;BR /&gt;I hope you are well.&lt;/P&gt;
&lt;P&gt;Yes, in loopback mode errors can be detected.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
      <pubDate>Wed, 05 Jul 2023 21:27:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Flex-CAN-Self-Test-Loop-back-mode/m-p/1682383#M25842</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2023-07-05T21:27:09Z</dc:date>
    </item>
    <item>
      <title>Re: Flex CAN Self Test / Loop back mode</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Flex-CAN-Self-Test-Loop-back-mode/m-p/1682676#M25848</link>
      <description>&lt;P&gt;Hi Omar,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for your response,&lt;/P&gt;&lt;P&gt;Can you please elaborate on the same, will it be associated with the rx error mode signal or need to monitor any other source.&lt;/P&gt;&lt;P&gt;The reference manual does not give the clear answer.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;&lt;P&gt;Basavanagouda Ganganagoudar&lt;/P&gt;</description>
      <pubDate>Thu, 06 Jul 2023 03:29:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Flex-CAN-Self-Test-Loop-back-mode/m-p/1682676#M25848</guid>
      <dc:creator>basu_gouda</dc:creator>
      <dc:date>2023-07-06T03:29:41Z</dc:date>
    </item>
    <item>
      <title>Re: Flex CAN Self Test / Loop back mode</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Flex-CAN-Self-Test-Loop-back-mode/m-p/1683480#M25865</link>
      <description>&lt;P&gt;The error detection is related to the methods described in 66.3.14 from the RM.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
      <pubDate>Thu, 06 Jul 2023 23:23:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Flex-CAN-Self-Test-Loop-back-mode/m-p/1683480#M25865</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2023-07-06T23:23:11Z</dc:date>
    </item>
  </channel>
</rss>