<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUsのトピックIMXRT1176 Multicore RTOS task stuck issue</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT1176-Multicore-RTOS-task-stuck-issue/m-p/1682093#M25834</link>
    <description>&lt;P&gt;Hi NXP Team &amp;amp; Other Experts,&lt;/P&gt;&lt;P&gt;We are working on #IMXRT1176 MCU board for development of our custom AR HUD&lt;/P&gt;&lt;P&gt;SDK version : v2.10.0&lt;BR /&gt;MCUXpresso IDE version : v11.4.1&lt;/P&gt;&lt;P&gt;We are using Multicore (M4 and M7 core) for our functionality and are communicating via IPC using RPMSG.&lt;BR /&gt;Here the CAN RTOS task is running in M4 core and UI display graphics(LVGL rendering) RTOS Task is running in M7 core.&lt;/P&gt;&lt;P&gt;But during firmware upgrade using CAN UDS, it blocks the LVGL UI rendering task on M7 and got stuck, but CAN task is running fine on M4 slave side.&lt;BR /&gt;The data transfer during CAN upgrade is around 2KB chunks with 5MB of firmware .s19 bin file and storing the binary on flash memory.&lt;BR /&gt;The CAN baud rate is 500kb/s.&lt;BR /&gt;The upgrade progress information is passed from M4 to M7 using RPMSG.&lt;/P&gt;&lt;P&gt;During this process , we observing M4 RPMSG is not sending any data to M7 and M7 is also stuck. so UI is not refreshing on progress.&lt;BR /&gt;Need support in possible causes for this behaviour.&lt;/P&gt;&lt;P&gt;1) Unable to understand why M7 is stuck and what is the common HW elements between M4 and M7 that can cause this issue.?&lt;BR /&gt;2) Is CAN interrupt (ISR) on M4 can block the LVGL task on M7 side during bulk CAN data transfer?&lt;BR /&gt;3) Is RPMSG shared memory get corrupted/overloaded during bulk CAN data transfer?&lt;/P&gt;&lt;P&gt;we tried upgrade to latest CAN and RPMSG from latest NXP SDK 2.13 but this issue still persists.&lt;/P&gt;&lt;P&gt;Please suggest how to handle other RTOS task on M7 side even if CAN is running too fast in M4 salve.&lt;BR /&gt;It should not block UI LVGL task functionality in M7 core.&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Prashanth&lt;/P&gt;</description>
    <pubDate>Wed, 05 Jul 2023 14:44:57 GMT</pubDate>
    <dc:creator>prashanthkk</dc:creator>
    <dc:date>2023-07-05T14:44:57Z</dc:date>
    <item>
      <title>IMXRT1176 Multicore RTOS task stuck issue</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT1176-Multicore-RTOS-task-stuck-issue/m-p/1682093#M25834</link>
      <description>&lt;P&gt;Hi NXP Team &amp;amp; Other Experts,&lt;/P&gt;&lt;P&gt;We are working on #IMXRT1176 MCU board for development of our custom AR HUD&lt;/P&gt;&lt;P&gt;SDK version : v2.10.0&lt;BR /&gt;MCUXpresso IDE version : v11.4.1&lt;/P&gt;&lt;P&gt;We are using Multicore (M4 and M7 core) for our functionality and are communicating via IPC using RPMSG.&lt;BR /&gt;Here the CAN RTOS task is running in M4 core and UI display graphics(LVGL rendering) RTOS Task is running in M7 core.&lt;/P&gt;&lt;P&gt;But during firmware upgrade using CAN UDS, it blocks the LVGL UI rendering task on M7 and got stuck, but CAN task is running fine on M4 slave side.&lt;BR /&gt;The data transfer during CAN upgrade is around 2KB chunks with 5MB of firmware .s19 bin file and storing the binary on flash memory.&lt;BR /&gt;The CAN baud rate is 500kb/s.&lt;BR /&gt;The upgrade progress information is passed from M4 to M7 using RPMSG.&lt;/P&gt;&lt;P&gt;During this process , we observing M4 RPMSG is not sending any data to M7 and M7 is also stuck. so UI is not refreshing on progress.&lt;BR /&gt;Need support in possible causes for this behaviour.&lt;/P&gt;&lt;P&gt;1) Unable to understand why M7 is stuck and what is the common HW elements between M4 and M7 that can cause this issue.?&lt;BR /&gt;2) Is CAN interrupt (ISR) on M4 can block the LVGL task on M7 side during bulk CAN data transfer?&lt;BR /&gt;3) Is RPMSG shared memory get corrupted/overloaded during bulk CAN data transfer?&lt;/P&gt;&lt;P&gt;we tried upgrade to latest CAN and RPMSG from latest NXP SDK 2.13 but this issue still persists.&lt;/P&gt;&lt;P&gt;Please suggest how to handle other RTOS task on M7 side even if CAN is running too fast in M4 salve.&lt;BR /&gt;It should not block UI LVGL task functionality in M7 core.&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Prashanth&lt;/P&gt;</description>
      <pubDate>Wed, 05 Jul 2023 14:44:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT1176-Multicore-RTOS-task-stuck-issue/m-p/1682093#M25834</guid>
      <dc:creator>prashanthkk</dc:creator>
      <dc:date>2023-07-05T14:44:57Z</dc:date>
    </item>
    <item>
      <title>Re: IMXRT1176 Multicore RTOS task stuck issue</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT1176-Multicore-RTOS-task-stuck-issue/m-p/1688053#M25956</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Sorry for the later reply.&lt;/P&gt;
&lt;P&gt;I check this issue is same with our online support case:&amp;nbsp;&lt;SPAN&gt;00549226.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Please check and update this issue at case: 00549226.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Thank you for the understanding.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Mike&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 14 Jul 2023 02:50:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT1176-Multicore-RTOS-task-stuck-issue/m-p/1688053#M25956</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2023-07-14T02:50:45Z</dc:date>
    </item>
  </channel>
</rss>