<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: RT1176 SAI1/2/3 for 8 channel  per SAI TDM audio transfer in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1176-SAI1-2-3-for-8-channel-per-SAI-TDM-audio-transfer/m-p/1667185#M25454</link>
    <description>&lt;P&gt;No, as SAI1 is the only interface capable of supporting 8 channels. By connecting each device to a single data line you are limiting the device to only have 2 channels per device.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
    <pubDate>Sat, 10 Jun 2023 00:22:33 GMT</pubDate>
    <dc:creator>Omar_Anguiano</dc:creator>
    <dc:date>2023-06-10T00:22:33Z</dc:date>
    <item>
      <title>RT1176 SAI1/2/3 for 8 channel  per SAI TDM audio transfer</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1176-SAI1-2-3-for-8-channel-per-SAI-TDM-audio-transfer/m-p/1663614#M25369</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Could you please help with understanding the limitations of SAI1/2/3 interfaces on RT1176 mcu?&lt;/P&gt;&lt;P&gt;In the Reference Manual I see the following:&lt;/P&gt;&lt;P&gt;&lt;EM&gt;"SAI-1 is used for multi-channel audio interface, which supports up to 8-channels audio&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;input or 8-channels audio output at 384 kHz/32-bit. SAI-2, SAI-3 and SAI-4 can be used&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;for stereo audio input and output up to 384 kHz/32-bit. Also SAI-3 is able to drive MQS&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;directly as a low-cost audio output."&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;Does that mean that I can't attach 8 channel TDM audio DAC to each SAI1 SAI2 and SAI3 to get 24 audio channel output?&lt;/P&gt;&lt;P&gt;I checked all the remaining Ref Manual and got no any signs that only SAI1 can work in TDM mode sending 8 channels of 24 or 32 bit samples&amp;nbsp; per frame.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;And another question please - is there any additional documentation with detailed interrupts description?&lt;/P&gt;&lt;P&gt;For my application I need an interrupt that happens every sample sent through SAI1. It seems that WSIE will do just what I need, but it will be great to have more info.&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
      <pubDate>Mon, 05 Jun 2023 16:00:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1176-SAI1-2-3-for-8-channel-per-SAI-TDM-audio-transfer/m-p/1663614#M25369</guid>
      <dc:creator>SergD</dc:creator>
      <dc:date>2023-06-05T16:00:52Z</dc:date>
    </item>
    <item>
      <title>Re: RT1176 SAI1/2/3 for 8 channel  per SAI TDM audio transfer</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1176-SAI1-2-3-for-8-channel-per-SAI-TDM-audio-transfer/m-p/1664605#M25388</link>
      <description>&lt;P&gt;Hello&lt;BR /&gt;I hope you are well.&lt;/P&gt;
&lt;P&gt;Your understanding is correct, SAI2/3/4 are limited to 2 channels so a source of 8 channels is not possible; only on SAI1.&lt;BR /&gt;This app note might be helpful: &lt;A href="https://www.nxp.com/docs/en/application-note/AN12090.pdf" target="_blank"&gt;Using Multi-Channel Feature of SAI (nxp.com)&lt;/A&gt;&lt;BR /&gt;Unfortunately, there is no additional documentation, the reference manual contains the SAI information.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
      <pubDate>Tue, 06 Jun 2023 20:43:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1176-SAI1-2-3-for-8-channel-per-SAI-TDM-audio-transfer/m-p/1664605#M25388</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2023-06-06T20:43:11Z</dc:date>
    </item>
    <item>
      <title>Re: RT1176 SAI1/2/3 for 8 channel  per SAI TDM audio transfer</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1176-SAI1-2-3-for-8-channel-per-SAI-TDM-audio-transfer/m-p/1666384#M25426</link>
      <description>&lt;P&gt;Thank you!&lt;/P&gt;&lt;P&gt;Reading the RM I see the following&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;EM&gt;SAI-1 is used for multi-channel audio interface, which supports up to 8-channels audio&lt;/EM&gt;&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;&lt;EM&gt;input or 8-channels audio output at 384 kHz/32-bit.&lt;/EM&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;But later in the document I see more detailed info:&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;• Transmitter with independent bit clock and frame sync supporting 4 data lines&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;• Receiver with independent bit clock and frame sync supporting 4 data lines&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;• Each data line can support a maximum frame size of 32 words&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;• 8- to 32-bit word size&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;• Word size configured separately for the first word and remaining words in a frame&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;• Asynchronous 32 x 32-bit FIFO for each transmit and receive data line supporting&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;So it looks like I can send &lt;STRONG&gt;eight&lt;/STRONG&gt; 32 bit words per frame on each data line.&lt;/P&gt;&lt;P&gt;So the question is - could you please confirm that I can attach three 8-channel DACs (to be precise - Texas Instruments PCM1690 DAC&amp;nbsp; &lt;A href="https://www.ti.com/lit/ds/symlink/pcm1690.pdf" target="_blank" rel="noopener"&gt;https://www.ti.com/lit/ds/symlink/pcm1690.pdf&lt;/A&gt; ) - each to a single data line ?&lt;EM&gt;&lt;STRONG&gt;&lt;BR /&gt;&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;</description>
      <pubDate>Thu, 08 Jun 2023 20:08:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1176-SAI1-2-3-for-8-channel-per-SAI-TDM-audio-transfer/m-p/1666384#M25426</guid>
      <dc:creator>SergD</dc:creator>
      <dc:date>2023-06-08T20:08:54Z</dc:date>
    </item>
    <item>
      <title>Re: RT1176 SAI1/2/3 for 8 channel  per SAI TDM audio transfer</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1176-SAI1-2-3-for-8-channel-per-SAI-TDM-audio-transfer/m-p/1667185#M25454</link>
      <description>&lt;P&gt;No, as SAI1 is the only interface capable of supporting 8 channels. By connecting each device to a single data line you are limiting the device to only have 2 channels per device.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
      <pubDate>Sat, 10 Jun 2023 00:22:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1176-SAI1-2-3-for-8-channel-per-SAI-TDM-audio-transfer/m-p/1667185#M25454</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2023-06-10T00:22:33Z</dc:date>
    </item>
    <item>
      <title>Re: RT1176 SAI1/2/3 for 8 channel  per SAI TDM audio transfer</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1176-SAI1-2-3-for-8-channel-per-SAI-TDM-audio-transfer/m-p/1667229#M25457</link>
      <description>&lt;P&gt;could you please comment on this topic then - &lt;A href="https://community.nxp.com/t5/i-MX-RT/How-many-TDM-channels-can-be-supported-in-RT1170-SAI1-TX-amp-RX/m-p/1628587#M24455" target="_blank"&gt;https://community.nxp.com/t5/i-MX-RT/How-many-TDM-channels-can-be-supported-in-RT1170-SAI1-TX-amp-RX/m-p/1628587#M24455&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sat, 10 Jun 2023 09:41:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1176-SAI1-2-3-for-8-channel-per-SAI-TDM-audio-transfer/m-p/1667229#M25457</guid>
      <dc:creator>SergD</dc:creator>
      <dc:date>2023-06-10T09:41:10Z</dc:date>
    </item>
  </channel>
</rss>