<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Could not connect to target in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Could-not-connect-to-target/m-p/1666686#M25439</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have a custom Board (inspired by the demoboard).&lt;/P&gt;&lt;P&gt;That's right, I use a Jlink with a 6-pin adapter (like this&amp;nbsp;&lt;A href="https://www.segger.com/products/debug-probes/j-link/accessories/adapters/6-pin-needle-adapter/" target="_blank"&gt;https://www.segger.com/products/debug-probes/j-link/accessories/adapters/6-pin-needle-adapter/&lt;/A&gt;).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I then respected the pinout on my board (except for the SWO, which arrives on the ground because I don't use it).&lt;/P&gt;&lt;P&gt;I checked (and compared with the demoboard) the SWDIO, SWDCLK and RST signals on the oscilloscope.&lt;BR /&gt;They're consistent. Obviously, the end is not the same, since there's a problem with my board.&lt;/P&gt;&lt;P&gt;Do you have an idea ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Best regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Corentin&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 09 Jun 2023 06:43:39 GMT</pubDate>
    <dc:creator>corentinalleard</dc:creator>
    <dc:date>2023-06-09T06:43:39Z</dc:date>
    <item>
      <title>Could not connect to target</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Could-not-connect-to-target/m-p/1665137#M25401</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have an error when&amp;nbsp; I want to debug an &lt;SPAN&gt;MIMXRT1052CVJ5B.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I debug in SWD with a Jlink&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;this error :&lt;/P&gt;&lt;P&gt;ERROR: Could not connect to target.&lt;BR /&gt;SEGGER J-Link GDB Server V7.54b Command Line Version&lt;BR /&gt;JLinkARM.dll V7.54b (DLL compiled Sep 14 2021 16:07:10)&lt;BR /&gt;Command line: -nosilent -swoport 2332 -select USB=609302740 -jlinkscriptfile C:\Users\corentin.alleart\Documents\MCUXpressoIDE_11.4.1_6260\workspace\.mcuxpressoide_packages_support\MIMXRT1052xxxxB_support/Script/evkbimxrt1050_sdram_init.jlinkscript -telnetport 2333 -singlerun -endian little -noir -speed auto -port 2331 -vd -device MCIMXRT1052 -if SWD -halt -reportuseraction&lt;BR /&gt;-----GDB Server start settings-----&lt;BR /&gt;GDBInit file: none&lt;BR /&gt;GDB Server Listening port: 2331&lt;BR /&gt;SWO raw output listening port: 2332&lt;BR /&gt;Terminal I/O port: 2333&lt;BR /&gt;Accept remote connection: localhost only&lt;BR /&gt;Generate logfile: off&lt;BR /&gt;Verify download: on&lt;BR /&gt;Init regs on start: off&lt;BR /&gt;Silent mode: off&lt;BR /&gt;Single run mode: on&lt;BR /&gt;Target connection timeout: 0 ms&lt;BR /&gt;------J-Link related settings------&lt;BR /&gt;J-Link Host interface: USB&lt;BR /&gt;J-Link script: C:\Users\corentin.alleart\Documents\MCUXpressoIDE_11.4.1_6260\workspace\.mcuxpressoide_packages_support\MIMXRT1052xxxxB_support/Script/evkbimxrt1050_sdram_init.jlinkscript&lt;BR /&gt;J-Link settings file: none&lt;BR /&gt;------Target related settings------&lt;BR /&gt;Target device: MCIMXRT1052&lt;BR /&gt;Target interface: SWD&lt;BR /&gt;Target interface speed: auto&lt;BR /&gt;Target endian: little&lt;BR /&gt;Connecting to J-Link...&lt;BR /&gt;J-Link is connected.&lt;BR /&gt;Device "MIMXRT1052XXXXA" selected.&lt;BR /&gt;Firmware: J-Link V9 compiled May 7 2021 16:26:12&lt;BR /&gt;Hardware: V9.30&lt;BR /&gt;S/N: 609302740&lt;BR /&gt;Feature(s): RDI, FlashBP, FlashDL, JFlash, GDB&lt;BR /&gt;Checking target voltage...&lt;BR /&gt;Target voltage: 3.33 V&lt;BR /&gt;Listening on TCP/IP port 2331&lt;BR /&gt;Connecting to target...&lt;BR /&gt;ConfigTargetSettings() start&lt;BR /&gt;Config JTAG Speed to 4000kHz&lt;BR /&gt;ConfigTargetSettings() end&lt;BR /&gt;ConfigTargetSettings() start&lt;BR /&gt;Config JTAG Speed to 4000kHz&lt;BR /&gt;ConfigTargetSettings() end&lt;BR /&gt;ConfigTargetSettings() start&lt;BR /&gt;Config JTAG Speed to 4000kHz&lt;BR /&gt;ConfigTargetSettings() end&lt;BR /&gt;ConfigTargetSettings() start&lt;BR /&gt;Config JTAG Speed to 4000kHz&lt;BR /&gt;ConfigTargetSettings() end&lt;BR /&gt;ERROR: Could not connect to target.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-------------------&lt;/P&gt;&lt;P&gt;and then a second error occured :&amp;nbsp;&lt;/P&gt;&lt;P&gt;"Error in final launch sequence&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Failed to execute MI command&amp;nbsp;&lt;/P&gt;&lt;P&gt;-target-select remote localhost:2331&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Connextion timed out&lt;/P&gt;&lt;P&gt;"&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for your help&lt;/P&gt;</description>
      <pubDate>Wed, 07 Jun 2023 11:57:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Could-not-connect-to-target/m-p/1665137#M25401</guid>
      <dc:creator>corentinalleard</dc:creator>
      <dc:date>2023-06-07T11:57:21Z</dc:date>
    </item>
    <item>
      <title>Re: Could not connect to target</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Could-not-connect-to-target/m-p/1665409#M25406</link>
      <description>&lt;P&gt;Hello, my name is Pavel, and I will be supporting your case, let me get into your case and when I have more information, I will contact you.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Pavel&lt;/P&gt;</description>
      <pubDate>Wed, 07 Jun 2023 18:50:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Could-not-connect-to-target/m-p/1665409#M25406</guid>
      <dc:creator>Pavel_Hernandez</dc:creator>
      <dc:date>2023-06-07T18:50:23Z</dc:date>
    </item>
    <item>
      <title>Re: Could not connect to target</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Could-not-connect-to-target/m-p/1666614#M25433</link>
      <description>&lt;P&gt;Hello, I reviewed your information, and the common error is that the user is using the wrong port, in this case, you just need to use the J2, by default the communication interface is SWD if you want to use a JTAG you need to do a rework.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Pavel_Hernandez_0-1686282407478.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/226946i26366E574DC2F6DB/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Pavel_Hernandez_0-1686282407478.png" alt="Pavel_Hernandez_0-1686282407478.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;I will suppose you are using SWD, in this case, you are using a J-Link I support you do not have any problem connecting this.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Pavel_Hernandez_1-1686282671206.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/226947i487A2E72597C6B55/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Pavel_Hernandez_1-1686282671206.png" alt="Pavel_Hernandez_1-1686282671206.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;With this you will not have any issue. Do you have a custom board?&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Pavel&lt;/P&gt;</description>
      <pubDate>Fri, 09 Jun 2023 04:11:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Could-not-connect-to-target/m-p/1666614#M25433</guid>
      <dc:creator>Pavel_Hernandez</dc:creator>
      <dc:date>2023-06-09T04:11:55Z</dc:date>
    </item>
    <item>
      <title>Re: Could not connect to target</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Could-not-connect-to-target/m-p/1666686#M25439</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have a custom Board (inspired by the demoboard).&lt;/P&gt;&lt;P&gt;That's right, I use a Jlink with a 6-pin adapter (like this&amp;nbsp;&lt;A href="https://www.segger.com/products/debug-probes/j-link/accessories/adapters/6-pin-needle-adapter/" target="_blank"&gt;https://www.segger.com/products/debug-probes/j-link/accessories/adapters/6-pin-needle-adapter/&lt;/A&gt;).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I then respected the pinout on my board (except for the SWO, which arrives on the ground because I don't use it).&lt;/P&gt;&lt;P&gt;I checked (and compared with the demoboard) the SWDIO, SWDCLK and RST signals on the oscilloscope.&lt;BR /&gt;They're consistent. Obviously, the end is not the same, since there's a problem with my board.&lt;/P&gt;&lt;P&gt;Do you have an idea ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Best regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Corentin&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 09 Jun 2023 06:43:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Could-not-connect-to-target/m-p/1666686#M25439</guid>
      <dc:creator>corentinalleard</dc:creator>
      <dc:date>2023-06-09T06:43:39Z</dc:date>
    </item>
    <item>
      <title>Re: Could not connect to target</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Could-not-connect-to-target/m-p/1667130#M25450</link>
      <description>&lt;P&gt;Hello, I reviewed again your log in some cases the problem is the number of MCU, I don't know if your code is from an example, maybe could you check if the MCU number coincides with the MCU shown in the config tool.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Pavel_Hernandez_0-1686338877045.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/227051i547F6CB5F547F390/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Pavel_Hernandez_0-1686338877045.png" alt="Pavel_Hernandez_0-1686338877045.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;If the MCU is the same, let me know these questions,&lt;/P&gt;
&lt;P&gt;Can you flash your board in the past?&amp;nbsp;&lt;BR /&gt;Did you follow the recommendation of the Hardware Development Guide?&amp;nbsp;&lt;BR /&gt;Do you have an external flash memory?&lt;BR /&gt;Could you tell me about your configuration of boo mode and boot cfg?&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Pavel&lt;/P&gt;</description>
      <pubDate>Fri, 09 Jun 2023 19:35:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Could-not-connect-to-target/m-p/1667130#M25450</guid>
      <dc:creator>Pavel_Hernandez</dc:creator>
      <dc:date>2023-06-09T19:35:38Z</dc:date>
    </item>
    <item>
      <title>Re: Could not connect to target</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Could-not-connect-to-target/m-p/1672502#M25579</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The MCU is the same.&lt;/P&gt;&lt;P&gt;I've never managed to flash my card, but I can flash the demoboard.&lt;/P&gt;&lt;P&gt;I followed the recommendations in the guide.&lt;/P&gt;&lt;P&gt;Yes, I have an external flash.&lt;/P&gt;&lt;P&gt;I am booting in internal boot.&lt;/P&gt;&lt;P&gt;Attached is my schematic. We added a pull down on JTAG_MOD ( GPIO1_IO08)&lt;/P&gt;&lt;P&gt;We notice a problem during flashing, the SWDIO quiescent voltage is high and SWDIO starts talking in 3V3 then goes to 1V7.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 20 Jun 2023 07:55:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Could-not-connect-to-target/m-p/1672502#M25579</guid>
      <dc:creator>corentinalleard</dc:creator>
      <dc:date>2023-06-20T07:55:52Z</dc:date>
    </item>
    <item>
      <title>Re: Could not connect to target</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Could-not-connect-to-target/m-p/1674042#M25613</link>
      <description>&lt;P&gt;Hello, I recommend opening an internal case, to check the schematic, tagging my name in the new case.&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;Pavel&lt;/P&gt;</description>
      <pubDate>Wed, 21 Jun 2023 21:34:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Could-not-connect-to-target/m-p/1674042#M25613</guid>
      <dc:creator>Pavel_Hernandez</dc:creator>
      <dc:date>2023-06-21T21:34:06Z</dc:date>
    </item>
  </channel>
</rss>