<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic How to configure RTS_B initial state of i.MX RT1064? in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/How-to-configure-RTS-B-initial-state-of-i-MX-RT1064/m-p/1665777#M25411</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I configured i.MX RT1064 pin B2 to RTS_B, I noted that I cannot configure initial state of at this function.&amp;nbsp; This pin can work in RS-485 application, but I found after the MCU reset the initial status of this pin is high.&amp;nbsp; I also noted when this pin output is low, after executed following code:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;LPUART_SoftwareReset(base);&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;This pin will output high and want the initial state is low.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;My question is can I set the initial state of this pin when it is configured as RTS_B.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Best Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Martin&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 08 Jun 2023 03:30:53 GMT</pubDate>
    <dc:creator>martinzhang</dc:creator>
    <dc:date>2023-06-08T03:30:53Z</dc:date>
    <item>
      <title>How to configure RTS_B initial state of i.MX RT1064?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/How-to-configure-RTS-B-initial-state-of-i-MX-RT1064/m-p/1665777#M25411</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I configured i.MX RT1064 pin B2 to RTS_B, I noted that I cannot configure initial state of at this function.&amp;nbsp; This pin can work in RS-485 application, but I found after the MCU reset the initial status of this pin is high.&amp;nbsp; I also noted when this pin output is low, after executed following code:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;LPUART_SoftwareReset(base);&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;This pin will output high and want the initial state is low.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;My question is can I set the initial state of this pin when it is configured as RTS_B.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Best Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Martin&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 08 Jun 2023 03:30:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/How-to-configure-RTS-B-initial-state-of-i-MX-RT1064/m-p/1665777#M25411</guid>
      <dc:creator>martinzhang</dc:creator>
      <dc:date>2023-06-08T03:30:53Z</dc:date>
    </item>
    <item>
      <title>Re: How to configure RTS_B initial state of i.MX RT1064?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/How-to-configure-RTS-B-initial-state-of-i-MX-RT1064/m-p/1667172#M25452</link>
      <description>&lt;P&gt;Hello&lt;BR /&gt;I hope you are well.&lt;/P&gt;
&lt;P&gt;To control the state of this pin you will need to do it by configuring it as GPIO, you might use DCD so the pin stays at the desired state during/after boot time.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
      <pubDate>Fri, 09 Jun 2023 22:52:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/How-to-configure-RTS-B-initial-state-of-i-MX-RT1064/m-p/1667172#M25452</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2023-06-09T22:52:59Z</dc:date>
    </item>
  </channel>
</rss>