<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: IMXRT 1024 RTC running faster than expected in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT-1024-RTC-running-faster-than-expected/m-p/1651435#M25061</link>
    <description>&lt;P class="lia-align-justify"&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/214093"&gt;@Punithintelli&lt;/a&gt;,&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;Could you please tell us if you are using an NXP EVK or a custom board? If is a custom board, could you please give us more information about your SNVS and RTC design?&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;Which MCUXpresso IDE and SDK version are you using? Have you made changes to the example? Is this behavior happening from the start of operation or after a certain time had passed? Also, how much timing difference are you getting?&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;Finally, in which boot mode are you testing the example? Could you please test it with QSPI Flash boot mode?&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;Best regards, Raul.&lt;/P&gt;</description>
    <pubDate>Tue, 16 May 2023 18:30:54 GMT</pubDate>
    <dc:creator>RaRo</dc:creator>
    <dc:date>2023-05-16T18:30:54Z</dc:date>
    <item>
      <title>IMXRT 1024 RTC running faster than expected</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT-1024-RTC-running-faster-than-expected/m-p/1651070#M25053</link>
      <description>&lt;P&gt;Hello All,&lt;/P&gt;&lt;P&gt;I am using IMXRT 1024 microcontroller and having a issue with RTC.&lt;/P&gt;&lt;P&gt;To begin with we are using SNVS_lp_srtc example program provided in SDK example. RTC time is running faster than the real time value. The result is same for both Internal RC oscillator and external crystal oscillator(32.768Khz).&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Punith P&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 16 May 2023 10:26:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT-1024-RTC-running-faster-than-expected/m-p/1651070#M25053</guid>
      <dc:creator>Punithintelli</dc:creator>
      <dc:date>2023-05-16T10:26:21Z</dc:date>
    </item>
    <item>
      <title>Re: IMXRT 1024 RTC running faster than expected</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT-1024-RTC-running-faster-than-expected/m-p/1651435#M25061</link>
      <description>&lt;P class="lia-align-justify"&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/214093"&gt;@Punithintelli&lt;/a&gt;,&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;Could you please tell us if you are using an NXP EVK or a custom board? If is a custom board, could you please give us more information about your SNVS and RTC design?&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;Which MCUXpresso IDE and SDK version are you using? Have you made changes to the example? Is this behavior happening from the start of operation or after a certain time had passed? Also, how much timing difference are you getting?&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;Finally, in which boot mode are you testing the example? Could you please test it with QSPI Flash boot mode?&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;Best regards, Raul.&lt;/P&gt;</description>
      <pubDate>Tue, 16 May 2023 18:30:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT-1024-RTC-running-faster-than-expected/m-p/1651435#M25061</guid>
      <dc:creator>RaRo</dc:creator>
      <dc:date>2023-05-16T18:30:54Z</dc:date>
    </item>
    <item>
      <title>Re: IMXRT 1024 RTC running faster than expected</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT-1024-RTC-running-faster-than-expected/m-p/1652015#M25077</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/206649"&gt;@RaRo&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We are using the custom board and I have attached the snapshot of the SNVS and RTC design.&lt;BR /&gt;MCUXpresso IDE Version - 11.7.1&lt;BR /&gt;1024 SDK version - 2.13.0&lt;BR /&gt;No code changes expect adding a additional printf statements for verification.&lt;BR /&gt;The behavior is observerd from the start.&lt;BR /&gt;When the code is configured to run using external crystal(32.768khz), for 1s real time we get 1.2sec in IMxRT1024.&lt;BR /&gt;When the code is configured to run using internal RC oscillator, for 1s real time we get 1.5sec in IMxRT1024.&lt;BR /&gt;We are running it in QSPI Flash boot mode.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="SNVS design.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/223596iD86074EC34141DD0/image-size/medium?v=v2&amp;amp;px=400" role="button" title="SNVS design.png" alt="SNVS design.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;SNVS design.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="RTC design.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/223597iFEFD9BE7FB0C8522/image-size/medium?v=v2&amp;amp;px=400" role="button" title="RTC design.png" alt="RTC design.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;RTC design.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;BR /&gt;Punith P&lt;/P&gt;</description>
      <pubDate>Wed, 17 May 2023 11:01:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT-1024-RTC-running-faster-than-expected/m-p/1652015#M25077</guid>
      <dc:creator>Punithintelli</dc:creator>
      <dc:date>2023-05-17T11:01:43Z</dc:date>
    </item>
    <item>
      <title>Re: IMXRT 1024 RTC running faster than expected</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT-1024-RTC-running-faster-than-expected/m-p/1653237#M25105</link>
      <description>&lt;P class="lia-align-justify"&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/214093"&gt;@Punithintelli&lt;/a&gt;,&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;Comparing your SNVS design to the &lt;A href="http://i.MX%20RT1024 | Crossover MCU with ARM Cortex-M7, 256 KB SRAM | NXP Semiconductors" target="_self"&gt;Hardware Development Guide for the MIMXRT1020 Processor&lt;/A&gt;, we found out that you are using an extra capacitor of 4.7uF(C40). Look at the following Power supply decoupling recommendations:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="RaulRomero_0-1684426318769.png" style="width: 443px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/223831i899ADA24DA6323B8/image-dimensions/443x310?v=v2" width="443" height="310" role="button" title="RaulRomero_0-1684426318769.png" alt="RaulRomero_0-1684426318769.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;RaulRomero_0-1684426318769.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;[MIMXRT1020HFUG. Chapter 3. Power supply. Table 2. Power supply decoupling recommendations]&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;Could you please remove the C40 capacitor of the VDD_SNVS_IN signal?&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;Let us know if this solves your problem.&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;Best regards, Raul.&lt;/P&gt;</description>
      <pubDate>Thu, 18 May 2023 16:19:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT-1024-RTC-running-faster-than-expected/m-p/1653237#M25105</guid>
      <dc:creator>RaRo</dc:creator>
      <dc:date>2023-05-18T16:19:20Z</dc:date>
    </item>
  </channel>
</rss>