<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Is there PWM_X Example Code? in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Is-there-PWM-X-Example-Code/m-p/1640120#M24807</link>
    <description>&lt;P&gt;I need to use the RT1176's PWM4 X,3 signal to control backlight intensity. Is there example code for setup of a PWM_X output? Something simple to get me started would be great. I'm using MCUXpresso and have enabled the PWM4 X,3 signal on GPIO_AD_21 configured as an output, but it doesn't look like the SDK 2.13.1 supports kPWM_PwmX as a signal channel for an output signal.&lt;/P&gt;&lt;P&gt;I did find &lt;A href="https://community.nxp.com/t5/i-MX-RT/Using-rt1050-flexpwm-X-output/m-p/854733" target="_self"&gt;this link&lt;/A&gt; where fsl_pwm.c was patched to provide PWM_X capability, but this hasn't worked for me either.&amp;nbsp;&amp;nbsp;I have also read &lt;A href="https://community.nxp.com/t5/Digital-Signal-Controllers/How-to-generate-duty-cycle-of-PWM-X-for-eFlexPWM-module/ta-p/1108875" target="_self"&gt;this article&lt;/A&gt; but I'm still struggling.&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;</description>
    <pubDate>Wed, 26 Apr 2023 02:40:41 GMT</pubDate>
    <dc:creator>mrd</dc:creator>
    <dc:date>2023-04-26T02:40:41Z</dc:date>
    <item>
      <title>Is there PWM_X Example Code?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Is-there-PWM-X-Example-Code/m-p/1640120#M24807</link>
      <description>&lt;P&gt;I need to use the RT1176's PWM4 X,3 signal to control backlight intensity. Is there example code for setup of a PWM_X output? Something simple to get me started would be great. I'm using MCUXpresso and have enabled the PWM4 X,3 signal on GPIO_AD_21 configured as an output, but it doesn't look like the SDK 2.13.1 supports kPWM_PwmX as a signal channel for an output signal.&lt;/P&gt;&lt;P&gt;I did find &lt;A href="https://community.nxp.com/t5/i-MX-RT/Using-rt1050-flexpwm-X-output/m-p/854733" target="_self"&gt;this link&lt;/A&gt; where fsl_pwm.c was patched to provide PWM_X capability, but this hasn't worked for me either.&amp;nbsp;&amp;nbsp;I have also read &lt;A href="https://community.nxp.com/t5/Digital-Signal-Controllers/How-to-generate-duty-cycle-of-PWM-X-for-eFlexPWM-module/ta-p/1108875" target="_self"&gt;this article&lt;/A&gt; but I'm still struggling.&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;</description>
      <pubDate>Wed, 26 Apr 2023 02:40:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Is-there-PWM-X-Example-Code/m-p/1640120#M24807</guid>
      <dc:creator>mrd</dc:creator>
      <dc:date>2023-04-26T02:40:41Z</dc:date>
    </item>
    <item>
      <title>Re: Is there PWM_X Example Code?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Is-there-PWM-X-Example-Code/m-p/1641161#M24827</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/182979"&gt;@mrd&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp; What's the board you are using? The MIMXRT1170-EVK from NXP?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;I think, we don't have the directly PWM_X example, but it is not difficult, you even can configure the register to realize it.&lt;/P&gt;
&lt;P&gt;&amp;nbsp; &amp;nbsp;Anyway, tell me your used board and IDE, then I will find time to help you to check it on my side.&lt;/P&gt;
&lt;P&gt;&amp;nbsp; &amp;nbsp;If you already write the related code, but can't work, just also upload it, I can help you to check it.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;kerry&lt;/P&gt;</description>
      <pubDate>Thu, 27 Apr 2023 04:06:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Is-there-PWM-X-Example-Code/m-p/1641161#M24827</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2023-04-27T04:06:20Z</dc:date>
    </item>
  </channel>
</rss>