<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: IMXRT1050-EVKB AVB sound card in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT1050-EVKB-AVB-sound-card/m-p/1637342#M24716</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/60336"&gt;@kerryzhou&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for your help&lt;/P&gt;&lt;P&gt;1. Yes the&amp;nbsp;&lt;SPAN&gt;MIMXRT1050-EVKB AVB demo works fine&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;2. I also tested the network successfully. I have an AVB sound card on the same switch and I can use it from the Mac&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;I have the following configuration on the AVB demo:&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;&lt;SPAN&gt;avb_app&lt;BR /&gt;&amp;nbsp; &amp;nbsp; mclock_role 1&lt;BR /&gt;avdecc&lt;BR /&gt;&amp;nbsp; &amp;nbsp; btb_mode 0&lt;BR /&gt;port0&lt;BR /&gt;&amp;nbsp; &amp;nbsp; gw_addr 192.168.0.1&lt;BR /&gt;&amp;nbsp; &amp;nbsp; hw_addr aa:bb:cc:dd:ee:ff&lt;BR /&gt;&amp;nbsp; &amp;nbsp; ip_addr 192.168.0.55&lt;BR /&gt;&amp;nbsp; &amp;nbsp; net_mask 255.255.255.0&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I think the problem is that the AVB demo from NXP is using AVDECC in Fast-connect mode (section 8.2.2.1.1 of the IEEE 1722.1-2013 standard) and not in&amp;nbsp;Controller-connect mode (section 8.2.2.1.3 of the IEEE 1722.1-2013 standard).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;This may explain why the device is not detected by the Mac on the network.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;What do you think ? Can it be the issue ? If so, how can we change this behavior by modifying the demo code ?&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 20 Apr 2023 14:56:02 GMT</pubDate>
    <dc:creator>sylvaing19</dc:creator>
    <dc:date>2023-04-20T14:56:02Z</dc:date>
    <item>
      <title>IMXRT1050-EVKB AVB sound card</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT1050-EVKB-AVB-sound-card/m-p/1633313#M24578</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am currently trying to build an AVB sound card using the&amp;nbsp;IMXRT1050-EVKB board with the&amp;nbsp;genavb-apps-freertos-4_3_0 stack and examples.&lt;/P&gt;&lt;P&gt;I successfully built the demo application "avb_audio_app" following the instructions in the document: NXP GenAVB/TSN MCUXpresso User's Guide (GAVBMCUXUG&amp;nbsp;Rev. 0, 01/2022)&lt;/P&gt;&lt;P&gt;The demo application is running on my evaluation board and I was able to configure the network settings (mac, ip, etc...) using the serial terminal, following the instructions in the document:&amp;nbsp;GenAVB/TSN Stack FreeRTOS Evaluation User's Guide (GAVBFREVALUG&amp;nbsp;Rev. 0, 01/2022)&lt;/P&gt;&lt;P&gt;I want to do the following connexion:&lt;/P&gt;&lt;P&gt;&lt;FONT face="courier new,courier"&gt;[Apple Mac mini M2] &amp;lt;---RJ45---&amp;gt; [AVB switch Netgear M4250] &amp;lt;---RJ45---&amp;gt; [IMXRT1050-EVKB] &amp;lt;---3.5mmJack---&amp;gt; [Speakers]&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;The eval board should be seen as an AVB sound card from the Mac mini, so that I can stream audio from the computer to the speakers. I don't need bidirectional stream, only from the computer to the board. Ideally the board should appear in the&amp;nbsp;&lt;SPAN&gt;Network Device Browser window (see below):&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="avb.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/219150i09A49007C815E3B8/image-size/large?v=v2&amp;amp;px=999" role="button" title="avb.png" alt="avb.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I was hoping that the "avb_audio_app" demo was capable of such thing. I was not able to get the eval board discovered on the network as an "AVB peripherial" by the computer, so my first question is:&lt;/P&gt;&lt;P&gt;Can the "avb_audio_app" be seen on the network as an AVB device ?&lt;/P&gt;&lt;P&gt;If so, what configuration is required to achieve this behavior ?&lt;/P&gt;&lt;P&gt;And if not, what would I need to change in the demo application to achieve this behavior ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you in advance for your help,&lt;/P&gt;&lt;P&gt;Sylvain&lt;/P&gt;</description>
      <pubDate>Thu, 13 Apr 2023 16:22:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT1050-EVKB-AVB-sound-card/m-p/1633313#M24578</guid>
      <dc:creator>sylvaing19</dc:creator>
      <dc:date>2023-04-13T16:22:21Z</dc:date>
    </item>
    <item>
      <title>Re: IMXRT1050-EVKB AVB sound card</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT1050-EVKB-AVB-sound-card/m-p/1635740#M24679</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/188926"&gt;@sylvaing19&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp; &amp;nbsp;Thanks so much for your interest in the NXP MIMXRT product.&lt;/P&gt;
&lt;P&gt;&amp;nbsp; &amp;nbsp;Just check the details at first:&lt;/P&gt;
&lt;P&gt;1. you follow the NXP doc, totally can make the MIMXRT1050-EVKB AVB works, right?&lt;/P&gt;
&lt;P&gt;2. Now, you want:&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Apple Mac mini M2] &amp;lt;---RJ45---&amp;gt; [AVB switch Netgear M4250] &amp;lt;---RJ45---&amp;gt; [IMXRT1050-EVKB] &amp;lt;---3.5mmJack---&amp;gt; [Speakers]&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;This still not success, then you want to make sure, whether it is supported by the PC with the network+AVB, right?&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;I will find time to test it on my side, and check it internally.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Best Regards,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Kerry&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 19 Apr 2023 02:09:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT1050-EVKB-AVB-sound-card/m-p/1635740#M24679</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2023-04-19T02:09:55Z</dc:date>
    </item>
    <item>
      <title>Re: IMXRT1050-EVKB AVB sound card</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT1050-EVKB-AVB-sound-card/m-p/1637342#M24716</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/60336"&gt;@kerryzhou&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for your help&lt;/P&gt;&lt;P&gt;1. Yes the&amp;nbsp;&lt;SPAN&gt;MIMXRT1050-EVKB AVB demo works fine&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;2. I also tested the network successfully. I have an AVB sound card on the same switch and I can use it from the Mac&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;I have the following configuration on the AVB demo:&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;&lt;SPAN&gt;avb_app&lt;BR /&gt;&amp;nbsp; &amp;nbsp; mclock_role 1&lt;BR /&gt;avdecc&lt;BR /&gt;&amp;nbsp; &amp;nbsp; btb_mode 0&lt;BR /&gt;port0&lt;BR /&gt;&amp;nbsp; &amp;nbsp; gw_addr 192.168.0.1&lt;BR /&gt;&amp;nbsp; &amp;nbsp; hw_addr aa:bb:cc:dd:ee:ff&lt;BR /&gt;&amp;nbsp; &amp;nbsp; ip_addr 192.168.0.55&lt;BR /&gt;&amp;nbsp; &amp;nbsp; net_mask 255.255.255.0&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I think the problem is that the AVB demo from NXP is using AVDECC in Fast-connect mode (section 8.2.2.1.1 of the IEEE 1722.1-2013 standard) and not in&amp;nbsp;Controller-connect mode (section 8.2.2.1.3 of the IEEE 1722.1-2013 standard).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;This may explain why the device is not detected by the Mac on the network.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;What do you think ? Can it be the issue ? If so, how can we change this behavior by modifying the demo code ?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 20 Apr 2023 14:56:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT1050-EVKB-AVB-sound-card/m-p/1637342#M24716</guid>
      <dc:creator>sylvaing19</dc:creator>
      <dc:date>2023-04-20T14:56:02Z</dc:date>
    </item>
    <item>
      <title>Re: IMXRT1050-EVKB AVB sound card</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT1050-EVKB-AVB-sound-card/m-p/1637813#M24733</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/188926"&gt;@sylvaing19&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp; &amp;nbsp;I also agree with you that the&amp;nbsp;&lt;SPAN&gt;&amp;nbsp;AVB demo may not match your Mac.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp;About the demo change, do you check the source code, you may need to find the&amp;nbsp;Controller-connect mode (section 8.2.2.1.3 of the IEEE 1722.1-2013 standard) code, and add it.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;BTW, please share me your used AVB related demo link, thanks.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Best Regards,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Kerry&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 21 Apr 2023 07:33:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT1050-EVKB-AVB-sound-card/m-p/1637813#M24733</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2023-04-21T07:33:12Z</dc:date>
    </item>
    <item>
      <title>Re: IMXRT1050-EVKB AVB sound card</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT1050-EVKB-AVB-sound-card/m-p/1637852#M24736</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;The code I am using can be downloaded from this page (at the bottom):&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/pages/wired-communications-middleware-for-nxp-microcontrollers:WIRED-COMM-MIDDLEWARE" target="_blank" rel="noopener"&gt;https://www.nxp.com/pages/wired-communications-middleware-for-nxp-microcontrollers:WIRED-COMM-MIDDLEWARE&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="sylvaing19_0-1682064169737.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/220261iB03E6E6603BE8D57/image-size/medium?v=v2&amp;amp;px=400" role="button" title="sylvaing19_0-1682064169737.png" alt="sylvaing19_0-1682064169737.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I followed the instructions in the included PDF files (in the directory "doc") to compile the example named "avb_audio_app" and flash it on my evaluation board IMXRT1050-EVKB.&lt;/P&gt;&lt;P&gt;Do you know where in the demo code I should look to modify the AVDECC behavior ?&lt;/P&gt;</description>
      <pubDate>Fri, 21 Apr 2023 08:44:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT1050-EVKB-AVB-sound-card/m-p/1637852#M24736</guid>
      <dc:creator>sylvaing19</dc:creator>
      <dc:date>2023-04-21T08:44:29Z</dc:date>
    </item>
  </channel>
</rss>