<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Is an external pulldown resistor necessary on the GP input with internal pulldown pin? in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Is-an-external-pulldown-resistor-necessary-on-the-GP-input-with/m-p/1636969#M24708</link>
    <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial, helvetica, sans-serif"&gt;&lt;SPAN&gt;GPIO_B0_04 is a 100kΩ pull-down input pin while MIMXRT1062 reset input POR_B = "L".&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial, helvetica, sans-serif"&gt;Furthermore, even after reset release, the default setting is an input pin with a 100kohm pulldown.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial, helvetica, sans-serif"&gt;Is an external pulldown resistor(e.g.10kohm) required to use the GPIO_B0_04 as an input pin with pulldown?&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif"&gt;&lt;SPAN&gt;Since the internal pulldown is not changed from the RESET state (pulldown 100Kohm), could this internal resistor be effective?&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 20 Apr 2023 07:19:11 GMT</pubDate>
    <dc:creator>Taka05</dc:creator>
    <dc:date>2023-04-20T07:19:11Z</dc:date>
    <item>
      <title>Is an external pulldown resistor necessary on the GP input with internal pulldown pin?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Is-an-external-pulldown-resistor-necessary-on-the-GP-input-with/m-p/1636969#M24708</link>
      <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial, helvetica, sans-serif"&gt;&lt;SPAN&gt;GPIO_B0_04 is a 100kΩ pull-down input pin while MIMXRT1062 reset input POR_B = "L".&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial, helvetica, sans-serif"&gt;Furthermore, even after reset release, the default setting is an input pin with a 100kohm pulldown.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial, helvetica, sans-serif"&gt;Is an external pulldown resistor(e.g.10kohm) required to use the GPIO_B0_04 as an input pin with pulldown?&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif"&gt;&lt;SPAN&gt;Since the internal pulldown is not changed from the RESET state (pulldown 100Kohm), could this internal resistor be effective?&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 20 Apr 2023 07:19:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Is-an-external-pulldown-resistor-necessary-on-the-GP-input-with/m-p/1636969#M24708</guid>
      <dc:creator>Taka05</dc:creator>
      <dc:date>2023-04-20T07:19:11Z</dc:date>
    </item>
    <item>
      <title>Re: Is an external pulldown resistor necessary on the GP input with internal pulldown pin?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Is-an-external-pulldown-resistor-necessary-on-the-GP-input-with/m-p/1637913#M24737</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/201127"&gt;@Taka05&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Please note, the&amp;nbsp;&lt;SPAN&gt;GPIO_B0_04 is the BOOT_CFG[0], so you can refer to the MIMXRT1060-EVK board&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="kerryzhou_0-1682067574785.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/220286i94FAE0156122F8C9/image-size/medium?v=v2&amp;amp;px=400" role="button" title="kerryzhou_0-1682067574785.png" alt="kerryzhou_0-1682067574785.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="kerryzhou_1-1682067581471.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/220287iD3BAF41817169B73/image-size/medium?v=v2&amp;amp;px=400" role="button" title="kerryzhou_1-1682067581471.png" alt="kerryzhou_1-1682067581471.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="kerryzhou_2-1682067589590.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/220288iC726463465A4CAD1/image-size/medium?v=v2&amp;amp;px=400" role="button" title="kerryzhou_2-1682067589590.png" alt="kerryzhou_2-1682067589590.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Wish it helps you!&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Kerry&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 21 Apr 2023 09:00:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Is-an-external-pulldown-resistor-necessary-on-the-GP-input-with/m-p/1637913#M24737</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2023-04-21T09:00:04Z</dc:date>
    </item>
  </channel>
</rss>