<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPADC1 Differential mode in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/LPADC1-Differential-mode/m-p/1629079#M24475</link>
    <description>&lt;P&gt;Ok, thank you very much for the support.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;Massimo&lt;/P&gt;</description>
    <pubDate>Thu, 06 Apr 2023 11:51:03 GMT</pubDate>
    <dc:creator>Max83</dc:creator>
    <dc:date>2023-04-06T11:51:03Z</dc:date>
    <item>
      <title>LPADC1 Differential mode</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/LPADC1-Differential-mode/m-p/1624108#M24336</link>
      <description>&lt;P&gt;Dear support,&lt;/P&gt;&lt;P&gt;I'm designing a custom board based on IMXRT1176 and I have to configure LPADC1 to take a differential reading through&amp;nbsp; pins GPIO_AD_06 (A,1_0) and GPIO_AD_07 (B, 1_0). I'm using the MCUXpresso Config Tool under the peripheral section to add a new command. The tool allow me to select Channel sample mode=Differential mode (A as plus, B as minus) and Channel number=A, 1_0 » [N13] GPIO_AD_06 and B, 1_0 » [T17] GPIO_AD_07. The problem is that I have a warning that say Signal channel 1B is not routed. On the Pin section of the tool the LPADC1 is already selected for the pins&amp;nbsp;GPIO_AD_06 and&amp;nbsp;GPIO_AD_07.&lt;/P&gt;&lt;P&gt;Why I have this warning? Am I doing something wrong? Herewith enclosed a screenshot of the tool.&lt;/P&gt;&lt;P&gt;Thank you in advance for the support.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;Max83&lt;/P&gt;</description>
      <pubDate>Wed, 29 Mar 2023 09:51:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/LPADC1-Differential-mode/m-p/1624108#M24336</guid>
      <dc:creator>Max83</dc:creator>
      <dc:date>2023-03-29T09:51:16Z</dc:date>
    </item>
    <item>
      <title>Re: LPADC1 Differential mode</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/LPADC1-Differential-mode/m-p/1624835#M24348</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/214947"&gt;@Max83&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;I tested both on MCUXpresso IDE and config tool. But I didn't see the warning. What's your tool version. I found the item name in Cahhenl number menu is different.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="jingpan_1-1680144950453.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/217008iF1F7FE68E5771E65/image-size/medium?v=v2&amp;amp;px=400" role="button" title="jingpan_1-1680144950453.png" alt="jingpan_1-1680144950453.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;jingpan_1-1680144950453.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Have you set ADC pins in pin config window like this?&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="jingpan_0-1680144928185.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/217007i6ADE627F02BCA75B/image-size/medium?v=v2&amp;amp;px=400" role="button" title="jingpan_0-1680144928185.png" alt="jingpan_0-1680144928185.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;jingpan_0-1680144928185.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Jing&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 30 Mar 2023 02:56:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/LPADC1-Differential-mode/m-p/1624835#M24348</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2023-03-30T02:56:45Z</dc:date>
    </item>
    <item>
      <title>Re: LPADC1 Differential mode</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/LPADC1-Differential-mode/m-p/1624981#M24355</link>
      <description>&lt;P&gt;Dear Jing,&lt;/P&gt;&lt;P&gt;thank you for your reply.&lt;/P&gt;&lt;P&gt;I'm using MCUXpresso Config Tools Pins version 13 and Peripheral Version 12.0. The SDK in in version 2.13.1.&lt;/P&gt;&lt;P&gt;Yesterday I did some tests with the MCUXpresso IDE and I can confirm that the Channel number conformed with your one. But also in this tool I have the same problem.&lt;/P&gt;&lt;P&gt;I have discovered that the warning appears as soon as in the Peripheral Signals of the Pins tool I enable OTG1_ID on pin GPIO_AD_09. The funny thing is that when I rout&amp;nbsp; pin OTG1_ID on pin GPIO_AD_09, the LPADC1 peripheral generate the warning for every conversion command that involve the B part of the ADC. (e.g. Channel sample mode = Single end mode, using B and Channel number=B, 1_0 » [T17] USB_OTG2_PWR/WL_DEV_WAKE/U354[10]/J10[2] or&amp;nbsp;B, 1_2 » [P16] USB_OTG1_OC/U26[A2]/J26[4] or&amp;nbsp;B, 1_3 » [L12] SPDIF_SR_CLK/ANATOP_32K_OUT/J26[8] etc....&lt;/P&gt;&lt;P&gt;I'm starting to think there is a bug in this part of the tool. The generated code per the pin mux looks correct to me (see below).&lt;/P&gt;&lt;P&gt;What's your opinion?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;Massimo&lt;/P&gt;&lt;P&gt;void BOARD_InitPins(void) {&lt;BR /&gt;CLOCK_EnableClock(kCLOCK_Iomuxc); /* LPCG on: LPCG is ON. */&lt;/P&gt;&lt;P&gt;IOMUXC_SetPinMux(&lt;BR /&gt;IOMUXC_GPIO_AD_06_GPIO_MUX3_IO05, /* GPIO_AD_06 is configured as GPIO_MUX3_IO05 */&lt;BR /&gt;0U); /* Software Input On Field: Input Path is determined by functionality */&lt;BR /&gt;IOMUXC_SetPinMux(&lt;BR /&gt;IOMUXC_GPIO_AD_07_GPIO_MUX3_IO06, /* GPIO_AD_07 is configured as GPIO_MUX3_IO06 */&lt;BR /&gt;0U); /* Software Input On Field: Input Path is determined by functionality */&lt;BR /&gt;IOMUXC_SetPinMux(&lt;BR /&gt;IOMUXC_GPIO_AD_09_USBPHY1_OTG_ID, /* GPIO_AD_09 is configured as USBPHY1_OTG_ID */&lt;BR /&gt;0U); /* Software Input On Field: Input Path is determined by functionality */&lt;BR /&gt;IOMUXC_SetPinMux(&lt;BR /&gt;IOMUXC_GPIO_AD_24_LPUART1_TXD, /* GPIO_AD_24 is configured as LPUART1_TXD */&lt;BR /&gt;0U); /* Software Input On Field: Input Path is determined by functionality */&lt;BR /&gt;IOMUXC_SetPinMux(&lt;BR /&gt;IOMUXC_GPIO_AD_25_LPUART1_RXD, /* GPIO_AD_25 is configured as LPUART1_RXD */&lt;BR /&gt;0U); /* Software Input On Field: Input Path is determined by functionality */&lt;BR /&gt;IOMUXC_SetPinConfig(&lt;BR /&gt;IOMUXC_GPIO_AD_24_LPUART1_TXD, /* GPIO_AD_24 PAD functional properties : */&lt;BR /&gt;0x02U); /* Slew Rate Field: Slow Slew Rate&lt;BR /&gt;Drive Strength Field: high drive strength&lt;BR /&gt;Pull / Keep Select Field: Pull Disable, Highz&lt;BR /&gt;Pull Up / Down Config. Field: Weak pull down&lt;BR /&gt;Open Drain Field: Disabled&lt;BR /&gt;Domain write protection: Both cores are allowed&lt;BR /&gt;Domain write protection lock: Neither of DWP bits is locked */&lt;BR /&gt;IOMUXC_SetPinConfig(&lt;BR /&gt;IOMUXC_GPIO_AD_25_LPUART1_RXD, /* GPIO_AD_25 PAD functional properties : */&lt;BR /&gt;0x02U); /* Slew Rate Field: Slow Slew Rate&lt;BR /&gt;Drive Strength Field: high drive strength&lt;BR /&gt;Pull / Keep Select Field: Pull Disable, Highz&lt;BR /&gt;Pull Up / Down Config. Field: Weak pull down&lt;BR /&gt;Open Drain Field: Disabled&lt;BR /&gt;Domain write protection: Both cores are allowed&lt;BR /&gt;Domain write protection lock: Neither of DWP bits is locked */&lt;BR /&gt;}&lt;/P&gt;</description>
      <pubDate>Thu, 30 Mar 2023 06:52:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/LPADC1-Differential-mode/m-p/1624981#M24355</guid>
      <dc:creator>Max83</dc:creator>
      <dc:date>2023-03-30T06:52:18Z</dc:date>
    </item>
    <item>
      <title>Re: LPADC1 Differential mode</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/LPADC1-Differential-mode/m-p/1626517#M24396</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/214947"&gt;@Max83&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Yes, it seems like a bug. I'll report it. You can ignore the warning message.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Jing&lt;/P&gt;</description>
      <pubDate>Mon, 03 Apr 2023 02:53:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/LPADC1-Differential-mode/m-p/1626517#M24396</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2023-04-03T02:53:48Z</dc:date>
    </item>
    <item>
      <title>Re: LPADC1 Differential mode</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/LPADC1-Differential-mode/m-p/1626621#M24402</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/61241"&gt;@jingpan&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;thank you for your reply. May you tell me where I can find chip related informations? For instance, is there any document that specify the pin couple that I have to use for a differential voltage conversion? I can't find this information in the reference manual.&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;Massimo&lt;/P&gt;</description>
      <pubDate>Mon, 03 Apr 2023 06:45:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/LPADC1-Differential-mode/m-p/1626621#M24402</guid>
      <dc:creator>Max83</dc:creator>
      <dc:date>2023-04-03T06:45:18Z</dc:date>
    </item>
    <item>
      <title>Re: LPADC1 Differential mode</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/LPADC1-Differential-mode/m-p/1627243#M24419</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/214947"&gt;@Max83&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;That is in datasheet.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/data-sheet/IMXRT1170CEC.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/data-sheet/IMXRT1170CEC.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Jing&lt;/P&gt;</description>
      <pubDate>Tue, 04 Apr 2023 03:07:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/LPADC1-Differential-mode/m-p/1627243#M24419</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2023-04-04T03:07:47Z</dc:date>
    </item>
    <item>
      <title>Re: LPADC1 Differential mode</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/LPADC1-Differential-mode/m-p/1629079#M24475</link>
      <description>&lt;P&gt;Ok, thank you very much for the support.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;Massimo&lt;/P&gt;</description>
      <pubDate>Thu, 06 Apr 2023 11:51:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/LPADC1-Differential-mode/m-p/1629079#M24475</guid>
      <dc:creator>Max83</dc:creator>
      <dc:date>2023-04-06T11:51:03Z</dc:date>
    </item>
  </channel>
</rss>