<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUs中的主题 Re: how to connect MIMXRT685's SWD with JLINK</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/how-to-connect-MIMXRT685-s-SWD-with-JLINK/m-p/1624692#M24345</link>
    <description>&lt;P&gt;Hello, my name is Pavel, and I will be supporting your case, I do not understand if you want to use the debug On-Board of an external debugger. Could you review the jumpers if there are in the default place? I attached the document that could help you to review that.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Could you share an image of your setup?&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Pavel&lt;/P&gt;</description>
    <pubDate>Thu, 30 Mar 2023 01:23:55 GMT</pubDate>
    <dc:creator>Pavel_Hernandez</dc:creator>
    <dc:date>2023-03-30T01:23:55Z</dc:date>
    <item>
      <title>how to connect MIMXRT685's SWD with JLINK</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/how-to-connect-MIMXRT685-s-SWD-with-JLINK/m-p/1624221#M24338</link>
      <description>&lt;P&gt;when i tried to "&lt;SPAN&gt;Getting Started with i.MX RT600 Evaluation Kit&lt;/SPAN&gt;", i run command like below:&lt;/P&gt;&lt;P&gt;xt-ocd.exe -c topology.xml&lt;/P&gt;&lt;P&gt;i meet some difference than website:&lt;/P&gt;&lt;P&gt;XOCD 14.09 2022-06-28 16:24:11&lt;BR /&gt;(c) 1999-2023 Cadence Design Systems Inc. All rights reserved.&lt;BR /&gt;[Debug Log 2023-03-29 20:28:12]&lt;BR /&gt;Loading module "gdbstub" v2.0.0.12&lt;BR /&gt;Loading module "jlink" v2.0.2.0&lt;BR /&gt;Using JLINK lib v.78605&lt;BR /&gt;Jlink USB Serial Number: 729706236&lt;BR /&gt;Connected to Jlink Device:&lt;BR /&gt;Name:'J-Link LPCXpresso V2 compiled Apr 4 2019 16:54:03'&lt;BR /&gt;S/N:729706236&lt;BR /&gt;Firmware: J-Link LPCXpresso V2 compiled Apr 4 2019 16:54:03&lt;BR /&gt;Requested/Set TCK: 1000kHz/1000kHz&lt;BR /&gt;Jlink: Select pipelined SWD&lt;BR /&gt;SWD-DP with ID 0x6BA02477&lt;BR /&gt;Loading module "jtag" v2.0.0.20&lt;BR /&gt;Loading module "xtensa" v2.0.0.48&lt;BR /&gt;Starting thread 'GDBStub'&lt;BR /&gt;Opened GDB socket at port 20000&lt;BR /&gt;Initialize XDM driver&lt;BR /&gt;Error: SWD Wait time-out expired!&lt;BR /&gt;SWD-DP with ID 0x6BA02477&lt;BR /&gt;SWD-DP with ID 0x6BA02477&lt;BR /&gt;SWD-DP with ID 0x6BA02477&lt;BR /&gt;SWD-DP with ID 0x6BA02477&lt;BR /&gt;Error: XDM initialization failed&lt;BR /&gt;ERROR: Couldn't initialize, exit...&lt;/P&gt;&lt;P&gt;is that means i have to connect board's SWD to a J-link?&lt;/P&gt;&lt;P&gt;i dont know how to connect my MIMXRT685 board with Jlink hardware, should i use jumper? or some&amp;nbsp;Transfer interface line？&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 29 Mar 2023 12:31:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/how-to-connect-MIMXRT685-s-SWD-with-JLINK/m-p/1624221#M24338</guid>
      <dc:creator>fwdykpa</dc:creator>
      <dc:date>2023-03-29T12:31:29Z</dc:date>
    </item>
    <item>
      <title>Re: how to connect MIMXRT685's SWD with JLINK</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/how-to-connect-MIMXRT685-s-SWD-with-JLINK/m-p/1624692#M24345</link>
      <description>&lt;P&gt;Hello, my name is Pavel, and I will be supporting your case, I do not understand if you want to use the debug On-Board of an external debugger. Could you review the jumpers if there are in the default place? I attached the document that could help you to review that.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Could you share an image of your setup?&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Pavel&lt;/P&gt;</description>
      <pubDate>Thu, 30 Mar 2023 01:23:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/how-to-connect-MIMXRT685-s-SWD-with-JLINK/m-p/1624692#M24345</guid>
      <dc:creator>Pavel_Hernandez</dc:creator>
      <dc:date>2023-03-30T01:23:55Z</dc:date>
    </item>
  </channel>
</rss>