<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: How to disable the OTG function of RT1062 and use it as device mode only. in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/How-to-disable-the-OTG-function-of-RT1062-and-use-it-as-device/m-p/1623662#M24308</link>
    <description>&lt;P&gt;&lt;SPAN&gt;Hello.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/61241"&gt;@jingpan&lt;/a&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;gt; 2. yes.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Could you tell me what to be aware of when using these pins as GPIO?&lt;/P&gt;</description>
    <pubDate>Wed, 29 Mar 2023 00:25:10 GMT</pubDate>
    <dc:creator>Taka05</dc:creator>
    <dc:date>2023-03-29T00:25:10Z</dc:date>
    <item>
      <title>How to disable the OTG function of RT1062 and use it as device mode only.</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/How-to-disable-the-OTG-function-of-RT1062-and-use-it-as-device/m-p/1622245#M24269</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;We want to use USB of MIMXRT1062 as device mode only.&lt;/P&gt;&lt;P&gt;We would like to use OTG1_PWR, OTG1_OC and OTG1_ID as GPIO because we do not use the OTG function.&lt;/P&gt;&lt;P&gt;The questions are&lt;/P&gt;&lt;P&gt;Q1. To disable OTG and enable device mode only, can I just set the CM register in&amp;nbsp; 42.7.33 USB Device Mode (USB_nUSBMODE) to Device Controller?&lt;/P&gt;&lt;P&gt;Q2. Are there any precautions when using&lt;/P&gt;&lt;P&gt;USB_OTG1_PWR (GPIO_AD_B0_02, GPIO_AD_B1_01)&lt;/P&gt;&lt;P&gt;USB_OTG1_OC (GPIO_AD_B0_03, GPIO_AD_B1_03)&lt;/P&gt;&lt;P&gt;USB_OTG1_ID (GPIO_AD_B0_01, GPIO_AD_B1_02)&lt;/P&gt;&lt;P&gt;as GPIO?&lt;/P&gt;</description>
      <pubDate>Mon, 27 Mar 2023 05:53:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/How-to-disable-the-OTG-function-of-RT1062-and-use-it-as-device/m-p/1622245#M24269</guid>
      <dc:creator>Taka05</dc:creator>
      <dc:date>2023-03-27T05:53:58Z</dc:date>
    </item>
    <item>
      <title>Re: How to disable the OTG function of RT1062 and use it as device mode only.</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/How-to-disable-the-OTG-function-of-RT1062-and-use-it-as-device/m-p/1623262#M24296</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/201127"&gt;@Taka05&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;1. yes. Please refer to the USB device examples.&lt;/P&gt;
&lt;P&gt;2. yes.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Jing&lt;/P&gt;</description>
      <pubDate>Tue, 28 Mar 2023 10:04:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/How-to-disable-the-OTG-function-of-RT1062-and-use-it-as-device/m-p/1623262#M24296</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2023-03-28T10:04:16Z</dc:date>
    </item>
    <item>
      <title>Re: How to disable the OTG function of RT1062 and use it as device mode only.</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/How-to-disable-the-OTG-function-of-RT1062-and-use-it-as-device/m-p/1623662#M24308</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hello.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/61241"&gt;@jingpan&lt;/a&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;gt; 2. yes.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Could you tell me what to be aware of when using these pins as GPIO?&lt;/P&gt;</description>
      <pubDate>Wed, 29 Mar 2023 00:25:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/How-to-disable-the-OTG-function-of-RT1062-and-use-it-as-device/m-p/1623662#M24308</guid>
      <dc:creator>Taka05</dc:creator>
      <dc:date>2023-03-29T00:25:10Z</dc:date>
    </item>
    <item>
      <title>Re: How to disable the OTG function of RT1062 and use it as device mode only.</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/How-to-disable-the-OTG-function-of-RT1062-and-use-it-as-device/m-p/1624946#M24352</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;No, I think nothing need to aware.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;jing&lt;/P&gt;</description>
      <pubDate>Thu, 30 Mar 2023 06:14:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/How-to-disable-the-OTG-function-of-RT1062-and-use-it-as-device/m-p/1624946#M24352</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2023-03-30T06:14:01Z</dc:date>
    </item>
  </channel>
</rss>