<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUsのトピックRe: POR Reset Trigger Pin</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/POR-Reset-Trigger-Pin/m-p/1610269#M24014</link>
    <description>&lt;P&gt;Hello&lt;BR /&gt;I hope you are well&lt;BR /&gt;Generally PMIC_ON_REQ/STBT_REQ are labeled as output during a reset or during the boot process.&lt;BR /&gt;When POR is triggered it returns the pins to the default state, most of them are input.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
    <pubDate>Mon, 06 Mar 2023 19:42:58 GMT</pubDate>
    <dc:creator>Omar_Anguiano</dc:creator>
    <dc:date>2023-03-06T19:42:58Z</dc:date>
    <item>
      <title>POR Reset Trigger Pin</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/POR-Reset-Trigger-Pin/m-p/1606037#M23904</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Are there any PIN triggered(as an output) by the POR or COLD Reset process, on the ROM before any firwmare configuration?&lt;/P&gt;&lt;P&gt;Considering the POR_B pin stable in high.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 27 Feb 2023 11:23:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/POR-Reset-Trigger-Pin/m-p/1606037#M23904</guid>
      <dc:creator>fsantiagop</dc:creator>
      <dc:date>2023-02-27T11:23:17Z</dc:date>
    </item>
    <item>
      <title>Re: POR Reset Trigger Pin</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/POR-Reset-Trigger-Pin/m-p/1610269#M24014</link>
      <description>&lt;P&gt;Hello&lt;BR /&gt;I hope you are well&lt;BR /&gt;Generally PMIC_ON_REQ/STBT_REQ are labeled as output during a reset or during the boot process.&lt;BR /&gt;When POR is triggered it returns the pins to the default state, most of them are input.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
      <pubDate>Mon, 06 Mar 2023 19:42:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/POR-Reset-Trigger-Pin/m-p/1610269#M24014</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2023-03-06T19:42:58Z</dc:date>
    </item>
  </channel>
</rss>