<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Implementing a bootloader Issue MIMXRT1064CVL5B in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Implementing-a-bootloader-Issue-MIMXRT1064CVL5B/m-p/1603813#M23855</link>
    <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am implementing a bootloader for IMX.RT1064. I'm using ROM API to erase and program the new firmware. I'm trying to erase the section after the bootloader and it is not working. When I tried erasing the sector that doesn't has the program, the erase API worked. Whether the sectors with the program is protected?&lt;/P&gt;&lt;P&gt;Our goal is to implement a bootloader that can read the firmware from external SPI flash and program to the internal flash.&lt;/P&gt;</description>
    <pubDate>Wed, 22 Feb 2023 15:56:23 GMT</pubDate>
    <dc:creator>kksakthi</dc:creator>
    <dc:date>2023-02-22T15:56:23Z</dc:date>
    <item>
      <title>Implementing a bootloader Issue MIMXRT1064CVL5B</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Implementing-a-bootloader-Issue-MIMXRT1064CVL5B/m-p/1603813#M23855</link>
      <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am implementing a bootloader for IMX.RT1064. I'm using ROM API to erase and program the new firmware. I'm trying to erase the section after the bootloader and it is not working. When I tried erasing the sector that doesn't has the program, the erase API worked. Whether the sectors with the program is protected?&lt;/P&gt;&lt;P&gt;Our goal is to implement a bootloader that can read the firmware from external SPI flash and program to the internal flash.&lt;/P&gt;</description>
      <pubDate>Wed, 22 Feb 2023 15:56:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Implementing-a-bootloader-Issue-MIMXRT1064CVL5B/m-p/1603813#M23855</guid>
      <dc:creator>kksakthi</dc:creator>
      <dc:date>2023-02-22T15:56:23Z</dc:date>
    </item>
    <item>
      <title>Re: Implementing a bootloader Issue MIMXRT1064CVL5B</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Implementing-a-bootloader-Issue-MIMXRT1064CVL5B/m-p/1609111#M23993</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;First of all, sorry for the later reply.&lt;/P&gt;
&lt;P&gt;Please refer attached example code about ROM API usage.&lt;/P&gt;
&lt;P&gt;Wish it helps.&lt;/P&gt;
&lt;P&gt;best regards,&lt;/P&gt;
&lt;P&gt;Mike&lt;/P&gt;</description>
      <pubDate>Fri, 03 Mar 2023 09:46:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Implementing-a-bootloader-Issue-MIMXRT1064CVL5B/m-p/1609111#M23993</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2023-03-03T09:46:11Z</dc:date>
    </item>
    <item>
      <title>Re: Implementing a bootloader Issue MIMXRT1064CVL5B</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Implementing-a-bootloader-Issue-MIMXRT1064CVL5B/m-p/1609240#M23994</link>
      <description>&lt;P&gt;Hi&lt;BR /&gt;&lt;BR /&gt;See the following for off-the-sheft loaders for the 1064:&lt;BR /&gt;- &lt;A href="https://www.utasker.com/iMX/RT1064.html" target="_blank" rel="noopener"&gt;https://www.utasker.com/iMX/RT1064.html&lt;/A&gt;&lt;BR /&gt;- &lt;A href="https://www.utasker.com/iMX/developers.html" target="_blank" rel="noopener"&gt;https://www.utasker.com/iMX/developers.html&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Supporting various methods (USB, Ethernet, SD card, Memory stick, external SPI) and allowing operation in Xip, XiP-BEE encrypted, RAM and SDRAM (with optional AES256 storage in Flash).&lt;BR /&gt;Stable, fully documented and industrial proven solution.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 03 Mar 2023 13:49:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Implementing-a-bootloader-Issue-MIMXRT1064CVL5B/m-p/1609240#M23994</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2023-03-03T13:49:52Z</dc:date>
    </item>
  </channel>
</rss>