<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUsのトピックRe: are i.MX RT 1170 family ASIL(ISO 26262)/SIL(IEC 61508) compliancy level ?</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/are-i-MX-RT-1170-family-ASIL-ISO-26262-SIL-IEC-61508-compliancy/m-p/1600293#M23757</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;No, RT1170 hasn't such certification.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 16 Feb 2023 07:57:46 GMT</pubDate>
    <dc:creator>jingpan</dc:creator>
    <dc:date>2023-02-16T07:57:46Z</dc:date>
    <item>
      <title>are i.MX RT 1170 family ASIL(ISO 26262)/SIL(IEC 61508) compliancy level ?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/are-i-MX-RT-1170-family-ASIL-ISO-26262-SIL-IEC-61508-compliancy/m-p/1595231#M23623</link>
      <description>&lt;P&gt;1. ASIL and SIL compliancy level for industrial and automotive ? ASIL-B/C/D and SIL-2/3 ? Do you have plans in the future to get these compliancy certificates ? or do you already have them ?&amp;nbsp;&lt;/P&gt;&lt;P&gt;2. Also,&lt;/P&gt;&lt;P&gt;It says temperature gradient from&lt;/P&gt;&lt;P&gt;-40 to +125 for Automotive Part Number under i.MX RT 1171/72 which is AEC-Q100 Grade 1 requirements.&lt;/P&gt;&lt;P&gt;Please let me know if there are any plans for AEC-Q100 Grade 1 compliance for the i.MX RT 1171/72 family ? Or do you already have it ? This is required for an automotive OEM.&lt;/P&gt;</description>
      <pubDate>Wed, 08 Feb 2023 05:18:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/are-i-MX-RT-1170-family-ASIL-ISO-26262-SIL-IEC-61508-compliancy/m-p/1595231#M23623</guid>
      <dc:creator>Kiyasul</dc:creator>
      <dc:date>2023-02-08T05:18:01Z</dc:date>
    </item>
    <item>
      <title>Re: are i.MX RT 1170 family ASIL(ISO 26262)/SIL(IEC 61508) compliancy level ?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/are-i-MX-RT-1170-family-ASIL-ISO-26262-SIL-IEC-61508-compliancy/m-p/1596296#M23639</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/212307"&gt;@Kiyasul&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;The i.MX RT 1170 auto PNs are qualified to AEC-Q100 Grade 3 with PPAP. However, the documents you need are shared under NDA with your nearest distributor.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;i.MX RT1170 (Auto version) isn't a ASIL rated device but QM. As a QM device, it only can be used in ASIL A/B system/application, cannot support ASIL D application.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Jing&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 09 Feb 2023 07:09:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/are-i-MX-RT-1170-family-ASIL-ISO-26262-SIL-IEC-61508-compliancy/m-p/1596296#M23639</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2023-02-09T07:09:18Z</dc:date>
    </item>
    <item>
      <title>Re: are i.MX RT 1170 family ASIL(ISO 26262)/SIL(IEC 61508) compliancy level ?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/are-i-MX-RT-1170-family-ASIL-ISO-26262-SIL-IEC-61508-compliancy/m-p/1596584#M23652</link>
      <description>&lt;P&gt;Thank you for the response&lt;/P&gt;</description>
      <pubDate>Thu, 09 Feb 2023 12:31:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/are-i-MX-RT-1170-family-ASIL-ISO-26262-SIL-IEC-61508-compliancy/m-p/1596584#M23652</guid>
      <dc:creator>Kiyasul</dc:creator>
      <dc:date>2023-02-09T12:31:21Z</dc:date>
    </item>
    <item>
      <title>Re: are i.MX RT 1170 family ASIL(ISO 26262)/SIL(IEC 61508) compliancy level ?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/are-i-MX-RT-1170-family-ASIL-ISO-26262-SIL-IEC-61508-compliancy/m-p/1599680#M23743</link>
      <description>&lt;P&gt;Hello jingpan,&lt;/P&gt;&lt;P&gt;And for auronautic market. Can we use it in a DALB/DALC applications?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 15 Feb 2023 15:40:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/are-i-MX-RT-1170-family-ASIL-ISO-26262-SIL-IEC-61508-compliancy/m-p/1599680#M23743</guid>
      <dc:creator>NaiaraU</dc:creator>
      <dc:date>2023-02-15T15:40:01Z</dc:date>
    </item>
    <item>
      <title>Re: are i.MX RT 1170 family ASIL(ISO 26262)/SIL(IEC 61508) compliancy level ?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/are-i-MX-RT-1170-family-ASIL-ISO-26262-SIL-IEC-61508-compliancy/m-p/1600293#M23757</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;No, RT1170 hasn't such certification.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 16 Feb 2023 07:57:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/are-i-MX-RT-1170-family-ASIL-ISO-26262-SIL-IEC-61508-compliancy/m-p/1600293#M23757</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2023-02-16T07:57:46Z</dc:date>
    </item>
    <item>
      <title>Re: are i.MX RT 1170 family ASIL(ISO 26262)/SIL(IEC 61508) compliancy level ?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/are-i-MX-RT-1170-family-ASIL-ISO-26262-SIL-IEC-61508-compliancy/m-p/2090179#M34206</link>
      <description>&lt;P&gt;Hi Jing&lt;/P&gt;&lt;P&gt;&amp;nbsp;Further question according to you reply. For ASIL A requirement of CAN and button (GPIO), Can just use&amp;nbsp;&lt;SPAN&gt;RT1170&amp;nbsp;standalone? Or it must has a additional ASIL A level of MCU to do it?&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 30 Apr 2025 10:37:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/are-i-MX-RT-1170-family-ASIL-ISO-26262-SIL-IEC-61508-compliancy/m-p/2090179#M34206</guid>
      <dc:creator>hctam</dc:creator>
      <dc:date>2025-04-30T10:37:37Z</dc:date>
    </item>
  </channel>
</rss>