<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic USB on MIMXRT1176 in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/USB-on-MIMXRT1176/m-p/1590549#M23518</link>
    <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'am working on USB on the MIMXRT1176 and i have some questions:&amp;nbsp;&lt;/P&gt;&lt;P&gt;1- I tested CDC class VCOM, but the speed seems to be slow for my usage (~300 KB/s), am i looping something to speed up the transfer? I tested the MSC class and the transfer speed reached about 5MB/s, i don't understand why i can't reach such speed on CDC class.&lt;/P&gt;&lt;P&gt;2- For the CDC VNIC SDK example project, there's no lwip stack, how can i test transfer (file or data) with this example for the RNDIS class ?&lt;/P&gt;&lt;P&gt;3- Is there a specific recommended class to reach high speed transfer on USB ?&lt;/P&gt;&lt;P&gt;Regards.&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 31 Jan 2023 11:58:36 GMT</pubDate>
    <dc:creator>ahmedhrabi</dc:creator>
    <dc:date>2023-01-31T11:58:36Z</dc:date>
    <item>
      <title>USB on MIMXRT1176</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/USB-on-MIMXRT1176/m-p/1590549#M23518</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'am working on USB on the MIMXRT1176 and i have some questions:&amp;nbsp;&lt;/P&gt;&lt;P&gt;1- I tested CDC class VCOM, but the speed seems to be slow for my usage (~300 KB/s), am i looping something to speed up the transfer? I tested the MSC class and the transfer speed reached about 5MB/s, i don't understand why i can't reach such speed on CDC class.&lt;/P&gt;&lt;P&gt;2- For the CDC VNIC SDK example project, there's no lwip stack, how can i test transfer (file or data) with this example for the RNDIS class ?&lt;/P&gt;&lt;P&gt;3- Is there a specific recommended class to reach high speed transfer on USB ?&lt;/P&gt;&lt;P&gt;Regards.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 31 Jan 2023 11:58:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/USB-on-MIMXRT1176/m-p/1590549#M23518</guid>
      <dc:creator>ahmedhrabi</dc:creator>
      <dc:date>2023-01-31T11:58:36Z</dc:date>
    </item>
    <item>
      <title>Re: USB on MIMXRT1176</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/USB-on-MIMXRT1176/m-p/1595975#M23634</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/128940"&gt;@ahmedhrabi&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;MSC is expected to be faster by definition. CDC often contains much more back and forth and setup data than MSC.&lt;/P&gt;
&lt;P&gt;The lwip stack can be found on our lwip examples on the SDK.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR,&lt;/P&gt;
&lt;P&gt;Edwin.&lt;/P&gt;</description>
      <pubDate>Wed, 08 Feb 2023 20:54:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/USB-on-MIMXRT1176/m-p/1595975#M23634</guid>
      <dc:creator>EdwinHz</dc:creator>
      <dc:date>2023-02-08T20:54:35Z</dc:date>
    </item>
  </channel>
</rss>