<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic RT1052: Can CSI VSYNC be set to falling-edge triggered? in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1052-Can-CSI-VSYNC-be-set-to-falling-edge-triggered/m-p/1586155#M23377</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;The manual states in section&amp;nbsp;34.3.1.2 Gated Clock Mode:&lt;/P&gt;&lt;P&gt;&lt;EM&gt;The CSI can be programmed to support rising/falling-edge&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;triggered VSYNC through CSI_CR1[SOF_POL]&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;However, when I set&amp;nbsp;SOF_POL=1 this has no effect. CSI still triggers on rising edge.&lt;/P&gt;&lt;P&gt;I'm using traditional interface,&amp;nbsp;CCIR_EN=0,&amp;nbsp;CCIR_MODE=0,&amp;nbsp;EXT_VSYNC=0.&lt;/P&gt;&lt;P&gt;Question: How can VSYNC be configured for falling edge?&lt;/P&gt;&lt;P&gt;Thanks&lt;BR /&gt;Udo&lt;/P&gt;</description>
    <pubDate>Fri, 20 Jan 2023 17:14:40 GMT</pubDate>
    <dc:creator>udoeb</dc:creator>
    <dc:date>2023-01-20T17:14:40Z</dc:date>
    <item>
      <title>RT1052: Can CSI VSYNC be set to falling-edge triggered?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1052-Can-CSI-VSYNC-be-set-to-falling-edge-triggered/m-p/1586155#M23377</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;The manual states in section&amp;nbsp;34.3.1.2 Gated Clock Mode:&lt;/P&gt;&lt;P&gt;&lt;EM&gt;The CSI can be programmed to support rising/falling-edge&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;triggered VSYNC through CSI_CR1[SOF_POL]&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;However, when I set&amp;nbsp;SOF_POL=1 this has no effect. CSI still triggers on rising edge.&lt;/P&gt;&lt;P&gt;I'm using traditional interface,&amp;nbsp;CCIR_EN=0,&amp;nbsp;CCIR_MODE=0,&amp;nbsp;EXT_VSYNC=0.&lt;/P&gt;&lt;P&gt;Question: How can VSYNC be configured for falling edge?&lt;/P&gt;&lt;P&gt;Thanks&lt;BR /&gt;Udo&lt;/P&gt;</description>
      <pubDate>Fri, 20 Jan 2023 17:14:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1052-Can-CSI-VSYNC-be-set-to-falling-edge-triggered/m-p/1586155#M23377</guid>
      <dc:creator>udoeb</dc:creator>
      <dc:date>2023-01-20T17:14:40Z</dc:date>
    </item>
    <item>
      <title>Re: RT1052: Can CSI VSYNC be set to falling-edge triggered?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1052-Can-CSI-VSYNC-be-set-to-falling-edge-triggered/m-p/1589588#M23490</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/152354"&gt;@udoeb&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;This is a interrupt control bit. Can you share how to test this condition?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Jing&lt;/P&gt;</description>
      <pubDate>Mon, 30 Jan 2023 07:37:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1052-Can-CSI-VSYNC-be-set-to-falling-edge-triggered/m-p/1589588#M23490</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2023-01-30T07:37:12Z</dc:date>
    </item>
    <item>
      <title>Re: RT1052: Can CSI VSYNC be set to falling-edge triggered?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1052-Can-CSI-VSYNC-be-set-to-falling-edge-triggered/m-p/1593813#M23596</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Thanks for your reply.&lt;/P&gt;&lt;P&gt;Let me rephrase the question: I do apply an external signal to VSYNC and notice that the DMA starts on the rising edge. My external circuitry requires that DMA starts on the falling edge. How can I achieve that?&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;&lt;SPAN&gt;Udo&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 06 Feb 2023 08:54:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1052-Can-CSI-VSYNC-be-set-to-falling-edge-triggered/m-p/1593813#M23596</guid>
      <dc:creator>udoeb</dc:creator>
      <dc:date>2023-02-06T08:54:48Z</dc:date>
    </item>
    <item>
      <title>Re: RT1052: Can CSI VSYNC be set to falling-edge triggered?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1052-Can-CSI-VSYNC-be-set-to-falling-edge-triggered/m-p/1595327#M23625</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;But SOF_POL default is 0, it is falling edge. SOF_POL=1 means rising edge. Opposite to your setting. So...&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Jing&lt;/P&gt;</description>
      <pubDate>Wed, 08 Feb 2023 07:23:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1052-Can-CSI-VSYNC-be-set-to-falling-edge-triggered/m-p/1595327#M23625</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2023-02-08T07:23:33Z</dc:date>
    </item>
  </channel>
</rss>