<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUs中的主题 Re: imx rt 1024 internal flash configure as RWW</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/imx-rt-1024-internal-flash-configure-as-RWW/m-p/1585150#M23345</link>
    <description>&lt;P&gt;The internal flash doesn't support RWW function.&lt;/P&gt;
&lt;P&gt;You have to run the code in RAM when you opreating the Flash.&lt;/P&gt;</description>
    <pubDate>Thu, 19 Jan 2023 02:56:03 GMT</pubDate>
    <dc:creator>lucas_cao</dc:creator>
    <dc:date>2023-01-19T02:56:03Z</dc:date>
    <item>
      <title>imx rt 1024 internal flash configure as RWW</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/imx-rt-1024-internal-flash-configure-as-RWW/m-p/1584737#M23338</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We are using the imx rt 1024 cpu to run our application. We use a portion of the flash as sort of "eeprom", In order to read / write to flash while executing code at the same time, we need RWW flash. We know by default this is not the case, so we run the nor_flash module (among others) in ITC ram to cope with this.&lt;/P&gt;&lt;P&gt;We were wondering though, is there any way to configure the flash so that we in fact are allowed to use it as RWW? I believe by default we run in SPI quad mode. Can we use a different mode which makes the flash usable as RWW?&lt;/P&gt;</description>
      <pubDate>Wed, 18 Jan 2023 15:35:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/imx-rt-1024-internal-flash-configure-as-RWW/m-p/1584737#M23338</guid>
      <dc:creator>bp1979</dc:creator>
      <dc:date>2023-01-18T15:35:11Z</dc:date>
    </item>
    <item>
      <title>Re: imx rt 1024 internal flash configure as RWW</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/imx-rt-1024-internal-flash-configure-as-RWW/m-p/1585150#M23345</link>
      <description>&lt;P&gt;The internal flash doesn't support RWW function.&lt;/P&gt;
&lt;P&gt;You have to run the code in RAM when you opreating the Flash.&lt;/P&gt;</description>
      <pubDate>Thu, 19 Jan 2023 02:56:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/imx-rt-1024-internal-flash-configure-as-RWW/m-p/1585150#M23345</guid>
      <dc:creator>lucas_cao</dc:creator>
      <dc:date>2023-01-19T02:56:03Z</dc:date>
    </item>
  </channel>
</rss>