<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUsのトピックi.MX RT1050 : external clock</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i-MX-RT1050-external-clock/m-p/743909#M232</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello everybody! I am a newbie with the community and with i.MX as well.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'd like to start with a (hopefully) simple question about RT1050. The datasheet always refers to an external 24 MHz clock. Although this frequency is defined as "typical" or "suggested", I can't understand if you can use a different value, say 24.576 MHz.&lt;/P&gt;&lt;P&gt;For example,it seems to me that both 480 MHz for USB and 25 MHz for ETH use fixed PLL that rely on a 24 MHz Xtal.&lt;/P&gt;&lt;P&gt;Suggestions?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Giuseppe&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 13 Feb 2018 14:54:51 GMT</pubDate>
    <dc:creator>giuseppescarpi</dc:creator>
    <dc:date>2018-02-13T14:54:51Z</dc:date>
    <item>
      <title>i.MX RT1050 : external clock</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i-MX-RT1050-external-clock/m-p/743909#M232</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello everybody! I am a newbie with the community and with i.MX as well.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'd like to start with a (hopefully) simple question about RT1050. The datasheet always refers to an external 24 MHz clock. Although this frequency is defined as "typical" or "suggested", I can't understand if you can use a different value, say 24.576 MHz.&lt;/P&gt;&lt;P&gt;For example,it seems to me that both 480 MHz for USB and 25 MHz for ETH use fixed PLL that rely on a 24 MHz Xtal.&lt;/P&gt;&lt;P&gt;Suggestions?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Giuseppe&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Feb 2018 14:54:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i-MX-RT1050-external-clock/m-p/743909#M232</guid>
      <dc:creator>giuseppescarpi</dc:creator>
      <dc:date>2018-02-13T14:54:51Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX RT1050 : external clock</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i-MX-RT1050-external-clock/m-p/743910#M233</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Giuseppe&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes this undersatnding is correct, in general one can try to&lt;/P&gt;&lt;P&gt;adjust plls values appropriately using formula in sect.18.6.1.3 PLL reference clock,&lt;/P&gt;&lt;P&gt;sect.18.8 CCM Analog Memory Map/Register Definition i.MX RT1050 Reference Manual &lt;BR /&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fwww.nxp.com%2Fdocs%2Fen%2Freference-manual%2FIMXRT1050RM.pdf" rel="nofollow" target="_blank"&gt;https://www.nxp.com/docs/en/reference-manual/IMXRT1050RM.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Feb 2018 22:55:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i-MX-RT1050-external-clock/m-p/743910#M233</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-02-13T22:55:21Z</dc:date>
    </item>
  </channel>
</rss>