<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUsのトピックRe: i2c touch panel init</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i2c-touch-panel-init/m-p/1575543#M23117</link>
    <description>&lt;P&gt;Hi Pavel,&lt;/P&gt;&lt;P&gt;thanks for your fast reply.&lt;/P&gt;&lt;P&gt;The evaluation kit we are using is from Embedded Artist and the display is the&amp;nbsp;RK043FN02H-CT.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've discovered the problem: the flat cable of the touch was damaged (bent during insertion has interrupted one I2C bus line). Also disabling the touch I was not able to run the demo application but I think the demo in MCUExpresso was for the 5.5" display and not for 4.3".&lt;/P&gt;&lt;P&gt;Now I've modified the demo developing one with a custom window for the 4.3" display, made of Azure GUIX IDE and it works fine.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 29 Dec 2022 11:23:06 GMT</pubDate>
    <dc:creator>Pianetti</dc:creator>
    <dc:date>2022-12-29T11:23:06Z</dc:date>
    <item>
      <title>i2c touch panel init</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i2c-touch-panel-init/m-p/1575216#M23097</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;IMG src="Board init" border="0" alt="" /&gt;we are using RT1166 developer's kit.&lt;/P&gt;&lt;P&gt;We are using MCUXspresso IDE and we are charged the demo project:&lt;/P&gt;&lt;P&gt;eaimxrt1166_guix_washing_machine_hd&lt;/P&gt;&lt;P&gt;but when the firmware arrived on&amp;nbsp;BOARD_InitTouchPanel() function:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;#if USE_FT5406_TOUCH()&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;// Use PCA9530 to initialize the LPI2C5 bus&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;PCA9530_Init();&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;if (kStatus_Success != FT5406_RT_Init(&amp;amp;s_touchHandle, LPI2C5))&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;{&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;FONT color="#FF0000"&gt;&lt;STRONG&gt;PRINTF("Touch IC initialization failed\r\n");&lt;/STRONG&gt;&lt;/FONT&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;assert(false);&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;}&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;the firmware go on line&amp;nbsp;&lt;FONT color="#FF0000"&gt;&lt;STRONG&gt;PRINTF("Touch IC initialization failed\r\n");&lt;/STRONG&gt;&lt;/FONT&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;FONT color="#000000"&gt;Somebody can help me?&lt;/FONT&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 28 Dec 2022 13:40:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i2c-touch-panel-init/m-p/1575216#M23097</guid>
      <dc:creator>Pianetti</dc:creator>
      <dc:date>2022-12-28T13:40:36Z</dc:date>
    </item>
    <item>
      <title>Re: i2c touch panel init</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i2c-touch-panel-init/m-p/1575317#M23103</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm reviewing your case, but could you share the information about the model of your screen? Because there are some differences in the SDK because &lt;SPAN&gt;Rocktech discontinued a&amp;nbsp;display.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;A href="https://community.nxp.com/t5/i-MX-RT-Knowledge-Base/Updated-LCD-panels-for-i-MX-RT-EVKs/ta-p/1452416" target="_blank"&gt;Updated LCD panels for i.MX RT EVKs - NXP Community&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;In this thread, you can find the steps to modify if this is your issue. Could you please review&amp;nbsp;the information and confirm? let me know if you have more questions.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;Pavel&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 28 Dec 2022 23:17:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i2c-touch-panel-init/m-p/1575317#M23103</guid>
      <dc:creator>Pavel_Hernandez</dc:creator>
      <dc:date>2022-12-28T23:17:00Z</dc:date>
    </item>
    <item>
      <title>Re: i2c touch panel init</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i2c-touch-panel-init/m-p/1575543#M23117</link>
      <description>&lt;P&gt;Hi Pavel,&lt;/P&gt;&lt;P&gt;thanks for your fast reply.&lt;/P&gt;&lt;P&gt;The evaluation kit we are using is from Embedded Artist and the display is the&amp;nbsp;RK043FN02H-CT.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've discovered the problem: the flat cable of the touch was damaged (bent during insertion has interrupted one I2C bus line). Also disabling the touch I was not able to run the demo application but I think the demo in MCUExpresso was for the 5.5" display and not for 4.3".&lt;/P&gt;&lt;P&gt;Now I've modified the demo developing one with a custom window for the 4.3" display, made of Azure GUIX IDE and it works fine.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 29 Dec 2022 11:23:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i2c-touch-panel-init/m-p/1575543#M23117</guid>
      <dc:creator>Pianetti</dc:creator>
      <dc:date>2022-12-29T11:23:06Z</dc:date>
    </item>
  </channel>
</rss>