<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUsのトピックimxRT1170 LPUART code with interrupts.</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/imxRT1170-LPUART-code-with-interrupts/m-p/1574787#M23078</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using imxRT1170 EVK board. I want to use &lt;STRONG&gt;LPUART1 peripheral in interrupt mode&lt;/STRONG&gt;. I am using IAR tool for coding. Can you please share me the &lt;STRONG&gt;example code for using LPUART in interrupt mode&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;I want to use the below &lt;STRONG&gt;API's&lt;/STRONG&gt;&amp;nbsp;provided:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;status_t LPUART_TransferSendNonBlocking(LPUART_Type *base, lpuart_handle_t *handle, lpuart_transfer_t *xfer)&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;status_t LPUART_TransferReceiveNonBlocking(LPUART_Type *base,lpuart_handle_t *handle,&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;lpuart_transfer_t *xfer, size_t *receivedBytes)&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;What are the configuration I need to do to use it in interrupt mode?&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;</description>
    <pubDate>Tue, 27 Dec 2022 04:54:04 GMT</pubDate>
    <dc:creator>Naveed</dc:creator>
    <dc:date>2022-12-27T04:54:04Z</dc:date>
    <item>
      <title>imxRT1170 LPUART code with interrupts.</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/imxRT1170-LPUART-code-with-interrupts/m-p/1574787#M23078</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using imxRT1170 EVK board. I want to use &lt;STRONG&gt;LPUART1 peripheral in interrupt mode&lt;/STRONG&gt;. I am using IAR tool for coding. Can you please share me the &lt;STRONG&gt;example code for using LPUART in interrupt mode&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;I want to use the below &lt;STRONG&gt;API's&lt;/STRONG&gt;&amp;nbsp;provided:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;status_t LPUART_TransferSendNonBlocking(LPUART_Type *base, lpuart_handle_t *handle, lpuart_transfer_t *xfer)&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;status_t LPUART_TransferReceiveNonBlocking(LPUART_Type *base,lpuart_handle_t *handle,&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;lpuart_transfer_t *xfer, size_t *receivedBytes)&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;What are the configuration I need to do to use it in interrupt mode?&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;</description>
      <pubDate>Tue, 27 Dec 2022 04:54:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/imxRT1170-LPUART-code-with-interrupts/m-p/1574787#M23078</guid>
      <dc:creator>Naveed</dc:creator>
      <dc:date>2022-12-27T04:54:04Z</dc:date>
    </item>
    <item>
      <title>Re: imxRT1170 LPUART code with interrupts.</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/imxRT1170-LPUART-code-with-interrupts/m-p/1575237#M23099</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/203896"&gt;@Naveed&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I hope you are doing great,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please refer to the lpuart_interrupt_transfer in the RT1170 SDK, there you will find those APIs implemented and the related interrupt mode configuration.&lt;/P&gt;
&lt;P&gt;Regarding IAR toolchain, just in case you need any info,&amp;nbsp; I know two ways to get the example :&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;Installing the RT1170 BSP/Pack,&amp;nbsp; and then import the example using the CMSIS Pack Manager&amp;nbsp;&lt;/LI&gt;
&lt;LI&gt;Build and download the RT1170 SDK from&amp;nbsp;&lt;A href="https://mcuxpresso.nxp.com/en/welcome" target="_blank" rel="noopener"&gt;https://mcuxpresso.nxp.com/en/welcome&lt;/A&gt;&amp;nbsp;. Then un-zip the SDK and find the project in the SDK folder, to finally open its workspace with IAR.&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;All the best,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Diego&lt;/P&gt;</description>
      <pubDate>Wed, 28 Dec 2022 15:07:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/imxRT1170-LPUART-code-with-interrupts/m-p/1575237#M23099</guid>
      <dc:creator>diego_charles</dc:creator>
      <dc:date>2022-12-28T15:07:56Z</dc:date>
    </item>
  </channel>
</rss>