<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: 10/100Mbps Ethernet sample code in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/10-100Mbps-Ethernet-sample-code/m-p/1560872#M22676</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/206240"&gt;@sai_shinde&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;1) Our example codes are designed with the intention to be used with both the 10/100 Mbps and 1G Mbps Modules. You can change ENET and ENET1G by removing the following definition: "BOARD_NETWORK_USE_100M_ENET_PORT" on the example projects. This will use the 1G instead of the 100M module.&lt;/P&gt;
&lt;P&gt;2) The ENET peripheral is not yet implemented on ConfigTools, so it is not possible to enable this module using the Peripherals tool on MCUXpresso.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR,&lt;/P&gt;
&lt;P&gt;Edwin.&lt;/P&gt;</description>
    <pubDate>Mon, 28 Nov 2022 22:16:51 GMT</pubDate>
    <dc:creator>EdwinHz</dc:creator>
    <dc:date>2022-11-28T22:16:51Z</dc:date>
    <item>
      <title>10/100Mbps Ethernet sample code</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/10-100Mbps-Ethernet-sample-code/m-p/1559744#M22640</link>
      <description>&lt;P&gt;Hello All,&lt;/P&gt;&lt;P&gt;I want to use&amp;nbsp;2-bit Reduced MII (RMII)100/100Mbps Ethernet on my custom board with IMXRT1170.&lt;/P&gt;&lt;P&gt;Below are my queries&lt;/P&gt;&lt;P&gt;1&amp;gt; I am not able to find the sample code for&amp;nbsp;10/100Mbps Ethernet. All code in SDK is for Ethernet1G. Where to find the sample code for&amp;nbsp;10/100Mbps Ethernet ?&lt;/P&gt;&lt;P&gt;2&amp;gt; I tried to add Ethernet peripheral from config tool but I am not able to find Ethernet as peripheral in MCUExpresso config tool. How to add and configure Ethernet peripheral from MCUExpresso config tool?&lt;/P&gt;&lt;P&gt;I am able to add "lwip" in middleware section but how to link/configure the pins for 2-bit Reduced MII (RMII)100/100Mbps Ethernet interface.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Sainath&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 25 Nov 2022 05:51:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/10-100Mbps-Ethernet-sample-code/m-p/1559744#M22640</guid>
      <dc:creator>sai_shinde</dc:creator>
      <dc:date>2022-11-25T05:51:50Z</dc:date>
    </item>
    <item>
      <title>Re: 10/100Mbps Ethernet sample code</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/10-100Mbps-Ethernet-sample-code/m-p/1560872#M22676</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/206240"&gt;@sai_shinde&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;1) Our example codes are designed with the intention to be used with both the 10/100 Mbps and 1G Mbps Modules. You can change ENET and ENET1G by removing the following definition: "BOARD_NETWORK_USE_100M_ENET_PORT" on the example projects. This will use the 1G instead of the 100M module.&lt;/P&gt;
&lt;P&gt;2) The ENET peripheral is not yet implemented on ConfigTools, so it is not possible to enable this module using the Peripherals tool on MCUXpresso.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR,&lt;/P&gt;
&lt;P&gt;Edwin.&lt;/P&gt;</description>
      <pubDate>Mon, 28 Nov 2022 22:16:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/10-100Mbps-Ethernet-sample-code/m-p/1560872#M22676</guid>
      <dc:creator>EdwinHz</dc:creator>
      <dc:date>2022-11-28T22:16:51Z</dc:date>
    </item>
    <item>
      <title>Re: 10/100Mbps Ethernet sample code</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/10-100Mbps-Ethernet-sample-code/m-p/1561223#M22696</link>
      <description>&lt;P&gt;Thanks&amp;nbsp;&lt;A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/186731" target="_self"&gt;&lt;SPAN class=""&gt;EdwinHz.&lt;/SPAN&gt;&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 29 Nov 2022 09:33:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/10-100Mbps-Ethernet-sample-code/m-p/1561223#M22696</guid>
      <dc:creator>sai_shinde</dc:creator>
      <dc:date>2022-11-29T09:33:31Z</dc:date>
    </item>
  </channel>
</rss>