<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUsのトピックLCDIF RGB mapping</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/LCDIF-RGB-mapping/m-p/1553853#M22476</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm currently designing a board which needs to be attached to an RGB888 Display.&lt;/P&gt;&lt;P&gt;From what I can understand from the Reference Manual of the iMXRT1064 there are various possibility to attach the display.&lt;/P&gt;&lt;P&gt;In the NXP board the display is attached in a BGR order and currently I attached the pins following that idea to give the firmware guys the same platform as the one they have on hands:&lt;BR /&gt;LCDIF_D0..D7 goes to DISPLAY_B0..B7&lt;BR /&gt;LCDIF_D8..D15 goes to DISPLAY_G0..G7&lt;BR /&gt;LCDIF_D16..D23 goes to DISPLAY_R0..R7&lt;BR /&gt;As in the attached picture.&lt;/P&gt;&lt;P&gt;Problem is that this project is a porting from an MCU of another manufacturer and the firmware guys allready have all the images and code ready to be ported on the iMXRT1064...&lt;/P&gt;&lt;P&gt;What is your advice? should I connect the bus in a RGB888 order like so:&lt;BR /&gt;D0..D7 to R0..R7&lt;BR /&gt;D8..D15 to G0..G7&lt;BR /&gt;D16..D24 to B0..B7&lt;/P&gt;&lt;P&gt;Thank you very much for you help.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 15 Nov 2022 08:39:16 GMT</pubDate>
    <dc:creator>SimoneT</dc:creator>
    <dc:date>2022-11-15T08:39:16Z</dc:date>
    <item>
      <title>LCDIF RGB mapping</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/LCDIF-RGB-mapping/m-p/1553853#M22476</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm currently designing a board which needs to be attached to an RGB888 Display.&lt;/P&gt;&lt;P&gt;From what I can understand from the Reference Manual of the iMXRT1064 there are various possibility to attach the display.&lt;/P&gt;&lt;P&gt;In the NXP board the display is attached in a BGR order and currently I attached the pins following that idea to give the firmware guys the same platform as the one they have on hands:&lt;BR /&gt;LCDIF_D0..D7 goes to DISPLAY_B0..B7&lt;BR /&gt;LCDIF_D8..D15 goes to DISPLAY_G0..G7&lt;BR /&gt;LCDIF_D16..D23 goes to DISPLAY_R0..R7&lt;BR /&gt;As in the attached picture.&lt;/P&gt;&lt;P&gt;Problem is that this project is a porting from an MCU of another manufacturer and the firmware guys allready have all the images and code ready to be ported on the iMXRT1064...&lt;/P&gt;&lt;P&gt;What is your advice? should I connect the bus in a RGB888 order like so:&lt;BR /&gt;D0..D7 to R0..R7&lt;BR /&gt;D8..D15 to G0..G7&lt;BR /&gt;D16..D24 to B0..B7&lt;/P&gt;&lt;P&gt;Thank you very much for you help.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 15 Nov 2022 08:39:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/LCDIF-RGB-mapping/m-p/1553853#M22476</guid>
      <dc:creator>SimoneT</dc:creator>
      <dc:date>2022-11-15T08:39:16Z</dc:date>
    </item>
    <item>
      <title>Re: LCDIF RGB mapping</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/LCDIF-RGB-mapping/m-p/1555506#M22519</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/208794"&gt;@SimoneT&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Maybe our &lt;/SPAN&gt;&lt;SPAN&gt;Printed Circuit Boards and Schematics can help you (&lt;/SPAN&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=i.MXRT160EVKDS" target="_blank"&gt;&lt;SPAN&gt;https://www.nxp.com/webapp/Download?colCode=i.MXRT160EVKDS&lt;/SPAN&gt;&lt;/A&gt;&lt;SPAN&gt;), it is a reference to design, and in a pdf page 6 have a schematic for an LCDIF&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;I hope it help you&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 17 Nov 2022 05:27:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/LCDIF-RGB-mapping/m-p/1555506#M22519</guid>
      <dc:creator>CarlosGarabito</dc:creator>
      <dc:date>2022-11-17T05:27:56Z</dc:date>
    </item>
  </channel>
</rss>