<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: usb code run on sdram failed in rt1170 in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/usb-code-run-on-sdram-failed-in-rt1170/m-p/1553549#M22471</link>
    <description>&lt;P&gt;ok, I will check it carefully.thanks&lt;/P&gt;</description>
    <pubDate>Tue, 15 Nov 2022 00:51:16 GMT</pubDate>
    <dc:creator>jingyangxie</dc:creator>
    <dc:date>2022-11-15T00:51:16Z</dc:date>
    <item>
      <title>usb code run on sdram failed in rt1170</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/usb-code-run-on-sdram-failed-in-rt1170/m-p/1552867#M22453</link>
      <description>&lt;P&gt;I have a imxrt1170 board, want to run code on sdram, when I debug with iar 9.30，the usb does not work correctly , but when I debug the code on ram , it works fine. the two link files are attachments&lt;/P&gt;</description>
      <pubDate>Mon, 14 Nov 2022 00:35:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/usb-code-run-on-sdram-failed-in-rt1170/m-p/1552867#M22453</guid>
      <dc:creator>jingyangxie</dc:creator>
      <dc:date>2022-11-14T00:35:05Z</dc:date>
    </item>
    <item>
      <title>Re: usb code run on sdram failed in rt1170</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/usb-code-run-on-sdram-failed-in-rt1170/m-p/1553041#M22456</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/114784"&gt;@jingyangxie&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Please refer to these post.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-RT-Knowledge-Base/Using-NonCached-Memory-on-i-MXRT/ta-p/1183369" target="_blank"&gt; https://community.nxp.com/t5/i-MX-RT-Knowledge-Base/Using-NonCached-Memory-on-i-MXRT/ta-p/1183369&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-RT/USB-Host-enumeration-fails/m-p/1436138" target="_blank"&gt;https://community.nxp.com/t5/i-MX-RT/USB-Host-enumeration-fails/m-p/1436138&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/MCUXpresso-IDE/Running-and-debugging-program-in-SDRAM/m-p/1405167" target="_blank"&gt;https://community.nxp.com/t5/MCUXpresso-IDE/Running-and-debugging-program-in-SDRAM/m-p/1405167&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Jing&lt;/P&gt;</description>
      <pubDate>Mon, 14 Nov 2022 07:19:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/usb-code-run-on-sdram-failed-in-rt1170/m-p/1553041#M22456</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2022-11-14T07:19:00Z</dc:date>
    </item>
    <item>
      <title>Re: usb code run on sdram failed in rt1170</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/usb-code-run-on-sdram-failed-in-rt1170/m-p/1553090#M22461</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I've follow these posts, and add definition&amp;nbsp;&lt;STRONG&gt;DATA_SECTION_IS_CACHEABLE=1&lt;/STRONG&gt;,&amp;nbsp; and the link file set the noncache region:&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="jingyangxie_0-1668413121856.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/200183iE7166D357B7EBF52/image-size/medium?v=v2&amp;amp;px=400" role="button" title="jingyangxie_0-1668413121856.png" alt="jingyangxie_0-1668413121856.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;after these ,the usb code debug on sdram still can not work&lt;/P&gt;</description>
      <pubDate>Mon, 14 Nov 2022 08:05:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/usb-code-run-on-sdram-failed-in-rt1170/m-p/1553090#M22461</guid>
      <dc:creator>jingyangxie</dc:creator>
      <dc:date>2022-11-14T08:05:56Z</dc:date>
    </item>
    <item>
      <title>Re: usb code run on sdram failed in rt1170</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/usb-code-run-on-sdram-failed-in-rt1170/m-p/1553092#M22462</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/114784"&gt;@jingyangxie&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Most of these kinds of problem is caused by cache. Please check carefully if the buffers used by both CPU and USB DMA are allocated in noncacheable area. I also suggest to put heap and stack in noncacheable area too.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;jing&lt;/P&gt;</description>
      <pubDate>Mon, 14 Nov 2022 08:11:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/usb-code-run-on-sdram-failed-in-rt1170/m-p/1553092#M22462</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2022-11-14T08:11:06Z</dc:date>
    </item>
    <item>
      <title>Re: usb code run on sdram failed in rt1170</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/usb-code-run-on-sdram-failed-in-rt1170/m-p/1553549#M22471</link>
      <description>&lt;P&gt;ok, I will check it carefully.thanks&lt;/P&gt;</description>
      <pubDate>Tue, 15 Nov 2022 00:51:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/usb-code-run-on-sdram-failed-in-rt1170/m-p/1553549#M22471</guid>
      <dc:creator>jingyangxie</dc:creator>
      <dc:date>2022-11-15T00:51:16Z</dc:date>
    </item>
  </channel>
</rss>