<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUsのトピックimx Rt595 I3C interface</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/imx-Rt595-I3C-interface/m-p/1549342#M22381</link>
    <description>&lt;P&gt;Hello All,&lt;/P&gt;&lt;P&gt;Can anyone please share or point an I3C sample code for the RT595 to me? I would like to run a test sending bytes over I3C. I'm using the MIMXRT595-EVK and I did not find any sample code for this EVK.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Gil&lt;/P&gt;&lt;P&gt;#RT595&lt;/P&gt;</description>
    <pubDate>Mon, 07 Nov 2022 03:47:22 GMT</pubDate>
    <dc:creator>gilmotta2</dc:creator>
    <dc:date>2022-11-07T03:47:22Z</dc:date>
    <item>
      <title>imx Rt595 I3C interface</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/imx-Rt595-I3C-interface/m-p/1549342#M22381</link>
      <description>&lt;P&gt;Hello All,&lt;/P&gt;&lt;P&gt;Can anyone please share or point an I3C sample code for the RT595 to me? I would like to run a test sending bytes over I3C. I'm using the MIMXRT595-EVK and I did not find any sample code for this EVK.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Gil&lt;/P&gt;&lt;P&gt;#RT595&lt;/P&gt;</description>
      <pubDate>Mon, 07 Nov 2022 03:47:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/imx-Rt595-I3C-interface/m-p/1549342#M22381</guid>
      <dc:creator>gilmotta2</dc:creator>
      <dc:date>2022-11-07T03:47:22Z</dc:date>
    </item>
    <item>
      <title>Re: imx Rt595 I3C interface</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/imx-Rt595-I3C-interface/m-p/1549534#M22385</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/205528"&gt;@gilmotta2&lt;/a&gt;&amp;nbsp;，&lt;BR /&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.&lt;BR /&gt;To provide the fastest support, I'd like to refer to the I3C demo in the &lt;A href="https://mcuxpresso.nxp.com/en/welcome" target="_self"&gt;SDK&lt;/A&gt; for RT 595.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the&lt;/P&gt;</description>
      <pubDate>Mon, 07 Nov 2022 08:58:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/imx-Rt595-I3C-interface/m-p/1549534#M22385</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2022-11-07T08:58:27Z</dc:date>
    </item>
    <item>
      <title>Re: imx Rt595 I3C interface</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/imx-Rt595-I3C-interface/m-p/1555470#M22517</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;SDK has two projects. One project is set up for I3C master and the other project is set up for I3C slave.&lt;/P&gt;&lt;P&gt;You can directly use these projects after connecting two MIMXRT595-EVK boards together as mentioned&lt;/P&gt;&lt;P&gt;in the code examples.&lt;/P&gt;</description>
      <pubDate>Thu, 17 Nov 2022 04:25:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/imx-Rt595-I3C-interface/m-p/1555470#M22517</guid>
      <dc:creator>Mahesh_Chandra</dc:creator>
      <dc:date>2022-11-17T04:25:35Z</dc:date>
    </item>
  </channel>
</rss>