<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Using the iMXRT1020 OTP memory to store manufacturing data? in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Using-the-iMXRT1020-OTP-memory-to-store-manufacturing-data/m-p/873277#M2237</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/jeremyzhou"&gt;jeremyzhou&lt;/A&gt;‌ for the quick response.‌&lt;/P&gt;&lt;P&gt;Can we also use ANALOG and MISC_CONF&amp;nbsp;sections?&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Ashish&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 07 Mar 2019 19:03:54 GMT</pubDate>
    <dc:creator>ashishpradhan</dc:creator>
    <dc:date>2019-03-07T19:03:54Z</dc:date>
    <item>
      <title>Using the iMXRT1020 OTP memory to store manufacturing data?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Using-the-iMXRT1020-OTP-memory-to-store-manufacturing-data/m-p/873275#M2235</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We would like to use the OTP (iMXRT1020) to store some of our production/manufacturing data. Would like to know which OTP regions are safe to write to?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The IMXRT1020 reference manual lists the OTP memory footprint as shown below. Could not find information in manual regarding which OTP regions can be used for storing manufacturing data.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have about 60 bytes of manufacturing info that we need to store on OTP. Can we use MEM, SW_GP,GP2 and MAC regions to store the info?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Our product does not have a MAC address so, can the MAC region be used to store some other data viz. serial number instead of MAC address?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="OTP.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/79017i04B086820AB87CEC/image-size/large?v=v2&amp;amp;px=999" role="button" title="OTP.png" alt="OTP.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Ashish&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Mar 2019 17:13:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Using-the-iMXRT1020-OTP-memory-to-store-manufacturing-data/m-p/873275#M2235</guid>
      <dc:creator>ashishpradhan</dc:creator>
      <dc:date>2019-03-06T17:13:58Z</dc:date>
    </item>
    <item>
      <title>Re: Using the iMXRT1020 OTP memory to store manufacturing data?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Using-the-iMXRT1020-OTP-memory-to-store-manufacturing-data/m-p/873276#M2236</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A _jive_internal="true" class="" data-content-finding="Community" data-userid="332492" data-username="ashishpradhan@smarttech.com" href="https://community.nxp.com/people/ashishpradhan@smarttech.com"&gt;Ashish Pradhan&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.&lt;/P&gt;&lt;P&gt;Q1) Can we use MEM, SW_GP, GP2 and MAC regions to store the info?&lt;BR /&gt;-- Yes, you can use the fields except for the MEM field, as the MEM field is reserved section.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Mar 2019 03:24:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Using-the-iMXRT1020-OTP-memory-to-store-manufacturing-data/m-p/873276#M2236</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2019-03-07T03:24:45Z</dc:date>
    </item>
    <item>
      <title>Re: Using the iMXRT1020 OTP memory to store manufacturing data?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Using-the-iMXRT1020-OTP-memory-to-store-manufacturing-data/m-p/873277#M2237</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/jeremyzhou"&gt;jeremyzhou&lt;/A&gt;‌ for the quick response.‌&lt;/P&gt;&lt;P&gt;Can we also use ANALOG and MISC_CONF&amp;nbsp;sections?&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Ashish&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Mar 2019 19:03:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Using-the-iMXRT1020-OTP-memory-to-store-manufacturing-data/m-p/873277#M2237</guid>
      <dc:creator>ashishpradhan</dc:creator>
      <dc:date>2019-03-07T19:03:54Z</dc:date>
    </item>
    <item>
      <title>Re: Using the iMXRT1020 OTP memory to store manufacturing data?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Using-the-iMXRT1020-OTP-memory-to-store-manufacturing-data/m-p/873278#M2238</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A _jive_internal="true" data-containerid="-1" data-containertype="-1" data-content-finding="Community" data-objectid="332492" data-objecttype="3" href="https://community.nxp.com/people/ashishpradhan@smarttech.com"&gt;Ashish Pradhan&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;Thanks for your reply.&lt;BR /&gt;1) Can we also use ANALOG and MISC_CONF sections?&lt;BR /&gt;-- I'm afraid you can't do that.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 Mar 2019 06:53:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Using-the-iMXRT1020-OTP-memory-to-store-manufacturing-data/m-p/873278#M2238</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2019-03-08T06:53:53Z</dc:date>
    </item>
  </channel>
</rss>