<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUsのトピックRe: Jlink flash load problem</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Jlink-flash-load-problem/m-p/1542305#M22183</link>
    <description>&lt;P&gt;Are you using i.MXRT? Which part? Which board and flash?&lt;/P&gt;</description>
    <pubDate>Mon, 24 Oct 2022 00:47:17 GMT</pubDate>
    <dc:creator>jay_heng</dc:creator>
    <dc:date>2022-10-24T00:47:17Z</dc:date>
    <item>
      <title>Jlink flash load problem</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Jlink-flash-load-problem/m-p/1541893#M22166</link>
      <description>&lt;P&gt;I working on zephyr, but it is not&amp;nbsp; a case.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Until i installed mcuxpresso i can't flash cpu using jlink.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I found the command west flash fails and invoked it myself in JLinkExe.&lt;/P&gt;&lt;P&gt;so:&amp;nbsp;J-Link&amp;gt;LoadFile zephyr.bin 0x60000000&lt;/P&gt;&lt;P&gt;i get:&lt;/P&gt;&lt;P&gt;'loadfile': Performing implicit reset &amp;amp; halt of MCU.&lt;BR /&gt;ResetTarget() start&lt;BR /&gt;ResetTarget() end&lt;BR /&gt;AfterResetTarget() start&lt;BR /&gt;AfterResetTarget() end&lt;BR /&gt;Downloading file [zephyr.bin]...&lt;/P&gt;&lt;P&gt;****** Error: Timeout while preparing target, core does not stop. (PC = 0x2000017E, XPSR = 0x41000000, SP = 0x20000B18)!&lt;BR /&gt;Failed to perform RAMCode-sided Prepare()&lt;BR /&gt;Unspecified error -1&lt;/P&gt;&lt;P&gt;I really don't know how to find solution.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 21 Oct 2022 09:29:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Jlink-flash-load-problem/m-p/1541893#M22166</guid>
      <dc:creator>gronoarona</dc:creator>
      <dc:date>2022-10-21T09:29:13Z</dc:date>
    </item>
    <item>
      <title>Re: Jlink flash load problem</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Jlink-flash-load-problem/m-p/1542305#M22183</link>
      <description>&lt;P&gt;Are you using i.MXRT? Which part? Which board and flash?&lt;/P&gt;</description>
      <pubDate>Mon, 24 Oct 2022 00:47:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Jlink-flash-load-problem/m-p/1542305#M22183</guid>
      <dc:creator>jay_heng</dc:creator>
      <dc:date>2022-10-24T00:47:17Z</dc:date>
    </item>
    <item>
      <title>Re: Jlink flash load problem</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Jlink-flash-load-problem/m-p/1542344#M22184</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/198126"&gt;@gronoarona&lt;/a&gt;&amp;nbsp;,&lt;BR /&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.&lt;BR /&gt;I was wondering if you can illustrate the steps of replicating the programming failure.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Mon, 24 Oct 2022 01:53:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Jlink-flash-load-problem/m-p/1542344#M22184</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2022-10-24T01:53:04Z</dc:date>
    </item>
    <item>
      <title>Re: Jlink flash load problem</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Jlink-flash-load-problem/m-p/1545796#M22267</link>
      <description>&lt;P&gt;Sorry for slow answer.&lt;/P&gt;&lt;P&gt;It turns out the problem was with newest&amp;nbsp;jlink&amp;nbsp;linux&amp;nbsp;drivers, after downgraded&amp;nbsp;everything&amp;nbsp;work.&lt;/P&gt;</description>
      <pubDate>Fri, 28 Oct 2022 18:44:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Jlink-flash-load-problem/m-p/1545796#M22267</guid>
      <dc:creator>gronoarona</dc:creator>
      <dc:date>2022-10-28T18:44:06Z</dc:date>
    </item>
    <item>
      <title>Re: Jlink flash load problem</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Jlink-flash-load-problem/m-p/1605577#M23894</link>
      <description>&lt;P&gt;This is a late response, but I consistently experience this issue with J-Link and MIMXRT1064. It is seemingly related to the J-Link version, but has anyone at NXP tested a fresh install recently? J-Link debugging while, for example, the SDK example Blinky is running in onboard flash is unusable. I've tested many different J-Links, all with the same issue.&lt;/P&gt;&lt;P&gt;MCU-Link-Pro doesn't have these issues.&lt;/P&gt;</description>
      <pubDate>Sun, 26 Feb 2023 01:32:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Jlink-flash-load-problem/m-p/1605577#M23894</guid>
      <dc:creator>max3</dc:creator>
      <dc:date>2023-02-26T01:32:06Z</dc:date>
    </item>
  </channel>
</rss>