<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: SEMC SRAM Interface Questions in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SEMC-SRAM-Interface-Questions/m-p/869767#M2189</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SEMC_CSX[0], SEMC_CSX[1], SEMC_CSX[2], and SEMC_CSX[3] has the same function with SEMC_ADD&lt;BR /&gt;R[8] pin. It add more flexible for pin selection during SRAM circuit design.&lt;/P&gt;&lt;P&gt;Thank you for the attention.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Mike&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 01 Feb 2019 07:58:03 GMT</pubDate>
    <dc:creator>Hui_Ma</dc:creator>
    <dc:date>2019-02-01T07:58:03Z</dc:date>
    <item>
      <title>SEMC SRAM Interface Questions</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SEMC-SRAM-Interface-Questions/m-p/869756#M2178</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm going to interface an FPGA to the i.MX RT1062 using the SEMC, operating in SYNC SRAM ADMUX 16-bit mode.&amp;nbsp; I need to make sure I choose the correct pins before I make my PCB.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Why does the documentation use the term "PSRAM" in some places and "SRAM" in others?&amp;nbsp; Is SRAM a subset of PSRAM?&amp;nbsp; For example, in the table in "24.5.3 Pin Mux in SEMC", the "CRE" bit would only apply to PSRAM and I would not need it for the FPGA. I also wouldn't need the "Column Address bit width" bits in register SRAMCR0.&amp;nbsp; All I want is the ability to burst multiple words in a single bus cycle (determined by BL bits in SRAMCR0, which ranges from 1 to 64).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm very confused about the chip selects.&amp;nbsp; Section 24.2.2 describes memory regions, of which SRAM is Region #6.&amp;nbsp; Note that Figure 23-1 is likely in error since it incorrectly shows the wrong CS signals for each type of memory.&amp;nbsp; Section "24.5.3 Pin Mux in SEMC" shows "SEMC_ADDR[8]" as being CS6, which I believe is the CE# signal shown in the timing diagrams.&amp;nbsp; It is selected via IOCR.MUX_A8.&amp;nbsp; Is this CE signal valid for any CS signal?&amp;nbsp; For example, if both SEMC_CSX[0] and SEMC_CSX[1] were enabled on the A24 and A25 pins, the CE# signal would activate when either SEMC_CSX memory region was accessed?&amp;nbsp; This is best described with a picture.&amp;nbsp; Is this correct?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/60098i0941C5384E27AE64/image-size/large?v=v2&amp;amp;px=999" title="CE_CS_Signals.png" alt="CE_CS_Signals.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here are screenshots of the timing diagrams that apply to my intended usage of the SEMC:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/60412i12E28A0E9C414805/image-size/large?v=v2&amp;amp;px=999" title="Figure 24-63 SRAM Read in SYNC Mode (ADMUX).png" alt="Figure 24-63 SRAM Read in SYNC Mode (ADMUX).png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/61240i430892436269337D/image-size/large?v=v2&amp;amp;px=999" title="Figure 24-66 SRAM Write in SYNC Mode (ADMUX).png" alt="Figure 24-66 SRAM Write in SYNC Mode (ADMUX).png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Why is cke shown in the timing diagrams?&amp;nbsp; The reference manual says it only applies to SDRAM.&lt;/P&gt;&lt;P&gt;Is "D0", "D1", etc. Data Word 0, Data Word 1, etc.?&amp;nbsp; It is confusing to use the same nomenclature as the data bits.&amp;nbsp; It would be better to say something like "DW0", "DW1", etc. (assuming I'm correct in my understanding).&amp;nbsp; Are 8 words shown as an example, but the range of possibilities is anywhere from 1 to 64?&lt;/P&gt;&lt;P&gt;Is the DQS signal required?&lt;/P&gt;&lt;P&gt;What is dqse?&lt;/P&gt;&lt;P&gt;Is ipg_clk available on a pin as well as CLK?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your help.&lt;/P&gt;&lt;P&gt;Greg&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Jan 2019 20:12:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SEMC-SRAM-Interface-Questions/m-p/869756#M2178</guid>
      <dc:creator>gcary</dc:creator>
      <dc:date>2019-01-29T20:12:52Z</dc:date>
    </item>
    <item>
      <title>Re: SEMC SRAM Interface Questions</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SEMC-SRAM-Interface-Questions/m-p/869757#M2179</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Greg,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am checking with this thread.&lt;/P&gt;&lt;P&gt;First,&amp;nbsp; about PSRAM (parallel SRAM) relationship with SRAM, I think PSRAM belongs to SRAM.&lt;/P&gt;&lt;P&gt;SRAM includes serial SRAM and PSRAM.&lt;/P&gt;&lt;P&gt;PSRAM is subset of SRAM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BTW: For this thread includes many questions, I will answer in following posts.&lt;/P&gt;&lt;P&gt;Thanks for the understanding.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;best regards,&lt;/P&gt;&lt;P&gt;Mike&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Jan 2019 06:30:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SEMC-SRAM-Interface-Questions/m-p/869757#M2179</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2019-01-30T06:30:52Z</dc:date>
    </item>
    <item>
      <title>Re: SEMC SRAM Interface Questions</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SEMC-SRAM-Interface-Questions/m-p/869758#M2180</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Mike.&amp;nbsp; I realize there were a lot of questions in there.&amp;nbsp; Thank you for tackling them!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I always knew PSRAM to be PseudoSRAM, a DRAM device that has internal refresh and an external interface more like SRAM.&amp;nbsp; On page 1567 of the 1060 reference manual is the following:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/63195i7D6BDC7A66F5DDF9/image-size/large?v=v2&amp;amp;px=999" title="CRE.png" alt="CRE.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I did not know what CRE was, so I downloaded a data sheet from a manufacturer of PsuedoSRAM, and in their data sheet was a signal named CRE.&amp;nbsp; Here is a link to the datasheet.&amp;nbsp; On page 6 it says that it stands for "Control Register Enable".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://www.winbond.com/resource-files/w956d6hb_datasheet_pkg_a01-003_20130529.pdf" title="http://www.winbond.com/resource-files/w956d6hb_datasheet_pkg_a01-003_20130529.pdf"&gt;http://www.winbond.com/resource-files/w956d6hb_datasheet_pkg_a01-003_20130529.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Greg&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Jan 2019 06:51:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SEMC-SRAM-Interface-Questions/m-p/869758#M2180</guid>
      <dc:creator>gcary</dc:creator>
      <dc:date>2019-01-30T06:51:20Z</dc:date>
    </item>
    <item>
      <title>Re: SEMC SRAM Interface Questions</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SEMC-SRAM-Interface-Questions/m-p/869759#M2181</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;About the SRAM chip select, the SRAM read/write timing diagrams CE# only related to&amp;nbsp; SEMC_ADDR[8] pin.&lt;/P&gt;&lt;P&gt;The CE# only available when access Region #6 memory range.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Mike&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Jan 2019 07:22:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SEMC-SRAM-Interface-Questions/m-p/869759#M2181</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2019-01-30T07:22:47Z</dc:date>
    </item>
    <item>
      <title>Re: SEMC SRAM Interface Questions</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SEMC-SRAM-Interface-Questions/m-p/869760#M2182</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;About SRAM read/write in SYNC mode timing diagram, D[0:7] should be data bit.&lt;/P&gt;&lt;P&gt;It only shows one byte during read/write operation.&lt;/P&gt;&lt;P&gt;DQS signal is required.&lt;/P&gt;&lt;P&gt;dqse is module internal signal doesn't output to external SRAM, which is also suitable with ipg_clk.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Mike&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Jan 2019 07:36:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SEMC-SRAM-Interface-Questions/m-p/869760#M2182</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2019-01-30T07:36:32Z</dc:date>
    </item>
    <item>
      <title>Re: SEMC SRAM Interface Questions</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SEMC-SRAM-Interface-Questions/m-p/869761#M2183</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I found some information that supports the definition of PSRAM as PsuedoSRAM:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://en.wikipedia.org/wiki/Dynamic_random-access_memory#PSRAM"&gt;https://en.wikipedia.org/wiki/Dynamic_random-access_memory#PSRAM&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What is the CRE signal for?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Greg&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Jan 2019 21:41:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SEMC-SRAM-Interface-Questions/m-p/869761#M2183</guid>
      <dc:creator>gcary</dc:creator>
      <dc:date>2019-01-30T21:41:15Z</dc:date>
    </item>
    <item>
      <title>Re: SEMC SRAM Interface Questions</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SEMC-SRAM-Interface-Questions/m-p/869762#M2184</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mike,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How do SEMC_CSX[0], SEMC_CSX[1], SEMC_CSX[2], and SEMC_CSX[3] differ from CE# on the SEMC_ADDR[8] pin?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Greg&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Jan 2019 21:44:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SEMC-SRAM-Interface-Questions/m-p/869762#M2184</guid>
      <dc:creator>gcary</dc:creator>
      <dc:date>2019-01-30T21:44:32Z</dc:date>
    </item>
    <item>
      <title>Re: SEMC SRAM Interface Questions</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SEMC-SRAM-Interface-Questions/m-p/869763#M2185</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mike,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I respectfully disagree that the timing diagram shows just one byte being transferred.&amp;nbsp; Apply the same reasoning to Figure 24-57 "SRAM Read in ASYNC mode (ADMUX)".&amp;nbsp; In that diagram you would conclude that just one bit is transferred per bus cycle.&amp;nbsp; There is no way that is the case.&amp;nbsp; If it were, SPI would have greater bandwidth.&amp;nbsp; I think you have proven my point that the documentation is misleading by calling it "D0", "D1", etc.&amp;nbsp; Very bad names.&amp;nbsp; Perhaps "W0", "W1", etc. would be better, since "DW0" is kind of long.&amp;nbsp; The bus width could be 8 bits or 16 bits, which is why it should be called "W0" for "Word0".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I apologize if I am wrong, but I am pretty sure that the performance enhancement of the SYNC bus over ASYNC bus is that a new 8 or 16-bit word can be transferred per clock cycle.&amp;nbsp; Assuming this is the case, how do I set up transfers of this nature?&amp;nbsp; Is DMA required?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Greg&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Jan 2019 22:04:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SEMC-SRAM-Interface-Questions/m-p/869763#M2185</guid>
      <dc:creator>gcary</dc:creator>
      <dc:date>2019-01-30T22:04:44Z</dc:date>
    </item>
    <item>
      <title>Re: SEMC SRAM Interface Questions</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SEMC-SRAM-Interface-Questions/m-p/869764#M2186</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I don't know how I missed it before, but on page 28 of the 1060 Reference Manual it says that PSRAM is Pseudo-Static Random Access Memory.&amp;nbsp; I also found information about it in i.MX6 documentation.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Feb 2019 05:23:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SEMC-SRAM-Interface-Questions/m-p/869764#M2186</guid>
      <dc:creator>gcary</dc:creator>
      <dc:date>2019-02-01T05:23:13Z</dc:date>
    </item>
    <item>
      <title>Re: SEMC SRAM Interface Questions</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SEMC-SRAM-Interface-Questions/m-p/869765#M2187</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, you are right.&lt;/P&gt;&lt;P&gt;The PSRAM is Pseudo-Static Random Access Memory.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please check below description about CRE signal function.&lt;/P&gt;&lt;P&gt;It was abstracted from Micron &lt;A href="http://application-notes.digchip.com/024/24-19998.pdf"&gt; TN-45-30: PSRAM 101: An Introduction to Micron PSRAM - DigChip.&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/64092iC4AC25724B5C5933/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;CRE signal used to access configuration register.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for the attention.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;best regards,&lt;/P&gt;&lt;P&gt;Mike&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Feb 2019 07:29:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SEMC-SRAM-Interface-Questions/m-p/869765#M2187</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2019-02-01T07:29:01Z</dc:date>
    </item>
    <item>
      <title>Re: SEMC SRAM Interface Questions</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SEMC-SRAM-Interface-Questions/m-p/869766#M2188</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Greg,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The timing diagram does make confusion.&lt;/P&gt;&lt;P&gt;The SEMC supported SRAM interface with 8/16 bit data width(mode).&lt;/P&gt;&lt;P&gt;If using 8 bit data width, the D0 should be one byte.&lt;/P&gt;&lt;P&gt;If using 16bit data width, the D0 should be one word (two bytes).&lt;/P&gt;&lt;P&gt;From SRAM control register 0 (SRAMCR0) burst length up to 64 bytes.&lt;/P&gt;&lt;P&gt;The SRAM read/write in SYNC mode figures are just an example for 8 or 16 bytes access.&lt;/P&gt;&lt;P&gt;Thanks for the attention.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Mike&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Feb 2019 07:41:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SEMC-SRAM-Interface-Questions/m-p/869766#M2188</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2019-02-01T07:41:29Z</dc:date>
    </item>
    <item>
      <title>Re: SEMC SRAM Interface Questions</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SEMC-SRAM-Interface-Questions/m-p/869767#M2189</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SEMC_CSX[0], SEMC_CSX[1], SEMC_CSX[2], and SEMC_CSX[3] has the same function with SEMC_ADD&lt;BR /&gt;R[8] pin. It add more flexible for pin selection during SRAM circuit design.&lt;/P&gt;&lt;P&gt;Thank you for the attention.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Mike&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Feb 2019 07:58:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SEMC-SRAM-Interface-Questions/m-p/869767#M2189</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2019-02-01T07:58:03Z</dc:date>
    </item>
  </channel>
</rss>