<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Secure Boot testing without efusing the signature in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Secure-Boot-testing-without-efusing-the-signature/m-p/1529951#M21820</link>
    <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/206945"&gt;@Nagaveni&lt;/a&gt;&amp;nbsp;，&lt;BR /&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.&lt;BR /&gt;1) Can I use open configuration to test the secure boot functionality with signature verification&lt;BR /&gt;-- No, I'm afraid not, in my opinion, I'd like to suggest not enabling the HAB boot in the design phase.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
    <pubDate>Thu, 29 Sep 2022 02:03:48 GMT</pubDate>
    <dc:creator>jeremyzhou</dc:creator>
    <dc:date>2022-09-29T02:03:48Z</dc:date>
    <item>
      <title>Secure Boot testing without efusing the signature</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Secure-Boot-testing-without-efusing-the-signature/m-p/1529561#M21815</link>
      <description>&lt;P&gt;We are using IMX RT 1172&lt;BR /&gt;We are using example project for Secure boot&lt;BR /&gt;My intention is as below&lt;BR /&gt;1. Create hello-world app&lt;BR /&gt;2. Secure it with signature&lt;BR /&gt;3. test it on board&lt;/P&gt;&lt;P&gt;My problem is due to board limited quantizes, I cannot efuse the signature on the board&lt;BR /&gt;Can I use open configuration to test the secure boot functionality with signature verification&lt;/P&gt;</description>
      <pubDate>Wed, 28 Sep 2022 13:22:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Secure-Boot-testing-without-efusing-the-signature/m-p/1529561#M21815</guid>
      <dc:creator>Nagaveni</dc:creator>
      <dc:date>2022-09-28T13:22:44Z</dc:date>
    </item>
    <item>
      <title>Re: Secure Boot testing without efusing the signature</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Secure-Boot-testing-without-efusing-the-signature/m-p/1529951#M21820</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/206945"&gt;@Nagaveni&lt;/a&gt;&amp;nbsp;，&lt;BR /&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.&lt;BR /&gt;1) Can I use open configuration to test the secure boot functionality with signature verification&lt;BR /&gt;-- No, I'm afraid not, in my opinion, I'd like to suggest not enabling the HAB boot in the design phase.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Thu, 29 Sep 2022 02:03:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Secure-Boot-testing-without-efusing-the-signature/m-p/1529951#M21820</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2022-09-29T02:03:48Z</dc:date>
    </item>
  </channel>
</rss>