<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUsのトピックRT1061 Dual Ethernet MDIO Interface Questions</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1061-Dual-Ethernet-MDIO-Interface-Questions/m-p/1521883#M21627</link>
    <description>&lt;P&gt;&amp;nbsp; &amp;nbsp;When using dual network ports, must ENET_MDC, ENET_MDIO and ENET2_MDC, ENET2_MDIO be connected to two PHYs respectively?&lt;BR /&gt;I now use ENET_MDC and ENET_MDIO to connect two PHYs in parallel, and distinguish them by PHY address. The result is that PHY2 has never been initialized, or it is stuck in the initialization process.&lt;/P&gt;&lt;P&gt;&amp;nbsp; The phy register address 0x02 read in the PHY_KSZ8081_Init() function using network 2 is always 0, while network 1 is normal. Here, the MDIO interface shared by network 1 and network 2 is in network 1, and the MDIO interface is not configured on network 2.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="QQ截图20220914181001.png" style="width: 895px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/193606iFA582778FFF0ED01/image-size/large?v=v2&amp;amp;px=999" role="button" title="QQ截图20220914181001.png" alt="QQ截图20220914181001.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;QQ截图20220914181001.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;</description>
    <pubDate>Wed, 14 Sep 2022 10:11:08 GMT</pubDate>
    <dc:creator>2548903578</dc:creator>
    <dc:date>2022-09-14T10:11:08Z</dc:date>
    <item>
      <title>RT1061 Dual Ethernet MDIO Interface Questions</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1061-Dual-Ethernet-MDIO-Interface-Questions/m-p/1521883#M21627</link>
      <description>&lt;P&gt;&amp;nbsp; &amp;nbsp;When using dual network ports, must ENET_MDC, ENET_MDIO and ENET2_MDC, ENET2_MDIO be connected to two PHYs respectively?&lt;BR /&gt;I now use ENET_MDC and ENET_MDIO to connect two PHYs in parallel, and distinguish them by PHY address. The result is that PHY2 has never been initialized, or it is stuck in the initialization process.&lt;/P&gt;&lt;P&gt;&amp;nbsp; The phy register address 0x02 read in the PHY_KSZ8081_Init() function using network 2 is always 0, while network 1 is normal. Here, the MDIO interface shared by network 1 and network 2 is in network 1, and the MDIO interface is not configured on network 2.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="QQ截图20220914181001.png" style="width: 895px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/193606iFA582778FFF0ED01/image-size/large?v=v2&amp;amp;px=999" role="button" title="QQ截图20220914181001.png" alt="QQ截图20220914181001.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;QQ截图20220914181001.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 14 Sep 2022 10:11:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1061-Dual-Ethernet-MDIO-Interface-Questions/m-p/1521883#M21627</guid>
      <dc:creator>2548903578</dc:creator>
      <dc:date>2022-09-14T10:11:08Z</dc:date>
    </item>
    <item>
      <title>Re: RT1061 Dual Ethernet MDIO Interface Questions</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1061-Dual-Ethernet-MDIO-Interface-Questions/m-p/1522778#M21647</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Due to NXP RT1060 EVK only provides one ENET design, I would recommend customer to refer ForLinx &lt;A href="https://www.forlinx.net/single-board-computer/rt1061-45.html" target="_self"&gt;OK1061-S&lt;/A&gt; board dual ENET design, which using two ENET PHYs:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Hui_Ma_0-1663233516173.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/193776iD1BFC1ED34F6BBDB/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Hui_Ma_0-1663233516173.png" alt="Hui_Ma_0-1663233516173.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Hui_Ma_0-1663233516173.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Wish it helps.&lt;/P&gt;
&lt;P&gt;Mike&lt;/P&gt;</description>
      <pubDate>Thu, 15 Sep 2022 09:19:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1061-Dual-Ethernet-MDIO-Interface-Questions/m-p/1522778#M21647</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2022-09-15T09:19:14Z</dc:date>
    </item>
  </channel>
</rss>