<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUs中的主题 Re: RK055HDMIPI4MA0 Jumpers</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RK055HDMIPI4MA0-Jumpers/m-p/1514267#M21366</link>
    <description>&lt;P&gt;I'm also wondering what the purpose is of these extra jumpers as there are already jumpers on the display. The photo below shows the extra 6 jumpers (in a small plastic bag) and the jumpers already inserted on the left side of the display:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="jumpers.jpg" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/191904i9A8D7C2BE43A2706/image-size/large?v=v2&amp;amp;px=999" role="button" title="jumpers.jpg" alt="jumpers.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Perhaps the display is already set up correctly and the extra jumpers are just spares?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also, can someone please confirm if the ribbon cable is inserted into the MIPI LCD connector on the MIMXRT1160-EVK as per the photo below? I'm assuming pin 1 and pin 40 on the display connect to pin 1 and pin 40, respectively, on the&amp;nbsp;MIMXRT1160-EVK but wanted to make sure the orientation is correct before applying power:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="RK055HDMIPI4MA0.jpg" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/191908i665AE88246202EB2/image-size/large?v=v2&amp;amp;px=999" role="button" title="RK055HDMIPI4MA0.jpg" alt="RK055HDMIPI4MA0.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 31 Aug 2022 02:34:16 GMT</pubDate>
    <dc:creator>danielmilutinov</dc:creator>
    <dc:date>2022-08-31T02:34:16Z</dc:date>
    <item>
      <title>RK055HDMIPI4MA0 Jumpers</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RK055HDMIPI4MA0-Jumpers/m-p/1506227#M21070</link>
      <description>&lt;P&gt;Is there a document that has the schematic, or at least just the jumper configuration information, for the&amp;nbsp;RK055HDMIPI4MA0 LCD board? I got a couple to interface with RT1160 and RT1170 EVK boards, but I couldn't find any info on the&amp;nbsp;RK055HDMIPI4MA0 besides the datasheet, which doesn't document what the jumpers do.&lt;/P&gt;</description>
      <pubDate>Mon, 15 Aug 2022 15:08:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RK055HDMIPI4MA0-Jumpers/m-p/1506227#M21070</guid>
      <dc:creator>mpocius</dc:creator>
      <dc:date>2022-08-15T15:08:44Z</dc:date>
    </item>
    <item>
      <title>Re: RK055HDMIPI4MA0 Jumpers</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RK055HDMIPI4MA0-Jumpers/m-p/1507604#M21121</link>
      <description>&lt;P&gt;I am asking if we have some data about it, but that information can be provided by the designer display Rocktech&lt;/P&gt;</description>
      <pubDate>Wed, 17 Aug 2022 16:12:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RK055HDMIPI4MA0-Jumpers/m-p/1507604#M21121</guid>
      <dc:creator>CarlosGarabito</dc:creator>
      <dc:date>2022-08-17T16:12:20Z</dc:date>
    </item>
    <item>
      <title>Re: RK055HDMIPI4MA0 Jumpers</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RK055HDMIPI4MA0-Jumpers/m-p/1514267#M21366</link>
      <description>&lt;P&gt;I'm also wondering what the purpose is of these extra jumpers as there are already jumpers on the display. The photo below shows the extra 6 jumpers (in a small plastic bag) and the jumpers already inserted on the left side of the display:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="jumpers.jpg" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/191904i9A8D7C2BE43A2706/image-size/large?v=v2&amp;amp;px=999" role="button" title="jumpers.jpg" alt="jumpers.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Perhaps the display is already set up correctly and the extra jumpers are just spares?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also, can someone please confirm if the ribbon cable is inserted into the MIPI LCD connector on the MIMXRT1160-EVK as per the photo below? I'm assuming pin 1 and pin 40 on the display connect to pin 1 and pin 40, respectively, on the&amp;nbsp;MIMXRT1160-EVK but wanted to make sure the orientation is correct before applying power:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="RK055HDMIPI4MA0.jpg" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/191908i665AE88246202EB2/image-size/large?v=v2&amp;amp;px=999" role="button" title="RK055HDMIPI4MA0.jpg" alt="RK055HDMIPI4MA0.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 31 Aug 2022 02:34:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RK055HDMIPI4MA0-Jumpers/m-p/1514267#M21366</guid>
      <dc:creator>danielmilutinov</dc:creator>
      <dc:date>2022-08-31T02:34:16Z</dc:date>
    </item>
    <item>
      <title>Re: RK055HDMIPI4MA0 Jumpers</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RK055HDMIPI4MA0-Jumpers/m-p/1514388#M21373</link>
      <description>&lt;P&gt;Actually, I had it upside down. The correct orientation is:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="20220831_162634.jpg" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/191932i37ED4D4A2C21F4F8/image-size/large?v=v2&amp;amp;px=999" role="button" title="20220831_162634.jpg" alt="20220831_162634.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;The "elcdif_rgb_cm7" SDK example works, so it appears the extra jumpers are not needed when the display is used with the&amp;nbsp;&lt;SPAN&gt;MIMXRT1160-EVK&lt;/SPAN&gt;:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="20220831_162526.jpg" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/191933i2898320C221542B3/image-size/large?v=v2&amp;amp;px=999" role="button" title="20220831_162526.jpg" alt="20220831_162526.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Wed, 31 Aug 2022 06:48:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RK055HDMIPI4MA0-Jumpers/m-p/1514388#M21373</guid>
      <dc:creator>danielmilutinov</dc:creator>
      <dc:date>2022-08-31T06:48:05Z</dc:date>
    </item>
    <item>
      <title>Re: RK055HDMIPI4MA0 Jumpers</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RK055HDMIPI4MA0-Jumpers/m-p/1515794#M21425</link>
      <description>&lt;P&gt;hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/163740"&gt;@danielmilutinov&lt;/a&gt;&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/205072"&gt;@mpocius&lt;/a&gt; , here are the schematics, i hope to still help you&lt;/P&gt;</description>
      <pubDate>Thu, 01 Sep 2022 20:03:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RK055HDMIPI4MA0-Jumpers/m-p/1515794#M21425</guid>
      <dc:creator>CarlosGarabito</dc:creator>
      <dc:date>2022-09-01T20:03:22Z</dc:date>
    </item>
    <item>
      <title>Re: RK055HDMIPI4MA0 Jumpers</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RK055HDMIPI4MA0-Jumpers/m-p/1762750#M27706</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/195771"&gt;@CarlosGarabito&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The schematic is very useful and clears up quite a few things. Is is possible to share the design files for the display board too? Its mostly to get the placement of connectors right on our custom board that uses a similar display.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 23 Nov 2023 13:38:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RK055HDMIPI4MA0-Jumpers/m-p/1762750#M27706</guid>
      <dc:creator>ET_Dev</dc:creator>
      <dc:date>2023-11-23T13:38:55Z</dc:date>
    </item>
  </channel>
</rss>