<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUsのトピックRe: lpspi interrupt b2b master example code doesn't work iMXRT1050</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/lpspi-interrupt-b2b-master-example-code-doesn-t-work-iMXRT1050/m-p/1508361#M21152</link>
    <description>&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I'm back with feedback this is a temporary patch, please help evaluate it.&lt;/P&gt;
&lt;P&gt;One known limitation is, the maximum frame length is 512 bytes, and it is from LPSPI IP limitation when work in non-continuous mode.&lt;/P&gt;
&lt;P&gt;If the issue still please let me know.&lt;BR /&gt;Pavel&lt;/P&gt;</description>
    <pubDate>Thu, 18 Aug 2022 17:00:41 GMT</pubDate>
    <dc:creator>Pavel_Hernandez</dc:creator>
    <dc:date>2022-08-18T17:00:41Z</dc:date>
    <item>
      <title>lpspi interrupt b2b master example code doesn't work iMXRT1050</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/lpspi-interrupt-b2b-master-example-code-doesn-t-work-iMXRT1050/m-p/1493548#M20747</link>
      <description>&lt;P&gt;I have imported the&amp;nbsp;lpspi_interrupt_b2b_master example for the MIMXRT1050-EVKB. When I changed the SPI transfer size from 64 bytes to 24, it worked. When I changed the transfer size to less than 24, like 16, it didn't work anymore. Why can't I transfer less than 24 bytes?&lt;/P&gt;</description>
      <pubDate>Thu, 21 Jul 2022 18:50:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/lpspi-interrupt-b2b-master-example-code-doesn-t-work-iMXRT1050/m-p/1493548#M20747</guid>
      <dc:creator>michaeldkfowler</dc:creator>
      <dc:date>2022-07-21T18:50:25Z</dc:date>
    </item>
    <item>
      <title>Re: lpspi interrupt b2b master example code doesn't work iMXRT1050</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/lpspi-interrupt-b2b-master-example-code-doesn-t-work-iMXRT1050/m-p/1495036#M20794</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;I replayed this example on my own, unfortunately, I have the same issue but I tested 8, 15, and 17 transfer sizes, I hope this helps you.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Pavel&lt;/P&gt;</description>
      <pubDate>Mon, 25 Jul 2022 21:41:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/lpspi-interrupt-b2b-master-example-code-doesn-t-work-iMXRT1050/m-p/1495036#M20794</guid>
      <dc:creator>Pavel_Hernandez</dc:creator>
      <dc:date>2022-07-25T21:41:38Z</dc:date>
    </item>
    <item>
      <title>Re: lpspi interrupt b2b master example code doesn't work iMXRT1050</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/lpspi-interrupt-b2b-master-example-code-doesn-t-work-iMXRT1050/m-p/1496741#M20840</link>
      <description>&lt;P&gt;So you will fix the SDK?&lt;/P&gt;</description>
      <pubDate>Wed, 27 Jul 2022 22:54:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/lpspi-interrupt-b2b-master-example-code-doesn-t-work-iMXRT1050/m-p/1496741#M20840</guid>
      <dc:creator>michaeldkfowler</dc:creator>
      <dc:date>2022-07-27T22:54:31Z</dc:date>
    </item>
    <item>
      <title>Re: lpspi interrupt b2b master example code doesn't work iMXRT1050</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/lpspi-interrupt-b2b-master-example-code-doesn-t-work-iMXRT1050/m-p/1497561#M20864</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;I will make a report and when I have more information I will contact you.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Pavel&lt;/P&gt;</description>
      <pubDate>Thu, 28 Jul 2022 22:47:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/lpspi-interrupt-b2b-master-example-code-doesn-t-work-iMXRT1050/m-p/1497561#M20864</guid>
      <dc:creator>Pavel_Hernandez</dc:creator>
      <dc:date>2022-07-28T22:47:39Z</dc:date>
    </item>
    <item>
      <title>Re: lpspi interrupt b2b master example code doesn't work iMXRT1050</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/lpspi-interrupt-b2b-master-example-code-doesn-t-work-iMXRT1050/m-p/1505122#M21032</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;We are working on this issue, thanks for the report. unfortunately, I don't know how much time would take for the new release.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Pavel&lt;/P&gt;</description>
      <pubDate>Thu, 11 Aug 2022 16:49:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/lpspi-interrupt-b2b-master-example-code-doesn-t-work-iMXRT1050/m-p/1505122#M21032</guid>
      <dc:creator>Pavel_Hernandez</dc:creator>
      <dc:date>2022-08-11T16:49:40Z</dc:date>
    </item>
    <item>
      <title>Re: lpspi interrupt b2b master example code doesn't work iMXRT1050</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/lpspi-interrupt-b2b-master-example-code-doesn-t-work-iMXRT1050/m-p/1508361#M21152</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I'm back with feedback this is a temporary patch, please help evaluate it.&lt;/P&gt;
&lt;P&gt;One known limitation is, the maximum frame length is 512 bytes, and it is from LPSPI IP limitation when work in non-continuous mode.&lt;/P&gt;
&lt;P&gt;If the issue still please let me know.&lt;BR /&gt;Pavel&lt;/P&gt;</description>
      <pubDate>Thu, 18 Aug 2022 17:00:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/lpspi-interrupt-b2b-master-example-code-doesn-t-work-iMXRT1050/m-p/1508361#M21152</guid>
      <dc:creator>Pavel_Hernandez</dc:creator>
      <dc:date>2022-08-18T17:00:41Z</dc:date>
    </item>
    <item>
      <title>Re: lpspi polling b2b master example code doesn't work iMXRT1170 EVK boards</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/lpspi-interrupt-b2b-master-example-code-doesn-t-work-iMXRT1050/m-p/2321039#M36230</link>
      <description>&lt;P&gt;Sir,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; We are working on LPSPI&amp;nbsp; polling b2b master imported SDK example code but we are unable to see the clock and data dout in oscilloscope.&lt;/P&gt;&lt;P&gt;&amp;nbsp;MIMXRT1170-EVK boards We are using pins are GPIO_AD_28 for LPSPI1_SCK, GPIO_AD_29 for LPSPI1_PCS0, GPIO_AD_30 for LPSPI1_SDO, GPIO_AD_31 for LPSPI1_SDI.Slave IC CC REF U27 LPSPI Flash.&lt;/P&gt;&lt;P&gt;&amp;nbsp;Request to provide the solution or forward to LPSPI Master full working code.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sun, 22 Feb 2026 14:55:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/lpspi-interrupt-b2b-master-example-code-doesn-t-work-iMXRT1050/m-p/2321039#M36230</guid>
      <dc:creator>Ravi07011983</dc:creator>
      <dc:date>2026-02-22T14:55:44Z</dc:date>
    </item>
  </channel>
</rss>