<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUs中的主题 Re: Using Hyperflash as Data-Storage</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Using-Hyperflash-as-Data-Storage/m-p/1500828#M20918</link>
    <description>&lt;P&gt;Hi NXP&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Could this sample call functions and the code flow can be shared ??&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We are trying to copy the contents from hyperflash to RAM area and then go for flash erase,write and read&lt;/P&gt;&lt;P&gt;with the hex files contents received from serial&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thanks in advance&lt;/P&gt;&lt;P&gt;ratna&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 04 Aug 2022 06:56:09 GMT</pubDate>
    <dc:creator>rathna</dc:creator>
    <dc:date>2022-08-04T06:56:09Z</dc:date>
    <item>
      <title>Using Hyperflash as Data-Storage</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Using-Hyperflash-as-Data-Storage/m-p/833466#M1514</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/tag/MIMX-RT1050-EVK/tg-p"&gt;#MIMX-RT1050-EVK&lt;/A&gt;‌&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Are there any examples around how to use the Hyperflash as Data-Storage while simultaneously running code out of it?&lt;/P&gt;&lt;P&gt;I’m aware that the SDK has some examples for using the flexSPI with NOR and Hyperflash, but this example run out of the On-Chip-RAM.&lt;/P&gt;&lt;P&gt;I believe with running out of the Hyperflash things are a bit different. The Interface should be already initialized by the On-Chip-Bootloader. The routines doing the actual access should be running out of RAM (ITCM) … anything else?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks and Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Aug 2018 15:02:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Using-Hyperflash-as-Data-Storage/m-p/833466#M1514</guid>
      <dc:creator>Masmiseim</dc:creator>
      <dc:date>2018-08-28T15:02:44Z</dc:date>
    </item>
    <item>
      <title>Re: Using Hyperflash as Data-Storage</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Using-Hyperflash-as-Data-Storage/m-p/833467#M1515</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It is not possible to simultaneously execute the code in XiP mode and write data to physically the same HyperFlash memory. A separate HyperFlash memory on the differnt chip select should be used to store data. Or, the code should be loaded into RAM and executed from there.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Aug 2018 08:54:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Using-Hyperflash-as-Data-Storage/m-p/833467#M1515</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2018-08-30T08:54:59Z</dc:date>
    </item>
    <item>
      <title>Re: Using Hyperflash as Data-Storage</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Using-Hyperflash-as-Data-Storage/m-p/833468#M1516</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Artur,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for the reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it enough to executed the Routines which do the actual reading\writing\erasing in the ITCM?&lt;BR /&gt; Based on the NXP-SDK: Is it enough that the routine FLEXSPI_TransferBlocking plus the ones called inside go into the ITCM and the rest is executed in XIP?&lt;BR /&gt; &lt;BR /&gt; I tried to do that and my program is crashing when trying to erase and ending in an endless loop when trying to write some Data. The endless loop is in this one here:&lt;BR /&gt; while (!((status = base-&amp;gt;INTR) &amp;amp; kFLEXSPI_IpTxFifoWatermarkEmpltyFlag))&lt;BR /&gt; {&lt;BR /&gt; }&lt;/P&gt;&lt;P&gt;Reading seems to be working fine.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What do I have to do for the initialization of the flexSPI. When booting from it everything should be initialized by the Bootloder, correct?&lt;BR /&gt; All the things which are done in ‘FLEXSPI_Init’ shouldn’t be necessary, only the LUT should be initialized, right?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Aug 2018 13:38:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Using-Hyperflash-as-Data-Storage/m-p/833468#M1516</guid>
      <dc:creator>Masmiseim</dc:creator>
      <dc:date>2018-08-30T13:38:58Z</dc:date>
    </item>
    <item>
      <title>Re: Using Hyperflash as Data-Storage</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Using-Hyperflash-as-Data-Storage/m-p/833469#M1517</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Q. When booting from it everything should be initialized by the Bootloder, correct? All the things which are done in ‘FLEXSPI_Init’ shouldn’t be necessary, only the LUT should be initialized, right?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A. Seems that only the Read path of the FlexSPI controller is initialized by the BootROM code to XiP the code from HyperFlash. So, the right sequence seems to move the code that initializes the FlexSPI Write path and then performs read/erase/write to ITCM, then jump there, initialize the Write path first and then perform read/erase/write only from ITCM as a separate and complete routine.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Sep 2018 09:47:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Using-Hyperflash-as-Data-Storage/m-p/833469#M1517</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2018-09-04T09:47:54Z</dc:date>
    </item>
    <item>
      <title>Re: Using Hyperflash as Data-Storage</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Using-Hyperflash-as-Data-Storage/m-p/833470#M1518</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hey Artur,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;now everything is working fine. We had some additional problems with the QSPI-Interface instead of the Hyperflash, but now it’s working.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Sep 2018 12:01:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Using-Hyperflash-as-Data-Storage/m-p/833470#M1518</guid>
      <dc:creator>Masmiseim</dc:creator>
      <dc:date>2018-09-18T12:01:09Z</dc:date>
    </item>
    <item>
      <title>Re: Using Hyperflash as Data-Storage</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Using-Hyperflash-as-Data-Storage/m-p/1310067#M15357</link>
      <description>&lt;P&gt;Hi Art. I hope you see this after those years&lt;/P&gt;&lt;P&gt;Did you mean that it is not possible to write to&amp;nbsp;&lt;STRONG&gt;any&lt;/STRONG&gt; address of the same hyperflash that's being used with XIP?&lt;/P&gt;&lt;P&gt;Even if my application is running, say in the first 4KB of a 32MB hyperflash, I cannot write to any address of such hyperflash?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
      <pubDate>Mon, 19 Jul 2021 22:02:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Using-Hyperflash-as-Data-Storage/m-p/1310067#M15357</guid>
      <dc:creator>jose_au_zone</dc:creator>
      <dc:date>2021-07-19T22:02:44Z</dc:date>
    </item>
    <item>
      <title>Re: Using Hyperflash as Data-Storage</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Using-Hyperflash-as-Data-Storage/m-p/1500828#M20918</link>
      <description>&lt;P&gt;Hi NXP&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Could this sample call functions and the code flow can be shared ??&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We are trying to copy the contents from hyperflash to RAM area and then go for flash erase,write and read&lt;/P&gt;&lt;P&gt;with the hex files contents received from serial&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thanks in advance&lt;/P&gt;&lt;P&gt;ratna&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 04 Aug 2022 06:56:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Using-Hyperflash-as-Data-Storage/m-p/1500828#M20918</guid>
      <dc:creator>rathna</dc:creator>
      <dc:date>2022-08-04T06:56:09Z</dc:date>
    </item>
  </channel>
</rss>