<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUsのトピックRe: Complete toolchain with standard libraries</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Complete-toolchain-with-standard-libraries/m-p/1500801#M20917</link>
    <description>&lt;P&gt;&lt;SPAN&gt;Well, sure, but it's kind of a workaround, not a proper solution. There should be a way to build the project without installing IDE, especially as there is a download for gcc-based MCU SDK.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 04 Aug 2022 06:02:33 GMT</pubDate>
    <dc:creator>jakobczyk_woj</dc:creator>
    <dc:date>2022-08-04T06:02:33Z</dc:date>
    <item>
      <title>Complete toolchain with standard libraries</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Complete-toolchain-with-standard-libraries/m-p/1496493#M20837</link>
      <description>&lt;P&gt;I'm trying to build my project on my build server.&lt;/P&gt;&lt;P&gt;I have prepared a makefile and it runs ok on my local machine, when using SDK installed in MCUExpresso IDE (my toolchain is at&amp;nbsp;/usr/local/mcuxpressoide-11.4.1_6260/ide/plugins/com.nxp.mcuxpresso.tools.linux_11.4.0.202103011116/tools/arm-none-eabi/)&lt;/P&gt;&lt;P&gt;However, on my build machine I don't want to install the IDE, so I'm using a gcc-enabled SDK built in the&amp;nbsp;MCU Xpresso SDK Builder and an ARM toolchain downloaded from developer.arm.com.&lt;/P&gt;&lt;P&gt;My problem is that the toolchain does not include some of the libraries used in the project, such as libm,&amp;nbsp;libstdc++_nano or libcr_newlib_semihost.&lt;BR /&gt;These libraries are available in the SDK installed from the IDE.&lt;/P&gt;&lt;P&gt;How can I get these without installing the IDE?&lt;/P&gt;&lt;P&gt;My board is iMX RT1051 and the project is bare metal.&lt;/P&gt;</description>
      <pubDate>Wed, 27 Jul 2022 15:18:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Complete-toolchain-with-standard-libraries/m-p/1496493#M20837</guid>
      <dc:creator>jakobczyk_woj</dc:creator>
      <dc:date>2022-07-27T15:18:21Z</dc:date>
    </item>
    <item>
      <title>Re: Complete toolchain with standard libraries</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Complete-toolchain-with-standard-libraries/m-p/1497096#M20851</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/156136"&gt;@jakobczyk_woj&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Maybe you can install MCUXpresso on another computer and then copy those files to your system.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;jing&lt;/P&gt;</description>
      <pubDate>Thu, 28 Jul 2022 07:34:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Complete-toolchain-with-standard-libraries/m-p/1497096#M20851</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2022-07-28T07:34:50Z</dc:date>
    </item>
    <item>
      <title>Re: Complete toolchain with standard libraries</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Complete-toolchain-with-standard-libraries/m-p/1500801#M20917</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Well, sure, but it's kind of a workaround, not a proper solution. There should be a way to build the project without installing IDE, especially as there is a download for gcc-based MCU SDK.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 04 Aug 2022 06:02:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Complete-toolchain-with-standard-libraries/m-p/1500801#M20917</guid>
      <dc:creator>jakobczyk_woj</dc:creator>
      <dc:date>2022-08-04T06:02:33Z</dc:date>
    </item>
  </channel>
</rss>