<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic usb problem in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/usb-problem/m-p/1498449#M20880</link>
    <description>&lt;P&gt;Hello, I have a confusion. Now I want to connect two identical development boards through USB for data interaction. I checked the example of USB, but I didn't see any example of communication between MCUs. Which one can I refer to? Modified example. The development board is RT1170, Thank you.&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 01 Aug 2022 02:52:01 GMT</pubDate>
    <dc:creator>eao</dc:creator>
    <dc:date>2022-08-01T02:52:01Z</dc:date>
    <item>
      <title>usb problem</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/usb-problem/m-p/1498449#M20880</link>
      <description>&lt;P&gt;Hello, I have a confusion. Now I want to connect two identical development boards through USB for data interaction. I checked the example of USB, but I didn't see any example of communication between MCUs. Which one can I refer to? Modified example. The development board is RT1170, Thank you.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 01 Aug 2022 02:52:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/usb-problem/m-p/1498449#M20880</guid>
      <dc:creator>eao</dc:creator>
      <dc:date>2022-08-01T02:52:01Z</dc:date>
    </item>
    <item>
      <title>Re: usb problem</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/usb-problem/m-p/1499316#M20897</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/204405"&gt;@eao&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Do you mean you want to connect two RT1170 board with USB? That is one board act as a master, the other act as a slave. You can download usb_device_cdc_vcom project to one board and usb_host_cdc to the other. These two project can be found in RT1170 SDK.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Jing&lt;/P&gt;</description>
      <pubDate>Tue, 02 Aug 2022 07:21:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/usb-problem/m-p/1499316#M20897</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2022-08-02T07:21:38Z</dc:date>
    </item>
    <item>
      <title>Re: usb problem</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/usb-problem/m-p/1500020#M20907</link>
      <description>&lt;P&gt;Thanks for the reply, it is probably this one, one as the master and one as the slave. I read the examples in the SDK and found that there is a difference between dev_cdc_vcom and dev_cdc_vcom_lite? thanks&lt;/P&gt;</description>
      <pubDate>Wed, 03 Aug 2022 06:37:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/usb-problem/m-p/1500020#M20907</guid>
      <dc:creator>eao</dc:creator>
      <dc:date>2022-08-03T06:37:55Z</dc:date>
    </item>
    <item>
      <title>Re: usb problem</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/usb-problem/m-p/1500070#M20908</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/204405"&gt;@eao&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;All most same.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Jing&lt;/P&gt;</description>
      <pubDate>Wed, 03 Aug 2022 07:53:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/usb-problem/m-p/1500070#M20908</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2022-08-03T07:53:19Z</dc:date>
    </item>
  </channel>
</rss>