<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUsのトピックQuestion about RMII connection on RT1050EVKB</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Question-about-RMII-connection-on-RT1050EVKB/m-p/740820#M207</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am studying the schematic of the new (A1) version of the RT1050 EVK board.&lt;/P&gt;&lt;P&gt;The schematic shows the signal &lt;SPAN class=""&gt;ENET_CRS_DV coming from the PHY to MCU pin C12, which is described as "ENET_RX_EN". On the other hand, signal ENET_INT goes to G13, which can be associated to ENET_CRS.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;So I wonder if these two signals are swapped, or if there is something I am missing (quite possible, I'm not an expert of Ethernet).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Hints and suggestions?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Giuseppe&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 10 May 2018 08:49:07 GMT</pubDate>
    <dc:creator>giuseppescarpi</dc:creator>
    <dc:date>2018-05-10T08:49:07Z</dc:date>
    <item>
      <title>Question about RMII connection on RT1050EVKB</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Question-about-RMII-connection-on-RT1050EVKB/m-p/740820#M207</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am studying the schematic of the new (A1) version of the RT1050 EVK board.&lt;/P&gt;&lt;P&gt;The schematic shows the signal &lt;SPAN class=""&gt;ENET_CRS_DV coming from the PHY to MCU pin C12, which is described as "ENET_RX_EN". On the other hand, signal ENET_INT goes to G13, which can be associated to ENET_CRS.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;So I wonder if these two signals are swapped, or if there is something I am missing (quite possible, I'm not an expert of Ethernet).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Hints and suggestions?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Giuseppe&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 May 2018 08:49:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Question-about-RMII-connection-on-RT1050EVKB/m-p/740820#M207</guid>
      <dc:creator>giuseppescarpi</dc:creator>
      <dc:date>2018-05-10T08:49:07Z</dc:date>
    </item>
    <item>
      <title>Re: Question about RMII connection on RT1050EVKB</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Question-about-RMII-connection-on-RT1050EVKB/m-p/740821#M208</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Giuseppe&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for names of rmii signals and its usage may be useful also to look&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/317401"&gt;How to use i.MX6SDL ENET_CRS_DV pad for CRS for RMII mode.&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I think there is no &lt;SPAN class=""&gt;swapping, ENET_INT is handled processor as gpio interrupt.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 May 2018 23:10:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Question-about-RMII-connection-on-RT1050EVKB/m-p/740821#M208</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-05-10T23:10:55Z</dc:date>
    </item>
    <item>
      <title>Re: Question about RMII connection on RT1050EVKB</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Question-about-RMII-connection-on-RT1050EVKB/m-p/1851654#M29912</link>
      <description>&lt;P&gt;Hi, I was curious why does the Pin CRS_DV only selected on G13 but not C12, while EVB sch shows it located on C12?&lt;/P&gt;&lt;P&gt;Does it correct?&lt;/P&gt;</description>
      <pubDate>Mon, 22 Apr 2024 13:01:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Question-about-RMII-connection-on-RT1050EVKB/m-p/1851654#M29912</guid>
      <dc:creator>Johnrita</dc:creator>
      <dc:date>2024-04-22T13:01:11Z</dc:date>
    </item>
  </channel>
</rss>