<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: RT1160 driver Init provided no flash parameters in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1160-driver-Init-provided-no-flash-parameters/m-p/1489219#M20592</link>
    <description>&lt;P&gt;For my situation, it turns out it is our PCB design problem. We didn't feed the correct voltage to the source port.&lt;/P&gt;</description>
    <pubDate>Thu, 14 Jul 2022 06:21:20 GMT</pubDate>
    <dc:creator>hedazhuang</dc:creator>
    <dc:date>2022-07-14T06:21:20Z</dc:date>
    <item>
      <title>RT1160 driver Init provided no flash parameters</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1160-driver-Init-provided-no-flash-parameters/m-p/1394779#M17871</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am using customed board with RT1166 chip. While connecting with Linkserver from MCUxpresso, I got the following information:&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;Inspected v.2 External Flash Device on SPI using SFDP JEDEC ID MIMXRT1160_SFDP_QSPI.cfx&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;Image 'iMXRT1160_FlexSPI_SFDP_QSPI Sep 14 2021 15:10:31'&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;Opening flash driver MIMXRT1160_SFDP_QSPI.cfx&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;Sending VECTRESET to run flash driver&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;Driver V.2 dynamic startup failed - driver Init provided no flash parameters&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;Flash Driver V.2 startup failed - rc Ef(55): Dynamic flash driver startup failed to provide flash parameters.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;Terminate (0x0, 0x0, 0x0) status 0x40 - driver reports init failure - EXTSPIJ driver rc 20107 (0x4E8B)&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;chip initialization failed - Ef(55): Dynamic flash driver startup failed to provide flash parameters.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;failed to initialize flash driver MIMXRT1160_SFDP_QSPI.cfx&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It seems that the Flash does not response. I use a 3.3V&amp;nbsp;QSPI Flash with same pin connection as the i.MX RT1160 Evaluation Kit. For the 24MHz crystal, I use an external clock oscillator instead.&lt;/P&gt;&lt;P&gt;I measured the SCK on the Flash, but there is no clock triggered.&lt;/P&gt;&lt;P&gt;The boot_cfg[0 .. 11] is set 0 and Boot_MODE[1:0] is 2b10 as internal boot.&lt;/P&gt;&lt;P&gt;What could the problem be? Where should I check?&lt;/P&gt;&lt;P&gt;Thank you&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 05 Jan 2022 13:11:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1160-driver-Init-provided-no-flash-parameters/m-p/1394779#M17871</guid>
      <dc:creator>hedazhuang</dc:creator>
      <dc:date>2022-01-05T13:11:25Z</dc:date>
    </item>
    <item>
      <title>Re: RT1160 driver Init provided no flash parameters</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1160-driver-Init-provided-no-flash-parameters/m-p/1395194#M17883</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.&lt;BR /&gt;Before answering your question, I was wondering if you can introduce your testing environment, such as debug tool, share schematics, etc&lt;BR /&gt;Before answering your question, &lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Thu, 06 Jan 2022 01:50:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1160-driver-Init-provided-no-flash-parameters/m-p/1395194#M17883</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2022-01-06T01:50:46Z</dc:date>
    </item>
    <item>
      <title>Re: RT1160 driver Init provided no flash parameters</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1160-driver-Init-provided-no-flash-parameters/m-p/1489032#M20578</link>
      <description>&lt;P&gt;&lt;SPAN&gt;I have seen the solved label, but I have not seen the specific solution. If possible, I would like to ask you to list the solution. I would be very grateful.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 14 Jul 2022 00:34:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1160-driver-Init-provided-no-flash-parameters/m-p/1489032#M20578</guid>
      <dc:creator>lishsh</dc:creator>
      <dc:date>2022-07-14T00:34:25Z</dc:date>
    </item>
    <item>
      <title>Re: RT1160 driver Init provided no flash parameters</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1160-driver-Init-provided-no-flash-parameters/m-p/1489219#M20592</link>
      <description>&lt;P&gt;For my situation, it turns out it is our PCB design problem. We didn't feed the correct voltage to the source port.&lt;/P&gt;</description>
      <pubDate>Thu, 14 Jul 2022 06:21:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1160-driver-Init-provided-no-flash-parameters/m-p/1489219#M20592</guid>
      <dc:creator>hedazhuang</dc:creator>
      <dc:date>2022-07-14T06:21:20Z</dc:date>
    </item>
  </channel>
</rss>