<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MIMXRT1060-EVKB LPSPI testing in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1060-EVKB-LPSPI-testing/m-p/1487641#M20528</link>
    <description>&lt;P&gt;Hello&lt;BR /&gt;Hope you are well.&lt;BR /&gt;You are correct, the connections need to be shorted to use those pins.&lt;/P&gt;
&lt;P&gt;If you have more questions do not hesitate to ask me.&lt;BR /&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
    <pubDate>Mon, 11 Jul 2022 20:09:02 GMT</pubDate>
    <dc:creator>Omar_Anguiano</dc:creator>
    <dc:date>2022-07-11T20:09:02Z</dc:date>
    <item>
      <title>MIMXRT1060-EVKB LPSPI testing</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1060-EVKB-LPSPI-testing/m-p/1486950#M20513</link>
      <description>&lt;P&gt;I am trying test the LP SPI on the&amp;nbsp;MIMXRT1060-EVKB Board, and I found that one of the SPI port is on the J17 connector, from the schematic there are DNP commented on the SPI lines.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="niz_1-1657299901846.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/186107i388AC419D552DBA3/image-size/medium?v=v2&amp;amp;px=400" role="button" title="niz_1-1657299901846.png" alt="niz_1-1657299901846.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;niz_1-1657299901846.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Does that mean that I need to short R356, R350, R346 and R362 to make it work with the connector J17?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks a lot for your help&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 08 Jul 2022 17:06:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1060-EVKB-LPSPI-testing/m-p/1486950#M20513</guid>
      <dc:creator>niz</dc:creator>
      <dc:date>2022-07-08T17:06:27Z</dc:date>
    </item>
    <item>
      <title>Re: MIMXRT1060-EVKB LPSPI testing</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1060-EVKB-LPSPI-testing/m-p/1487641#M20528</link>
      <description>&lt;P&gt;Hello&lt;BR /&gt;Hope you are well.&lt;BR /&gt;You are correct, the connections need to be shorted to use those pins.&lt;/P&gt;
&lt;P&gt;If you have more questions do not hesitate to ask me.&lt;BR /&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
      <pubDate>Mon, 11 Jul 2022 20:09:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1060-EVKB-LPSPI-testing/m-p/1487641#M20528</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2022-07-11T20:09:02Z</dc:date>
    </item>
    <item>
      <title>Re: MIMXRT1060-EVKB LPSPI testing</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1060-EVKB-LPSPI-testing/m-p/1489680#M20617</link>
      <description>&lt;P&gt;Hi Omar&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for the confirmation, that is helpful.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have one more question about the CAN testing:&amp;nbsp;&lt;/P&gt;&lt;P&gt;According to the circuit, it needs the 10K pull up resister:&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="niz_0-1657825980139.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/186697i09DAEAA4A53FE622/image-size/medium?v=v2&amp;amp;px=400" role="button" title="niz_0-1657825980139.png" alt="niz_0-1657825980139.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;niz_0-1657825980139.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;So is it OK that we just short the R269 and put the CAN_STBY to high by the MCU without putting 10K resister at R268?&amp;nbsp;&lt;/P&gt;&lt;P&gt;I did this modification without connecting R268, drive the CAN_STBY to high by MCU.&amp;nbsp;&lt;/P&gt;&lt;P&gt;And I cannot send CAN out successfully by running "flexcan_ping_pong_buffer_transfer" example. The&amp;nbsp;MbStatusFlags are always 0 (IFLAG1 and IFLAG2).&lt;/P&gt;&lt;P&gt;So is pull up resister R 267 is a must? or something else might be wrong?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks a lot for your help&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Ni&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 14 Jul 2022 19:17:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1060-EVKB-LPSPI-testing/m-p/1489680#M20617</guid>
      <dc:creator>niz</dc:creator>
      <dc:date>2022-07-14T19:17:21Z</dc:date>
    </item>
    <item>
      <title>Re: MIMXRT1060-EVKB LPSPI testing</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1060-EVKB-LPSPI-testing/m-p/1489692#M20618</link>
      <description>&lt;P&gt;Never mind, I just figure that out, I need to put the standby to low instead of high.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Now I can see it is transmitting messages.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Ni&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 14 Jul 2022 19:56:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1060-EVKB-LPSPI-testing/m-p/1489692#M20618</guid>
      <dc:creator>niz</dc:creator>
      <dc:date>2022-07-14T19:56:10Z</dc:date>
    </item>
  </channel>
</rss>