<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: rt1050 ADC interrupt example in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/rt1050-ADC-interrupt-example/m-p/1480791#M20312</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;I review the example and there is a misspelled with the names of the ADC but use this.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Pavel_Hernandez_0-1656369026134.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/184797i29521B7582C6353A/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Pavel_Hernandez_0-1656369026134.png" alt="Pavel_Hernandez_0-1656369026134.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Pavel_Hernandez_0-1656369026134.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Pavel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 27 Jun 2022 22:31:04 GMT</pubDate>
    <dc:creator>Pavel_Hernandez</dc:creator>
    <dc:date>2022-06-27T22:31:04Z</dc:date>
    <item>
      <title>rt1050 ADC interrupt example</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/rt1050-ADC-interrupt-example/m-p/1478242#M20221</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;i want to work with the ADC on the RT1050. Therefor i imported the example "evkbimxrt1050_adc_12b1msps_sar_interrupt". I routed the ADC IN0 to the connectors J13.&lt;/P&gt;&lt;P&gt;The first question:&amp;nbsp;&lt;/P&gt;&lt;P&gt;As J13 is a 2x Pin header, which header is used?&amp;nbsp;&lt;/P&gt;&lt;P&gt;I connected a variable voltage source with + to J13 Pin1 and - to TB1 for grounding.&lt;/P&gt;&lt;P&gt;The debuging process usw works fine and everytime i press a keyboard button the program returns a value. The main problem is that the returning value is almost constant. It doesnt matter if i power the adc input with 0.1V or 1.0V.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Have i forgot some config settings?&amp;nbsp;&lt;/P&gt;&lt;P&gt;best regards,&lt;/P&gt;&lt;P&gt;Andy&lt;/P&gt;</description>
      <pubDate>Wed, 22 Jun 2022 14:15:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/rt1050-ADC-interrupt-example/m-p/1478242#M20221</guid>
      <dc:creator>Andy_h</dc:creator>
      <dc:date>2022-06-22T14:15:32Z</dc:date>
    </item>
    <item>
      <title>Re: rt1050 ADC interrupt example</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/rt1050-ADC-interrupt-example/m-p/1479385#M20254</link>
      <description>&lt;P&gt;Hello Andy,&lt;/P&gt;
&lt;P&gt;I will work on your case, give me a chance to review your case, when I have more information I will contact you.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Pavel&lt;/P&gt;</description>
      <pubDate>Thu, 23 Jun 2022 23:20:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/rt1050-ADC-interrupt-example/m-p/1479385#M20254</guid>
      <dc:creator>Pavel_Hernandez</dc:creator>
      <dc:date>2022-06-23T23:20:04Z</dc:date>
    </item>
    <item>
      <title>Re: rt1050 ADC interrupt example</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/rt1050-ADC-interrupt-example/m-p/1479979#M20273</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;I review the example, Could you tell me if you are using pin #2 of the header J23? please. I reproduced the same example I do not have any problem, I recommend reviewing the RM to review the ADC IN.&amp;nbsp;&lt;BR /&gt;The &lt;EM&gt;readme.txt&lt;/EM&gt; of the example has the configuration for the&amp;nbsp;&lt;EM&gt;ADC1_IN0.&lt;/EM&gt;&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;&lt;EM&gt;ADC1_IN0 is ADC input. Please sample voltage by J23-2 pin.&amp;nbsp;&lt;/EM&gt;&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Pavel_Hernandez_0-1656103043814.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/184615iC1534FE6DFDE76B2/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Pavel_Hernandez_0-1656103043814.png" alt="Pavel_Hernandez_0-1656103043814.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Pavel_Hernandez_0-1656103043814.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Pavel_Hernandez_1-1656103071253.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/184616iF76CA9BCB025476F/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Pavel_Hernandez_1-1656103071253.png" alt="Pavel_Hernandez_1-1656103071253.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Pavel_Hernandez_1-1656103071253.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;I don't know if you're confused with pin 1 ADC0, tell me if you need more information I'll help you.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Pavel&lt;/P&gt;</description>
      <pubDate>Fri, 24 Jun 2022 20:40:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/rt1050-ADC-interrupt-example/m-p/1479979#M20273</guid>
      <dc:creator>Pavel_Hernandez</dc:creator>
      <dc:date>2022-06-24T20:40:34Z</dc:date>
    </item>
    <item>
      <title>Re: rt1050 ADC interrupt example</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/rt1050-ADC-interrupt-example/m-p/1480658#M20309</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;yes, now it works fine. But i have another question. I want to use the ADC1 with two inout sources. The Problem is that the function adc_GetChannelConversionValue() doesnt take the routed pin channel as parameter. How is it possible to measure two different voltages on different pads?&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 27 Jun 2022 14:36:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/rt1050-ADC-interrupt-example/m-p/1480658#M20309</guid>
      <dc:creator>Andy_h</dc:creator>
      <dc:date>2022-06-27T14:36:54Z</dc:date>
    </item>
    <item>
      <title>Re: rt1050 ADC interrupt example</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/rt1050-ADC-interrupt-example/m-p/1480782#M20311</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;I recommend use another example&amp;nbsp;evkbimxrt1050_adc_etc_hardware_trigger_conv, this could help you.&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;&lt;EM&gt;ADC0_IN15 and ADC1_IN0 are ADC inputs. Please sample voltage by J23-1 and J23-2 pins.&lt;/EM&gt;&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Pavel&lt;/P&gt;</description>
      <pubDate>Mon, 27 Jun 2022 22:19:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/rt1050-ADC-interrupt-example/m-p/1480782#M20311</guid>
      <dc:creator>Pavel_Hernandez</dc:creator>
      <dc:date>2022-06-27T22:19:34Z</dc:date>
    </item>
    <item>
      <title>Re: rt1050 ADC interrupt example</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/rt1050-ADC-interrupt-example/m-p/1480791#M20312</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;I review the example and there is a misspelled with the names of the ADC but use this.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Pavel_Hernandez_0-1656369026134.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/184797i29521B7582C6353A/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Pavel_Hernandez_0-1656369026134.png" alt="Pavel_Hernandez_0-1656369026134.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Pavel_Hernandez_0-1656369026134.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Pavel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 27 Jun 2022 22:31:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/rt1050-ADC-interrupt-example/m-p/1480791#M20312</guid>
      <dc:creator>Pavel_Hernandez</dc:creator>
      <dc:date>2022-06-27T22:31:04Z</dc:date>
    </item>
    <item>
      <title>Re: rt1050 ADC interrupt example</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/rt1050-ADC-interrupt-example/m-p/1481703#M20353</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you very much, now it works fine. I have a last question. Is it possible to configure the ADC to give an interrupt everytime when the conversionvalue changes?&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 29 Jun 2022 09:00:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/rt1050-ADC-interrupt-example/m-p/1481703#M20353</guid>
      <dc:creator>Andy_h</dc:creator>
      <dc:date>2022-06-29T09:00:15Z</dc:date>
    </item>
    <item>
      <title>Re: rt1050 ADC interrupt example</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/rt1050-ADC-interrupt-example/m-p/1482882#M20380</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I think you can active de bit register&amp;nbsp;ADC_GC[ACFE]=1 for active the feature of the comparator.&lt;/P&gt;&lt;P&gt;Then you can read the&amp;nbsp;ADCx_HS to know about the trigger comes from.&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;EM&gt;When the compare function is enabled (ADC_GC[ACFE]=1), the COCOn flag is set&amp;nbsp;upon completion of a conversion only if the compare result is true.&lt;/EM&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Best regards,&lt;BR /&gt;Pavel&lt;/P&gt;</description>
      <pubDate>Thu, 30 Jun 2022 15:31:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/rt1050-ADC-interrupt-example/m-p/1482882#M20380</guid>
      <dc:creator>Pavel_Hernandez</dc:creator>
      <dc:date>2022-06-30T15:31:24Z</dc:date>
    </item>
  </channel>
</rss>