<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic The process of booting to XIP and jumping to SDRAM in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/The-process-of-booting-to-XIP-and-jumping-to-SDRAM/m-p/1480125#M20285</link>
    <description>&lt;P&gt;Hello.&lt;/P&gt;&lt;P&gt;I'm using RT1020-EVK.&amp;nbsp;I want to run the main program from SDRAM.&lt;/P&gt;&lt;P&gt;Please check if the procedure below is correct.&lt;/P&gt;&lt;P&gt;------------------&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;# Preparation&lt;/STRONG&gt;&lt;BR /&gt;-&amp;nbsp;Boot area: XIP operation, copy the main program area of serial flash to SDRAM&lt;BR /&gt;-&amp;nbsp;Program area: XIP operation removal, RAM operation setting, LED blinking&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;#&amp;nbsp;Progress&lt;/STRONG&gt;&lt;BR /&gt;1.&amp;nbsp;The boot region is booted with XIP.&lt;BR /&gt;2.&amp;nbsp;Copy the program area of serial flash to SDRAM.&lt;BR /&gt;3.&amp;nbsp;Jump to the starting point of SDRAM (0x80000000).&lt;BR /&gt;4.&amp;nbsp;The main program is running and the LED is blinking. (?)&lt;/P&gt;&lt;P&gt;------------------&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;# Questions&lt;/STRONG&gt;&lt;BR /&gt;1.&amp;nbsp;Is it possible with the above method?&lt;BR /&gt;1-1.&amp;nbsp;If possible, how do I create a binary file?&lt;BR /&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;A binary file is created in which the boot area with a size of 128KB is arranged from address 0, and the program area with a size of 128KB is arranged from address 0x20000. If I download this from MCUXpresso, is all data normally downloaded to serial flash?&lt;BR /&gt;1-2.&amp;nbsp;If that's not possible, what are the other ways?&lt;BR /&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;It is not possible to use directly SDRAM booting. This is because the method of making a binary file is very complicated and difficult to apply to mass production.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The reason for asking this question is that it takes a very long time to erase the blank area of the serial flash in which the firmware is running while booting with XIP. (link time)&lt;BR /&gt;(I need to write data to the last 2MByte area of serial flash driven by XIP when power is off)&lt;/P&gt;&lt;P&gt;Please help me.&amp;nbsp;&lt;BR /&gt;My RT1020-EVK's MCU fell into a communication failure state and tried to recover, but it doesn't come back to life. So direct testing is not possible.&amp;nbsp;So I leave a question.&lt;BR /&gt;(I tried to enter the debug mode after booting into serial download mode, but it didn't work.)&lt;/P&gt;&lt;P&gt;Thanks in advance for your reply.&lt;BR /&gt;Have a happy day always.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Sun, 26 Jun 2022 14:54:52 GMT</pubDate>
    <dc:creator>stanley-kylee</dc:creator>
    <dc:date>2022-06-26T14:54:52Z</dc:date>
    <item>
      <title>The process of booting to XIP and jumping to SDRAM</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/The-process-of-booting-to-XIP-and-jumping-to-SDRAM/m-p/1480125#M20285</link>
      <description>&lt;P&gt;Hello.&lt;/P&gt;&lt;P&gt;I'm using RT1020-EVK.&amp;nbsp;I want to run the main program from SDRAM.&lt;/P&gt;&lt;P&gt;Please check if the procedure below is correct.&lt;/P&gt;&lt;P&gt;------------------&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;# Preparation&lt;/STRONG&gt;&lt;BR /&gt;-&amp;nbsp;Boot area: XIP operation, copy the main program area of serial flash to SDRAM&lt;BR /&gt;-&amp;nbsp;Program area: XIP operation removal, RAM operation setting, LED blinking&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;#&amp;nbsp;Progress&lt;/STRONG&gt;&lt;BR /&gt;1.&amp;nbsp;The boot region is booted with XIP.&lt;BR /&gt;2.&amp;nbsp;Copy the program area of serial flash to SDRAM.&lt;BR /&gt;3.&amp;nbsp;Jump to the starting point of SDRAM (0x80000000).&lt;BR /&gt;4.&amp;nbsp;The main program is running and the LED is blinking. (?)&lt;/P&gt;&lt;P&gt;------------------&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;# Questions&lt;/STRONG&gt;&lt;BR /&gt;1.&amp;nbsp;Is it possible with the above method?&lt;BR /&gt;1-1.&amp;nbsp;If possible, how do I create a binary file?&lt;BR /&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;A binary file is created in which the boot area with a size of 128KB is arranged from address 0, and the program area with a size of 128KB is arranged from address 0x20000. If I download this from MCUXpresso, is all data normally downloaded to serial flash?&lt;BR /&gt;1-2.&amp;nbsp;If that's not possible, what are the other ways?&lt;BR /&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;It is not possible to use directly SDRAM booting. This is because the method of making a binary file is very complicated and difficult to apply to mass production.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The reason for asking this question is that it takes a very long time to erase the blank area of the serial flash in which the firmware is running while booting with XIP. (link time)&lt;BR /&gt;(I need to write data to the last 2MByte area of serial flash driven by XIP when power is off)&lt;/P&gt;&lt;P&gt;Please help me.&amp;nbsp;&lt;BR /&gt;My RT1020-EVK's MCU fell into a communication failure state and tried to recover, but it doesn't come back to life. So direct testing is not possible.&amp;nbsp;So I leave a question.&lt;BR /&gt;(I tried to enter the debug mode after booting into serial download mode, but it didn't work.)&lt;/P&gt;&lt;P&gt;Thanks in advance for your reply.&lt;BR /&gt;Have a happy day always.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sun, 26 Jun 2022 14:54:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/The-process-of-booting-to-XIP-and-jumping-to-SDRAM/m-p/1480125#M20285</guid>
      <dc:creator>stanley-kylee</dc:creator>
      <dc:date>2022-06-26T14:54:52Z</dc:date>
    </item>
    <item>
      <title>Re: The process of booting to XIP and jumping to SDRAM</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/The-process-of-booting-to-XIP-and-jumping-to-SDRAM/m-p/1480481#M20302</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/202046"&gt;@stanley-kylee&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Please refer to the attachment.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Jing&lt;/P&gt;</description>
      <pubDate>Mon, 27 Jun 2022 09:23:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/The-process-of-booting-to-XIP-and-jumping-to-SDRAM/m-p/1480481#M20302</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2022-06-27T09:23:56Z</dc:date>
    </item>
  </channel>
</rss>