<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: FLEXCAN1 Pins assignment indication for IMXRT105/6x on the reference manual. in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/FLEXCAN1-Pins-assignment-indication-for-IMXRT105-6x-on-the/m-p/863378#M2020</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The pinmux at page 2564 is not correct. The correct is:&lt;/P&gt;&lt;P&gt;FLEXCAN1_TX is muxed on&amp;nbsp;GPIO_AD_B1_08&lt;/P&gt;&lt;P&gt;FLEXCAN1_RX on pin&amp;nbsp;GPIO_AD_B1_09 &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are sorry for the typo and will correct it in next version.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 18 Feb 2019 08:31:11 GMT</pubDate>
    <dc:creator>miduo</dc:creator>
    <dc:date>2019-02-18T08:31:11Z</dc:date>
    <item>
      <title>FLEXCAN1 Pins assignment indication for IMXRT105/6x on the reference manual.</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/FLEXCAN1-Pins-assignment-indication-for-IMXRT105-6x-on-the/m-p/863377#M2019</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;On the reference manual of the IMXRT105/6x microcontrollers ( i'm referreìing to 1052 , 1060 and 1064 in particular ) there is a erratic indication of the pinout for the FLEXCAN1 interface .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For example , referring to the&amp;nbsp;i.MX RT1064 Processor Reference&amp;nbsp;Manual ( Rev. 0.1 ) at page 280 the&amp;nbsp;FLEXCAN1_TX is indicated that can be&amp;nbsp;muxed on&amp;nbsp;pin GPIO_AD_B1_08 ( or&amp;nbsp;GPIO_B0_02, or&amp;nbsp;GPIO_EMC_17, or GPIO_SD_B1_02 ) and FLEXCAN1_RX is muxed on&amp;nbsp;GPIO_AD_B1_09 ( or&amp;nbsp;GPIO_B0_03 , or&amp;nbsp;GPIO_EMC_18 , or&amp;nbsp;GPIO_SD_B1_03 ).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, on the same manual, at page 2564, the FLEXCAN1_TX is muxed on&amp;nbsp;GPIO_AD_B1_09 and FLEXCAN1_RX on pin&amp;nbsp;GPIO_AD_B1_08 : they are pratically inverted respect to what declared previously ...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The MCUXpresso Config Tools 5.0 software indicates the FLEXCAN1 pinout as indicated at page 280 of said reference manual.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can NXP confirm that the user manual has an error on page 2564 ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Feb 2019 13:41:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/FLEXCAN1-Pins-assignment-indication-for-IMXRT105-6x-on-the/m-p/863377#M2019</guid>
      <dc:creator>GottiLuca</dc:creator>
      <dc:date>2019-02-14T13:41:29Z</dc:date>
    </item>
    <item>
      <title>Re: FLEXCAN1 Pins assignment indication for IMXRT105/6x on the reference manual.</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/FLEXCAN1-Pins-assignment-indication-for-IMXRT105-6x-on-the/m-p/863378#M2020</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The pinmux at page 2564 is not correct. The correct is:&lt;/P&gt;&lt;P&gt;FLEXCAN1_TX is muxed on&amp;nbsp;GPIO_AD_B1_08&lt;/P&gt;&lt;P&gt;FLEXCAN1_RX on pin&amp;nbsp;GPIO_AD_B1_09 &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are sorry for the typo and will correct it in next version.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Feb 2019 08:31:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/FLEXCAN1-Pins-assignment-indication-for-IMXRT105-6x-on-the/m-p/863378#M2020</guid>
      <dc:creator>miduo</dc:creator>
      <dc:date>2019-02-18T08:31:11Z</dc:date>
    </item>
    <item>
      <title>Re: FLEXCAN1 Pins assignment indication for IMXRT105/6x on the reference manual.</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/FLEXCAN1-Pins-assignment-indication-for-IMXRT105-6x-on-the/m-p/863379#M2021</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Mr. Li,&lt;/P&gt;&lt;P&gt;Many thanks for the clarification.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;L.Gotti&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Feb 2019 10:47:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/FLEXCAN1-Pins-assignment-indication-for-IMXRT105-6x-on-the/m-p/863379#M2021</guid>
      <dc:creator>GottiLuca</dc:creator>
      <dc:date>2019-02-19T10:47:32Z</dc:date>
    </item>
  </channel>
</rss>