<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: i.MX RT1050 parallel RGB LCD H-res / dot clock rating in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i-MX-RT1050-parallel-RGB-LCD-H-res-dot-clock-rating/m-p/861633#M2004</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&amp;gt;&amp;gt;What is the maximum dot clock ?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;The LCD_DOTCLK is max 75MHz, see LCDIF_CLK_ROOT in Reference Manual, please!&lt;/P&gt;&lt;P&gt;&amp;gt;&amp;gt;what is the maximum RGB dots per HSYNC that can be supported ?&lt;/P&gt;&lt;P&gt;HSYNC is determined by dotclock, resolution &amp;amp; Frames per second.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&amp;gt;&amp;gt;Wanting to use 1280 pixel horizontal in RGB666&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;LCDIF on i.MXRT1050 supprts WXGA(1280x800), which is max resolution, you can calculate dot clock according to requirments, assume 60fps &amp;amp; 50fps &amp;amp; 30fps:&amp;nbsp; &amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; --&amp;nbsp; dot clock = 1280x800 * 60 * 130% =79.872MHz.&amp;nbsp; &amp;gt;&amp;nbsp; 75MHz&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; dot clock = 1280x800 * 50 * 130% =51.2MHz.&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;lt;&amp;nbsp; 75MHz&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; dot clock = 1280x800 * 30 * 130% =39.936MHz.&amp;nbsp; &amp;lt; 75MHz&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; [ 30% is reserved for "blank" ]&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Taking 30fps an example:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; -- display data (Byte) = 1280x800 *3*30 = 92.16MB/s&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; If external SDRAM can work at 166MHz,&amp;nbsp; the resolution should be OK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; So you can evaluate it according to your requirments.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a nice day!&lt;/P&gt;&lt;P&gt;Weidong Sun&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 10 Jan 2019 05:20:32 GMT</pubDate>
    <dc:creator>weidong_sun</dc:creator>
    <dc:date>2019-01-10T05:20:32Z</dc:date>
    <item>
      <title>i.MX RT1050 parallel RGB LCD H-res / dot clock rating</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i-MX-RT1050-parallel-RGB-LCD-H-res-dot-clock-rating/m-p/861632#M2003</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What is the maximum dot clock / what is the maximum RGB dots per HSYNC that can be supported ?&amp;nbsp; (DPI interface)&lt;/P&gt;&lt;P&gt;Wanting to use 1280 pixel horizontal in RGB666&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Jan 2019 08:16:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i-MX-RT1050-parallel-RGB-LCD-H-res-dot-clock-rating/m-p/861632#M2003</guid>
      <dc:creator>Bugger</dc:creator>
      <dc:date>2019-01-09T08:16:36Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX RT1050 parallel RGB LCD H-res / dot clock rating</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i-MX-RT1050-parallel-RGB-LCD-H-res-dot-clock-rating/m-p/861633#M2004</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&amp;gt;&amp;gt;What is the maximum dot clock ?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;The LCD_DOTCLK is max 75MHz, see LCDIF_CLK_ROOT in Reference Manual, please!&lt;/P&gt;&lt;P&gt;&amp;gt;&amp;gt;what is the maximum RGB dots per HSYNC that can be supported ?&lt;/P&gt;&lt;P&gt;HSYNC is determined by dotclock, resolution &amp;amp; Frames per second.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&amp;gt;&amp;gt;Wanting to use 1280 pixel horizontal in RGB666&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;LCDIF on i.MXRT1050 supprts WXGA(1280x800), which is max resolution, you can calculate dot clock according to requirments, assume 60fps &amp;amp; 50fps &amp;amp; 30fps:&amp;nbsp; &amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; --&amp;nbsp; dot clock = 1280x800 * 60 * 130% =79.872MHz.&amp;nbsp; &amp;gt;&amp;nbsp; 75MHz&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; dot clock = 1280x800 * 50 * 130% =51.2MHz.&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;lt;&amp;nbsp; 75MHz&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; dot clock = 1280x800 * 30 * 130% =39.936MHz.&amp;nbsp; &amp;lt; 75MHz&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; [ 30% is reserved for "blank" ]&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Taking 30fps an example:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; -- display data (Byte) = 1280x800 *3*30 = 92.16MB/s&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; If external SDRAM can work at 166MHz,&amp;nbsp; the resolution should be OK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; So you can evaluate it according to your requirments.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a nice day!&lt;/P&gt;&lt;P&gt;Weidong Sun&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Jan 2019 05:20:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i-MX-RT1050-parallel-RGB-LCD-H-res-dot-clock-rating/m-p/861633#M2004</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2019-01-10T05:20:32Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX RT1050 parallel RGB LCD H-res / dot clock rating</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i-MX-RT1050-parallel-RGB-LCD-H-res-dot-clock-rating/m-p/861634#M2005</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;How can I set LCD PANEL CLOCK ? I use an MXRT 1050 microprocessor.&amp;nbsp;&lt;EM&gt; I need to know which registers I have to set.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Thank you&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Best Regards&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Giovanni Grondona&lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Jan 2019 11:01:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i-MX-RT1050-parallel-RGB-LCD-H-res-dot-clock-rating/m-p/861634#M2005</guid>
      <dc:creator>giannigrondona</dc:creator>
      <dc:date>2019-01-17T11:01:45Z</dc:date>
    </item>
  </channel>
</rss>