<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUsのトピックRe: Boot from NAND Flash</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Boot-from-NAND-Flash/m-p/1462169#M19702</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/195606"&gt;@Ankush_9881&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;1. Yes, NAND flash doesn't support XIP because it doesn't support random read.&lt;/P&gt;
&lt;P&gt;2. Yes, the code in NAND flash must be read to RAM before executing. ROM bootloader is capable to do so.&lt;/P&gt;
&lt;P&gt;3. Please see the 10.6.2 section in reference manual.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Jing&lt;/P&gt;</description>
    <pubDate>Mon, 23 May 2022 06:20:06 GMT</pubDate>
    <dc:creator>jingpan</dc:creator>
    <dc:date>2022-05-23T06:20:06Z</dc:date>
    <item>
      <title>Boot from NAND Flash</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Boot-from-NAND-Flash/m-p/1451761#M19414</link>
      <description>&lt;P&gt;Hello All,&lt;/P&gt;&lt;P&gt;&amp;nbsp;I am working on the custom board of iMXRT1176. We are exploring with the NAND memory and have some query for the same.&lt;/P&gt;&lt;P&gt;1. As existing memory is NOR Flash and XIP is there but in case of Serial NAND Flash it is not possible! Am i right ?&lt;/P&gt;&lt;P&gt;2. If XIP is not possible then for Serial NAND Flash , need to copy the code from NAND flash to SDRAM and run from there. Is ROM boot is capable of doing same ?&lt;/P&gt;&lt;P&gt;3. If the ROM Boot is not capable , how do the same ?&lt;/P&gt;&lt;P&gt;Thanks in Advance&lt;/P&gt;&lt;P&gt;Ankush&lt;/P&gt;</description>
      <pubDate>Mon, 02 May 2022 09:39:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Boot-from-NAND-Flash/m-p/1451761#M19414</guid>
      <dc:creator>Ankush_9881</dc:creator>
      <dc:date>2022-05-02T09:39:00Z</dc:date>
    </item>
    <item>
      <title>Re: Boot from NAND Flash</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Boot-from-NAND-Flash/m-p/1462169#M19702</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/195606"&gt;@Ankush_9881&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;1. Yes, NAND flash doesn't support XIP because it doesn't support random read.&lt;/P&gt;
&lt;P&gt;2. Yes, the code in NAND flash must be read to RAM before executing. ROM bootloader is capable to do so.&lt;/P&gt;
&lt;P&gt;3. Please see the 10.6.2 section in reference manual.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Jing&lt;/P&gt;</description>
      <pubDate>Mon, 23 May 2022 06:20:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Boot-from-NAND-Flash/m-p/1462169#M19702</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2022-05-23T06:20:06Z</dc:date>
    </item>
  </channel>
</rss>